Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Intelligent Wheelchair: Mechanical/Electrical Specifications
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: vu2iti
  • Date Created: 7 Dec 2013 4:20 PM Date Created
  • Views 1636 views
  • Likes 1 like
  • Comments 6 comments
  • psoc4
  • smarter_life_challenge
  • intelligent_wheelchair
  • smarter_life
Related
Recommended

Intelligent Wheelchair: Mechanical/Electrical Specifications

vu2iti
vu2iti
7 Dec 2013

Intelligent Wheelchair Specifications

 


image

Figure1. Wheelchair showing the BLDC motors and Battery compartment

 

My idea of an intelligent wheelchair comes to my mind because of my 22 year old daughter Greeshma. She is mentally and physically disabled and her wheelchair ‘Karma’ ( http://www.karmahealthcare.com) is her best friend! Karma is not intelligent, it is a manual one. I am thinking of making an intelligent wheel chair for my daughter.

The dimensions of the wheel chair are fixed that is suitable for a person like her and is as note below:

a. Wheelchair Mechanical Specifications:

    • Maximum carrying  capacity : 100kg
    • Body using aircraft aluminum for light weight ( 25 Kg Maximum)
    • Width of the seat : 40cm
    • length of the seat : 45 cm
    • Height of the seat : 50 cm
    • Inclination of the seat: adjustable

b.    Electrical Specifications

    • Motor Specifications:
      • BLDC Hub Motor : 24V 100W  ( 2 Nos.)
      • Torque: 14Nm
      • Diameter: 30cm

c. Control system

    • Distance sensors ( front and rear)
    • Floor sensors
    • Head movement detectors
    • Speed Sensors (left and right)
    • Battery monitoring
    • More features will be added

d. Overall specifications:

    • Maximum Forward speed: 9km/h
    • Maximum Reverse speed: 3km/hr
    • Capacity of motors:100W, 7Nm
    • Battery : 24V 15Ah
    • Carrying capacity :100kg
    • Turning radius  : 0.5m   
    • Climbing capacity: 12⁰
    • Breaking distance:<1m
    • obstacle detection: 20-150cm
    • min height of obstacle: 6cm
  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 11 years ago

    Hey, very nice site. I came across this on Google, and I am stoked that I did. I will definitely be coming back here more often. Wish I could add to the conversation and bring a bit more to the table, but am just taking in as much info as I can at the moment. Thanks for sharing.

     

    Karma KM-8020

     

     

    Keep Posting:)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vu2iti
    vu2iti over 12 years ago in reply to tomluque

    Thank you for your suggestion. I am using a MEMS sensor and that can also be used as a tilt sensor.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • tomluque
    tomluque over 12 years ago

    Incorporate a mercury tilt switch as fail safe.  There tilt switches with 4 poles and single poles.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vu2iti
    vu2iti over 12 years ago in reply to vsluiter

    Dear Victor Slutier,

    Yest Safety is the very important aspect. If the controller fails, then the whellchair will not move. All possible safety mechanisms like obstacle detection, slope, acceleration, braking in case of enmergency, panic alrams etc are to be incorporated. For a toatally disbale person, helper assisted drivng is only allowed. I wll be updating on these features in the next blog post.

    Thanks

    -Mani

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago

    Hi Mani,

     

    An autonomous wheelchair... That raises questions on safety with me. Have you thought about how your daughter could switch off the device when it fails?

     

    It's a very ambitious project, which will probably take longer than the PSOC Smarter Life challenge. I would love to see some updates during your build / design!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
>