Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog IO and Resource Allocation Spreadsheets
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: steveturner
  • Date Created: 10 Dec 2013 10:49 PM Date Created
  • Views 643 views
  • Likes 0 likes
  • Comments 2 comments
  • smarter_life
Related
Recommended

IO and Resource Allocation Spreadsheets

steveturner
steveturner
10 Dec 2013

When I start a new project one of the first tasks is matching the needed IO to the resources available on the microprocessor. I create a spreadsheet to keep track of the connections and any changes as I move through the design steps. I've done a few PSoC projects now and thought I would share my spreadsheet. Perhaps others will find them helpful.

 

If you find any errors, please post them in the comments or send a message to me.

 

PSoC Family Resources

The attachment named "PSoC_Ports.xls" shows all the ports for the PSoC3, 4 and 5LP family. This snapshot on the left below shows my setup notes for my current PSoC Design Challenge project The UnCoStat. It's not going to solve all your problems, but hopefully it will save some of you a little time.

          imageimage

 

PSoC4 Pioneer Development Board

When I am dealing with a board such as the PSoC4 Pioneer, I want to connect my external circuits in a logical manner, based on the pinout of the board. For that, I made the attached spreadsheet named "PSOC4 Pioneer Ports.xls". This spreadsheet lays out the pins in the approximate location on the board, so I can group all the signals for a sub-circuit together on the board. The PSoC family makes this easy, since most signals can be on any pin, it's really easy to move signals around so it is user friendly on the board resulting in Less Breadboard Errors!

 

I hope some of you find this helpful.

Attachments:
PSoC_Ports.xlsPSoC_Ports.xls
PSoC4 Pioneer Ports.xlsPSoC4 Pioneer Ports.xls
  • Sign in to reply
Parents
  • DAB
    DAB over 12 years ago

    Hi Steve,

     

    Good move.

    The more you get things organized and documented the easier it gets to build and test the device.

    Input/output issues usually consume about 50% of integration and test time.

    Plus they are the one area in a project where you can actually release the magic smoke.  So it is to your benefit to double check the I/O.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 12 years ago

    Hi Steve,

     

    Good move.

    The more you get things organized and documented the easier it gets to build and test the device.

    Input/output issues usually consume about 50% of integration and test time.

    Plus they are the one area in a project where you can actually release the magic smoke.  So it is to your benefit to double check the I/O.

     

    DAB