Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Oven Control with PSOC 4: Post 7
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: malamitra
  • Date Created: 21 Dec 2013 5:25 PM Date Created
  • Views 1283 views
  • Likes 2 likes
  • Comments 6 comments
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • oven_control
  • smarter_life
Related
Recommended

Oven Control with PSOC 4: Post 7

malamitra
malamitra
21 Dec 2013

I started with the op-amps. I put it in the non-inverting mode,  I measured the voltage at the Arduino compatible I/O header J2.  I could measure only digital voltage VDD = 3.42 volt. When the noninverting input is connected to VSS the output becomes zero. There is no in-between value. Though  I  selected 3 analog pins. I took one example for op-amp. For this also no analog output. If the pins can give only digital output then why analog pins are listed in components? Next I'll try the ADC input pins and check whether I can get an analog value. Following gives the screen-shot of the circuit.


image

 

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 12 years ago

    Hi Dab,

    It's not that weird is it? Looks like a standard noninverting opamp...Pin2 has a voltage divider as input, and pin 1 is the inverting input. Output voltage would be ( 1+(10k/20k))*Vin.

     

    Mala: please do check all connections, I think you can also set up an opamp as buffer. If you're missing the feedback resistor it 'll act as a comparator....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to vsluiter

    Hi Victor,

     

    My eyesight is not what it used to be, which is why it looked a little strange.

    That and I was less than coherent yesterday due to pain and sinus issues.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to DAB

    No problem, hope that you're having less pain now.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago in reply to DAB

    No problem, hope that you're having less pain now.