Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Oven Control with PSOC 4: Post 7
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: malamitra
  • Date Created: 21 Dec 2013 5:25 PM Date Created
  • Views 1282 views
  • Likes 2 likes
  • Comments 6 comments
  • psoc4
  • psoc_4
  • smarter_life_challenge
  • oven_control
  • smarter_life
Related
Recommended

Oven Control with PSOC 4: Post 7

malamitra
malamitra
21 Dec 2013

I started with the op-amps. I put it in the non-inverting mode,  I measured the voltage at the Arduino compatible I/O header J2.  I could measure only digital voltage VDD = 3.42 volt. When the noninverting input is connected to VSS the output becomes zero. There is no in-between value. Though  I  selected 3 analog pins. I took one example for op-amp. For this also no analog output. If the pins can give only digital output then why analog pins are listed in components? Next I'll try the ADC input pins and check whether I can get an analog value. Following gives the screen-shot of the circuit.


image

 

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 12 years ago

    Hi Dab,

    It's not that weird is it? Looks like a standard noninverting opamp...Pin2 has a voltage divider as input, and pin 1 is the inverting input. Output voltage would be ( 1+(10k/20k))*Vin.

     

    Mala: please do check all connections, I think you can also set up an opamp as buffer. If you're missing the feedback resistor it 'll act as a comparator....

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • malamitra
    malamitra over 12 years ago in reply to vsluiter

    DAB! Do you mean giving a positive voltage as input to the inverting terminal? In that case output should be zero as the op-amp is single supply. Isn't it?  I tried voltage follower as well. But the same problem occurs. I tried opamp0 as well. In this case, the output is 1.21 volt for an input of 0.3 volt. Whereas the output should be 0.45 volt as the gain is 1.5. Victor! Do you mean voltage follower when u r suggesting buffer? I tried that. For opamp1 the output is  always digital. For opamp0 the output is incorrect. 

     

    What are these off-chip components? Do they really exist on the board or the user needs to connect it externally. Is this facility provided to get the schematic and a successful build?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • malamitra
    malamitra over 12 years ago in reply to vsluiter

    DAB! Do you mean giving a positive voltage as input to the inverting terminal? In that case output should be zero as the op-amp is single supply. Isn't it?  I tried voltage follower as well. But the same problem occurs. I tried opamp0 as well. In this case, the output is 1.21 volt for an input of 0.3 volt. Whereas the output should be 0.45 volt as the gain is 1.5. Victor! Do you mean voltage follower when u r suggesting buffer? I tried that. For opamp1 the output is  always digital. For opamp0 the output is incorrect. 

     

    What are these off-chip components? Do they really exist on the board or the user needs to connect it externally. Is this facility provided to get the schematic and a successful build?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • vsluiter
    vsluiter over 12 years ago in reply to malamitra

    Hi Mala,

     

    You need to put them outside the chip, that's probably the reason why it doesn't work image They just exist 'graphically', to make the circuit make sense on screen.