Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Post 3: Smarter Life Challenge: Oven Control with PSOC 4
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: malamitra
  • Date Created: 10 Nov 2013 5:46 PM Date Created
  • Views 1139 views
  • Likes 0 likes
  • Comments 7 comments
  • psoc_4
  • smarter_life_challenge
  • oven_control
  • smarter_life
Related
Recommended

Post 3: Smarter Life Challenge: Oven Control with PSOC 4

malamitra
malamitra
10 Nov 2013

In post 2, block diagram for control voltage implementation was given. This control voltage can be actuated in many ways. The standard technique is PWM i.e. longer off time for the control pulse or less duty cycle that keeps the heating coil off for a longer time when the actual temperature is more than the set-point temperature. As DAB pointed out rightly, this may give too many on-offs, an undesirable effect. A smooth control is possible by use of a Voltage Variable Resistor (VVR). VVR may be implemented by a MOSFET, SCR or TRIAC. In case of MOSFET, the device can be kept in saturation region. As current varies in a quadratic manner with overdrive voltage the dc resistance changes very fast in this region. By reducing the resistance more heating of the coil is possible. If the actual temperature is much above the set-point, switch off can be done by applying a control voltage to the gate below the threshold voltage. On-Semi MCH 3481 is a suitable device for this implementation. At port pin of PSOC 4 the control voltage that can be sent is 0 to 5.5 volt. MCH 3481 can accept maximum gate voltage of 9 volts. This is well above 5.5 volts. The threshold voltage is 0.9 volts. The control vector can be scaled to the range 0.9 to 5.5 volts. If sensed temperature or actual temperature goes too high control voltage can be set to zero. This will switch off the circuit.


Update of the week is:

1. Listing of the components.

2. Download of CadSoft Eagle. But board development will be difficult as vendors take only bulk order. I could not find any simulation facility to do a total hardware simulation of PID controller. I am not getting the idea how to utilize the tool for this project. 

3. Spending a lot of time to get the kit. The board has reached Bangalore on 6th .  The last promise from the courier UPS is: they will deliver it on Monday, anytime between 8.30 am to 3.30 pm. I am not in a hurry. A safe and smooth delivery  without any damage of the kit is all that I am trying.

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 12 years ago

    Hello Mala,

    I'm using iteadstudio or Wuerth Elektronik for fast prototyping, both do small orders. Simulating a  full board is done, but unusual. The most practical way is - in general - to simulate a few core sections, and then design a PCB / protoboard. Nasty side effects never show up in simulations, so doing 'the real stuff' is very important.

    You could of course also do PID control in the digital domain, in the PSOC.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • malamitra
    malamitra over 12 years ago in reply to vsluiter

    Thanks a lot Victor for your comments. I need only 1 or 2 boards. No vendor in Bangalore will agree for that. For small order, the delivery date is uncertain. I do not have any plan for board simulation. I have got the license for Eagle Cadsoft as a part of facilities provided by the organizers. I am wondering how to utilize it That's all.

     

    How to do PID in digital domain? We need to do differentiation and integration. Do you mean PID in software? Yes, I am doing that for comparison. Several multiplications are there. I am using hardware multiplier.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to malamitra

    Hi Mala,

     

    PID is software is very wel possible, There's a very widely used library for Arduino, which is also ported to mbed. Here's some good documentation on that:

    We've used up to 4 PID controllers in parallel on the Freescale KL25Z for a student project. these were all running at 1kHz cycle time, using floating point multiplications! Don't underestimate the power of a Cortex-M0 !

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to vsluiter

    Here's the link: http://mbed.org/cookbook/PID

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago in reply to vsluiter

    Here's the link: http://mbed.org/cookbook/PID