Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog PSoC Challange "Smart reflow oven"
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: Kilohercas
  • Date Created: 1 Nov 2013 10:02 AM Date Created
  • Views 2119 views
  • Likes 3 likes
  • Comments 15 comments
  • stm32f429i-disco
  • smps
  • pwm
  • uart
  • smarter_life
  • amoled
  • pid
  • reflow_oven
  • psoc
Related
Recommended

PSoC Challange "Smart reflow oven"

Kilohercas
Kilohercas
1 Nov 2013

Hello, i would like to present my Smart Life challenge idea.

 

I am thinking about making reflow oven. It will have 3.7 inch capacitive touchscreen with 800x480 AMOLED or SLCD screen for user interace as well as encoder for setting up time and temperatures of each reflow process steps. (maybe i will going to use unipolar stepper for this function, since it has very positive feedback, and very long life span )

 

 

PSoC4/5 will run control algorithms for heating, and so on. I will use two K type thermocouples for temperature measurement ( maybe one will be glued to small pcb with only copper and solder mask to get idea about this arrangement temperature, and also maybe second thermocouple will be glued to small FR4 board, to get idea about pcb temperature without any copper around.So i could guess temperature of pcb. It will get all commands for GUI controller ( for now i am thinking about STM32F429isince i need lot of power to drive large 800x480 screen and at the same time get information from touchscreen

 

And third large part will be SMPS for heating. Since i want to get precise temperature control, i will use PWM control for heaters.  I don't want to use SCR , or even relay, since it can produce high temperature fluctuations.

 

Ok so first job was to reverse engineer HTC desire screen. that take me some time, but i finally get it working, so now i can produce similar user experience as any high end smartphone can give for users. I will share code and pin-out, so others can try this out  ( as well as where to get connectors, since it nonstandard 10 pin 0,4mm pitch small size board to board  connector)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Still have many problems with AMOLED screen. It has not only RGB565 interface but also SPI interface for seting up screen, and at this time i don't know exact registers and data. but at least, i getit display something. This part will be hardest in this project

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Now comes easy part, making 2000-3000W PWM controller for heater. For now i am thinking about PWM controller driving high power IGBT transistor, and all data will come via Analog ISO digital I2C or simple isolator, since i don't want to have common ground that is directly connected to heater ground. So i will have to separate power supply, one for driver electronics, one for heater control electronics, simple .

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

YES, get AMOLED panel working with my user interface controller. That was very very hard, but result is superb. I guess that would be oven with best display in the market image
Only problem is that screen is 800x480, i will try to get resolution cut by half of each axis (240x400 would be tip top but i will have to add small fpga fr it, bummer )

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

wow, quality compared to other screens are just mind boggling

 

Fullscreen contentimage_45769.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

mini IR oven for my project. Its 800W and it has nice flat side for touchscreen mounting. Problem is, it will "just fit" with not much place around.

image

Also, all markings will be removed, and if all goes well, i have access to laser engraver for some custom markings ( in university we have laser marking machine ). Biggest problem is that i have very little room for my PWM controller, 12v power supply and my driver. I bet i have to integrate all electronics on single pcb and also send it to OHS Park for manufacturing, so not much time to spear image

 

Heater power control

 

As you might know,i will use PWM control, so i can adjust heating power , and by doing that i should get better temperature control ( low temperature "ringing" with flat temperature profile )

Idea is this. PSoC 5 will generate PWM signal by measuring temperature from sensors, and adjusting pulse width according to PID controller state. Set point will be controlled by STM32F429 via UART. At start-up, PSoC will check if driver has ULVO, if yes, displays error, since i can't run power mosfet with gate voltage below 10V. Temperature fault will not be used, since i have 100mOhms MOSFET and rms current is just 5A, that is very little of heat. ( maybe i will add more heaters to get faster heating curve, but for now original heaters will work just fine.

 

Simple schematic:

image

 

User interface

image

Hrr, is is very hard to make nice looking front panel. I have no room for any mountings, also very little room for AMOLED itself.
Plan is to use FR4 sheets, cut it with cnc, and glue them . For now it's my only option

 

If some one still has a question, do i really need stm32f429i, here is the answer : (still, it's only for basic functions, more pins will be used in this design )

 

image

 

 

 

 

 

 

 

 

 

Still lot of work to be done.

  • Sign in to reply
  • e14 Contributor
    e14 Contributor over 12 years ago in reply to Kilohercas

    Think of ZC based switching as a PWM with 50Hz clock image

    you could use PSoC's hardware PWM and take external zero cross signal as it's clock source.

    From software point of view the result would be more or less identical to high speed PWM solution - same duty cycle control as before.

    But there would be no RF noise, and depending on switching solution, less heat problems.

     

    Heating element is slow to respond anyway, so you're not loosing any features by using slower PWM.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Kilohercas
    Kilohercas over 12 years ago in reply to e14 Contributor

    I will get heat only on bridge rectifier, since form my HV work, i have many high power FET/IGBT transistors.  I can do zero switching, but that would mean i have very small control over heater ( i know, it would work just fine, but i have no experience on SCR ). I can use pulse picker topology for heating control, but that will add some complexity. PWM is simple and effective from design time perspective it is already working since all i need is to set duty cycle, and PWM will do all magic, no measurements, no other task are needed for heating control. Downside as you mentioned is RF noise and Heat, but i can live with that
    Ačiū

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 12 years ago

    heater control looks very problematic:

    1. you will be getting a lot of RF noise when trying to PWM high voltage power line.

    2. by using PWM you are also doing way too many on/off transitions on your IGBT which results in a lot of heat and the need for expensive IGBT.

    3. bridge is also generating a lot of heat.

     

    doesn't the heater run off AC? if so why not using a simple zero-cross enabled optocoupler + triac?

    this would be simple, would save some heat, but still not super efficient.

     

    and if it does need DC or you just want to make it very efficient, then you would be able to solve all 3 issues above by using 2 N-mosfets(4 if DC is needed) like this:

    http://1.bp.blogspot.com/-NhkIxnLAraY/Ty2HT74B3cI/AAAAAAAAAEg/kzvyyHG3at4/s1600/ac+main+switch+mosfet+app.JPG

     

    i used similar schematic for a dimmer and it makes basically no heat - if switching on zero cross you should be able to use 2 mosfets with no heatsink at all, saving not only power but space and cooling issues.

     

    Sėkmės image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Kilohercas
    Kilohercas over 12 years ago in reply to vsluiter

    I don't like idea that i use other part for this project. I could do simple reflow oven, with 16x2 character by using only Cypress parts without any problem ( i would use PSoC 5 ), but it's not a challenge then. This project is not cost orientated, it's more lets do what i wanted to do and see how it turns out.

    This would be the first oven capable of running precision temperature control for cooking, and at the same time fractal calculation on screen ( Mandelbrot or Julia series )

     

    And where is no question if i going to use 800x480 AMOLED screen, i have to use high end mcu. In other forum ( my.ST.com ) i get lot of pounding that my STM32F429i is too weak for large AMOLED panel like mine, i should switch to Arm Cortex A8/9/15 for that.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to Kilohercas

    Very good, you convinced me image that it's a sh..load of work to get going from the PSOC, and indeed, you don't have much time. Wouldh have been nice though...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>