Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Smarter Life Challenge - Researching coffee and espresso machines
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: PaulMakesThings
  • Date Created: 29 Oct 2013 3:10 AM Date Created
  • Views 900 views
  • Likes 1 like
  • Comments 4 comments
  • psoc4
  • smarter_life_challenge
  • smarter_life
  • auto_barista
Related
Recommended

Smarter Life Challenge - Researching coffee and espresso machines

PaulMakesThings
PaulMakesThings
29 Oct 2013

I’m looking into coffee makers to use as the basis of my design. It seems like a logical first step since it will help me narrow down what features are viable. I still haven’t decided if I want to use an espresso machine or one that just makes coffee.

 

The case for using an espresso machine

 

An espresso machine is needed to make a wide variety of drinks. Espresso is used in lattes, mochas, cappuccinos and Americanos. It is also generally more impressive, a coffee maker just makes coffee and other drinks that use hot water. In either case I’ll probably need to automatically clean the machine somehow. Since it will be heavily modified I'm open to using a used one too, and a quick search shows I could get a decent home quality one for about $400 that way.

 

The case for just using a coffee maker

 

Most espresso machines cost nearly the whole budget for the project. I haven’t found any that don’t involve several manual steps that would need to be automated. For example you must grind the coffee into the portafilter (the metal cup with a nozzle) then press it up into the grouphead (the part that pushes the hot water through the coffee), lock it into place and then start the brewing. Besides that it would need a way to clean the portafilter. This could certainly be automated, but it might not be practical in the amount of time I have. Also, there are coffee machines that include a lot of the features I need such as automatically grinding the beans.

 

Making my own?

 

Probably the least practical option since time is limited, but I have found examples of people making their own espresso machine.

Robo-Pavoni-minimal, and well designed, this is basically a well controlled brewing head without all the other parts attached. If I were to take the route of making my own this would be a good starting point

Portable espresso plunger - This is basically what I have seen called an Aeropress elsewhere, it would just be a part of the machinery needed, but it could be a starting point. It's basically a pneumatic ram with a filter at the end, you pour in boiling water and force it through the filter with the air plunger.

The main advantage of building my own would be that it would save money on parts I would modify anyway. If I buy a ready made machine I'm going to be pulling out and cutting up a lot of the existing hardware. I'm sure if I need to I can make parts that meet the mechanical requirements to make good espresso, so this option isn't totally off the table.

 

I'll be getting into more technical specifics and feature specifications as the project develops.

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 12 years ago

    As an avid Aeropress user I'd be completely in favor of that one. I also use the steel mesh available for it; it minimizes waste! My favourite electrical coffee maker is my 70's Krups T8 Typ264 (Typ265 is more widespread) which unfortunately broke down a few weeks ago. The principle is very nice. An air tight seal is created, and the device uses a pressostat to push the boiling water with constant force through the grounds.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • PaulMakesThings
    PaulMakesThings over 12 years ago in reply to vsluiter

    I really appreciate your feedback because there are so many options. I do like the idea of an Aeropress - I enjoy the flavor you get, it would be easy to adjust the brew time, amount of grounds and fineness of grind, and the process should be easier to automate than some others. I was unaware that there were screened ones, and that really helps because removing and replacing the filter automatically was a big concern, it would have to happen cleanly enough to not leave torn filter bits, and accurately enough that the filter wasn't being bypassed. I'll read up on the screen kind, if it could simply be flushed with water that would be very practical to automate.

     

    The main reason I might not do it this way is that I seem to have gotten that espresso machine I had a lead on. I'm hoping I wont have to gut it too much because it's a nice unit, I would like to keep it as close to original as possible. Maybe if I can get a robot arm on the cheap I'll just have it run the machine!

     

    Thanks again for the feedback!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • PaulMakesThings
    PaulMakesThings over 12 years ago in reply to vsluiter

    I really appreciate your feedback because there are so many options. I do like the idea of an Aeropress - I enjoy the flavor you get, it would be easy to adjust the brew time, amount of grounds and fineness of grind, and the process should be easier to automate than some others. I was unaware that there were screened ones, and that really helps because removing and replacing the filter automatically was a big concern, it would have to happen cleanly enough to not leave torn filter bits, and accurately enough that the filter wasn't being bypassed. I'll read up on the screen kind, if it could simply be flushed with water that would be very practical to automate.

     

    The main reason I might not do it this way is that I seem to have gotten that espresso machine I had a lead on. I'm hoping I wont have to gut it too much because it's a nice unit, I would like to keep it as close to original as possible. Maybe if I can get a robot arm on the cheap I'll just have it run the machine!

     

    Thanks again for the feedback!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • vsluiter
    vsluiter over 12 years ago in reply to PaulMakesThings

    You're welcome. My steel filter is the "Kaffeologie"