Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Smight - smart light system project
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: gelmi
  • Date Created: 30 Oct 2013 8:25 PM Date Created
  • Views 1498 views
  • Likes 2 likes
  • Comments 6 comments
  • pioneer_kit
  • psoc4
  • smight
  • smarter_life
Related
Recommended

Smight - smart light system project

gelmi
gelmi
30 Oct 2013

Hello to you all!

I would like to give you an overview of my project idea I am planning to execute for this challenge. I have called this project Smigth as a shortened version of smart light system. Probably all of us have seen some movies on youtube showing automation systems for homes. I don't know about you, but I would like to have one of these at my place. There is one tiny problem which prevents me from getting it. These systems are pretty expensive. That is why I want to realize an affordable automation system. At the moment the lightning system is the one I would like to automate and make it smart. Since I do not carry smartphone on me at all times at home and I do not feel like clapping every time I want to turn on or off the lights, I thought that it would be really cool if I could control the lightning system through voice commands, real life phrases. And not only 'switch on/off', but also 'dim the kitchen light', 'create romantic mood' and stuff like that. Wouldn't that be great?image

We all have different bulbs at home – energy friendly, LED, normal ones, halogen, etc. – so I will try to cover most of them. Since PSoC4 chips are based on Cortex-M0 (energy friendly, but not so powerful computation units), I will use them for driving the bulbs, running lightning scenarios and communicating with a more powerful unit for voice recognition and Internet connectivity. I am thinking about Raspberry Pi for this. I will report about technical stuff every time I make some progress or I have some interesting (in my opinion) thoughts.

I told you what I want to do and how. Now, I would like to tell you why I have decided to do this. There are multiple reasons. Since I was a kid, I have always wanted to have voice controlled home automation system and now the technology is ready for this. Hopefully, some of you will benefit from my project and my posts. Plus, I believe that this system can help me and you save some money on electricity bills. Also this might be the first step to some affordable automation smart system for the whole house. And the last reason for me is to avoid the situations when I am reading a book in my bed, suddenly I get sleepy and I have to turn off the lights. I don't know about you but when I am in my warm bed I don't feel like walking just to switch off the lights image

So, that's it. That's my idea and my reasons. Hope you enjoyed this post and you will follow my updates. If you have some ideas that could help me to improve this project, do not hesitate to post a comment below.

  • Sign in to reply

Top Comments

  • vsluiter
    vsluiter over 12 years ago in reply to gelmi +1
    Ha! The conductive paint - capacitive sensing seems such a weird idea to me that it's ultimately fascinating to try out. Have you seen this? http://makezine.com/projects/a-touchless-3d-tracking-interface…
Parents
  • DAB
    DAB over 12 years ago

    Sounds interesting.

     

    With the built in programable analog devices, you should be able to set up an audio input and then set up a few basic commands for it to recognize and implement.

     

    Are you considering RF or local Wifi to cover all of you devices?

     

    You might also consider the Cypress capacitive touch capability to detect room to room change to keep lights following you through the house.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • gelmi
    gelmi over 12 years ago in reply to DAB

    DAB, right now I am focusing on getting everything working on cables as fast as I can, but if I have some time left I am going to use BlueTooth LE as a communication interface between nodes. Since the devices will be mains powered I have also considered sending data via home power lines image But transmitters are not so cheap.

    As for capacitive touch I wanted to replace on/off switches with touch ones. Also, this sound a little crazy, but some time ago I was wondering if I painted a room with some conductive paint, could I use walls to detect human bodies? Methodology just like cap based accelerometers with a small ball inside. Wouldn't that be great image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to gelmi

    Good idea.

    Once you verify the comm ports, you can then add the RF stuff one channel at a time with only the RF being an issue.

     

    I like the idea of the conductive paint, but I would first use conductive tape on the door jams to see if you can detect movement.

    You might be able to use two sets per door to detect when you leave one and enter another.

    Using the conductive tape also lets you experiment with how large a surface you need.  You might get by with just a small strip.

     

    Either way, it sounds like fun testing out the options.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to gelmi

    Ha!

    The conductive paint - capacitive sensing seems such a weird idea to me that it's ultimately fascinating to try out.

    Have you seen this?

    http://makezine.com/projects/a-touchless-3d-tracking-interface/

    Your idea would just be enlarging the surfaces image

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago in reply to vsluiter

    Hi Victor,

     

    Thanks for the post.  I wonder if you could use this approach for action capture?

    Hmm, I might have to find some time to experiment.

     

    DAB


    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to DAB

    DAB,

     

    I guess you can only vaguely determine position of someone in space; if possible at all. With several people you'd get an average blob position image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago in reply to DAB

    DAB,

     

    I guess you can only vaguely determine position of someone in space; if possible at all. With several people you'd get an average blob position image