Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Soil moisture sensor assembly
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: wireb
  • Date Created: 9 Dec 2013 10:17 PM Date Created
  • Views 737 views
  • Likes 1 like
  • Comments 2 comments
  • psoc4
  • smarter_life_challenge
  • soil_moisture_sensor
  • soil
  • smarter_life
  • sensor
  • moisture
Related
Recommended

Soil moisture sensor assembly

wireb
wireb
9 Dec 2013

Finally got all packed from Thanksgiving and having a good leg day so decided to get down to the shop and work on building up the sensor boards.

 

image

Here are the boards as they arrived from OSH park. Went with the minimum order of 3 for now until I am sure no other changes are needed on the boards.

 

image

Manually applied the solder paste (direct from the syringe) and placed the first part (LED1).

 

image

Boards all placed and ready for the reflow oven.

 

image

Boards loaded in my toaster reflow oven ready for heat. Note the wire on the right side is the thermal couple probe inserted in a via on the card. This way I get a accurate card temp over a general air temp in the oven.

 

image

Here is my reflow setup left to right I have a over insulated toaster oven, Kearsarge timer, and PID thermal controller. Start to cool down it takes a little under 3 minutes to reflow a oven full of cards. Typically I just crack the door on the oven and let the cards cool naturally.

 

image

While waiting for the cards to cool I put together a quick sensor to Pioneer kit adapter. One thing I noted about the kit is the included wires don't make good connections in the headers on the kit. To get a better connection I cut up a 0.1" pin strip and soldered the pins on the end of all the connections.

 

image

Cards post reflow but before cleaning. Joints look good and no opens or shorts found. Next a quick scrub with rubbing alcohol to remove the flux and loose solder then a rinse and blow dry and they are ready to go.

 

image

image

Sensor wires attached and sensor ready for use. Long term plan is to coat the sensor in epoxy or silicone to provide strain relief on the cable and protect it from moisture.

 

image

And the sensor wired up to the pioneer kit. Did a quick probe of the sensor output to verify functionality with my scope and all looks good so far. Hopefully if I don't have a relapse on the leg I should have about 6 hours to work on it this Friday. Plan is to finish up the frequency counter code and set up a quick data logger so I can collect some real data off one of my plants.   

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 12 years ago

    Nice update. You're right about the wires, they're a bit flimsy. I folded the ends to have some spring-like action.

    Hope your sensors work!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago

    Nice update. You're right about the wires, they're a bit flimsy. I folded the ends to have some spring-like action.

    Hope your sensors work!