Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog SteadyClip, An Economical Camera Gimbal – Part 04: Logistics and Roadblocks
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: jliu83
  • Date Created: 10 Nov 2013 10:56 PM Date Created
  • Views 1371 views
  • Likes 1 like
  • Comments 7 comments
  • pioneer
  • steady_clip
  • psoc4
  • smarter_life_challenge
  • motors
  • smarter_life
  • brushless_dc_motor
Related
Recommended

SteadyClip, An Economical Camera Gimbal – Part 04: Logistics and Roadblocks

jliu83
jliu83
10 Nov 2013

I had high hopes of getting a significant portion of the design finish this weekend, but it seems like I’ve hit a road block.  It seems that upgrading to the latest operating system might have hindered my efforts to create the SteadyClip.  The PSoC 4 Pioneer Kit doesn’t seem to enumerate on the USB port when I plug the device into a Windows 8.1 machine.  As it stands right now, I cannot get any code loaded into my device. I’ve opened a ticket with Cypress and hopefully this gets resolved quickly.

 

On the electronic hardware front, I am waiting for some parts to arrive.  I have also added several parts to my EDA suite’s library. When and if the time comes to spin a board, I should be able to pump one out revisions relatively fast.  On a separate note, since I no longer have access to my lab and tools of my last job, I might opt to use off the shelf hardware for the whole project.  Previously, it was rather convenient to etch a set of boards in the kitchen sink.

 

So what’s new?  Well I’ve thought about the approach that I will take to create this design.  Perhaps this is only in hindsight, but I think I might have bitten off more than I can chew. What I mean by this is that there is a lot of mechanical parts to this project, and I am woefully unprepared in terms of tools and skill to create anything mechanical.  I’m looking to see if there are any suitable pieces of hardware off of EBay that I can make modifications in order to get frame that I can use as the mechanical prototype.  The alternative is to head to the hardware store, buy a Dremel type tool, and see if I can make something meaningful.  I am leaning towards the EBay option.

 

On the software side, I’m worried about the program timing determinism. Since I will be using a PID as the control loop for the motors, the timing will need to be rather critical.  The D portion of the PID constant uses the rate of the controller error.  If my time slices are off, then the D portion of the controller will not work properly.  The loop that does the PID loop iteration must be relatively accurate.  Due to this timing complication, software becomes rather complicated to write.

 

I’ve taken a look at some event processors that will take care of the timing for me.  Instead of having to play around with multiple interrupts racing against each other, the event processor should facilitate the whole affair.  Think of it as a simplified operating system, and as long as I remain within the guidelines of the API calls, I should be able to guarantee the timing requirements of my PID loops.  Since I’ve used the QP event processor before, I’ve decided to see if they have a solution for the ARM Cortex M series.  Luckily a lot of the difficult work in porting over the code to ARM Cortex M has been done.  I just needed to compile the library using the gcc compiler included in PSOC Creator package.  At least this portion of went pretty smoothly.  Now if only I can load the code and test it out in my PSoC 4 Pioneer Kit…

  • Sign in to reply

Top Comments

  • jliu83
    jliu83 over 12 years ago in reply to cy.gul +1
    Hi Gagan, thank you for your response. The issue has been fixed. Cypress support was very quick to reply and I was able to resolve the issue on Tuesday. It's a rather busy week for me as I have been trying…
Parents
  • vsluiter
    vsluiter over 12 years ago

    Ouch. The Windows 8.1 issue has also blocked some mbed functionality. One of my students found that out....

    On the programming side: in the project with that student we used a software based PID. The timing source is a timer interrupt. You should be able to create something like that from the standard timers, or from a digital timer block in the PSOC, generating an interrupt at which time you calculate your PID.

     

    Good luck,

    Victor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago

    Ouch. The Windows 8.1 issue has also blocked some mbed functionality. One of my students found that out....

    On the programming side: in the project with that student we used a software based PID. The timing source is a timer interrupt. You should be able to create something like that from the standard timers, or from a digital timer block in the PSOC, generating an interrupt at which time you calculate your PID.

     

    Good luck,

    Victor

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jliu83
    jliu83 over 12 years ago in reply to vsluiter

    Thanks Victor, I'm glad I'm not the only one with the problems.  As for the software based PID, of course the timer interrupt can be used.  However, my concern is the race conditions if other interrupts are used.  These race conditions can be somewhat mitigated by using an event processor, and that's why I went to the extra length to compile the library.  We will see if it is useful, but as of right now, there's not much for me to do (due to the Windows 8.1 issue).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • vsluiter
    vsluiter over 12 years ago in reply to jliu83

    Hey Jianyi,

    I think race conditions can be easily avoided when using interrupt levels and short interrupt code, but that's my experience image I've never used QP before, would be nice to see your experience with that!