Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Blog Temperature Sensor
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: e14 Contributor
  • Date Created: 19 Nov 2013 4:14 AM Date Created
  • Views 667 views
  • Likes 0 likes
  • Comments 1 comment
  • sleep_sensor
  • psoc4
  • smarter_life_challenge
  • smarter_life
Related
Recommended

Temperature Sensor

e14 Contributor
e14 Contributor
19 Nov 2013

Hello All,

 

I have been having good momentum in the past few weeks. I was able to get the FRAM I2C to work. You can see the example code below:

 

/********************************************
writeSample
- Writes one 16 bit (two byte) sample to FRAM
- Uses FRAM automatic incrementing
- Assumes that A1 and A0 lines are set to logic zero
********************************************/
void writeSample(uint32 addr, uint16 sample)
{
  uint8 slaveAddr = 0x50;
  uint8 pageBit = 0;
  uint8 msb = 0;
  uint8 lsb = 0;

  //Step 1: Break address into components, set the slave address
  pageBit = HI16(addr) & 1U;
  msb = HI8(LO16(addr));
  lsb = LO8(LO16(addr));
  slaveAddr |= pageBit;

  //Step 2: Write the slave address/page bit & address MSB/LSB to FRAM
  I2C_I2CMasterSendStart(slaveAddr, 0);
  I2C_I2CMasterWriteByte(msb);
  I2C_I2CMasterWriteByte(lsb);

  //Step 3: Write the MSB then LSB of the sample to FRAM
  I2C_I2CMasterWriteByte(HI8(sample));
  I2C_I2CMasterWriteByte(LO8(sample));
  I2C_I2CMasterSendStop();
}

 

I recently hit a stumbling block though. The amount of data transferred off of the FRAM is so large that my computer has difficulty processing all of the USB-UART data! I've been hoping to get around this by using a Python script with PySerial:

 

import sys

import csv

import serial

 

#Setup serial port

ser = serial.Serial(port='COM22', baudrate=115200, timeout=60)

 

#Read

myData = ser.readline()

ser.close()  

 

So far, this has kind of been working. I will need to determine how I can get around this stumbling block. I hope to have a more interesting blog post next time with some sleep data.

  • Sign in to reply
Parents
  • vsluiter
    vsluiter over 12 years ago

    Hello Alex,

    One question, two hints:

    * I thought you would like to use a very low power solution. How are you going to combine that with sending so much data that your computer is getting into trouble?

    * I've recently used RealTerm quite a lot, it can log (store) the data that's coming through on the serial port. Sometimes helps.

    * If you're inserting code, please use the ">>" button in the editor, there you can choose to insert C++ style code. It looks prettier, and reads easier!

     

    Good luck with your project!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • vsluiter
    vsluiter over 12 years ago

    Hello Alex,

    One question, two hints:

    * I thought you would like to use a very low power solution. How are you going to combine that with sending so much data that your computer is getting into trouble?

    * I've recently used RealTerm quite a lot, it can log (store) the data that's coming through on the serial port. Sometimes helps.

    * If you're inserting code, please use the ">>" button in the editor, there you can choose to insert C++ style code. It looks prettier, and reads easier!

     

    Good luck with your project!