Smarter Life
  • Challenges & Projects
  • Design Challenges
  • Smarter Life
  • More
  • Cancel
Smarter Life
Forum Does anybody know if this can be a problem?
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 3 replies
  • Subscribers 4 subscribers
  • Views 915 views
  • Users 0 members are here
  • reflow
  • psoc4
  • smarter_life
  • question
Related

Does anybody know if this can be a problem?

camuyano
camuyano over 12 years ago

I am just starting to work with the PSoC 4. It is very interesting, and feels as a professional device. While running my sample codes I notice two resistors in the board almost touching each other. Wonder what they are for and if this could be a problem latter on. Just know I have only run the Cap+RGB led sample and it is working perfect. So I do not see any problem so far with those resistor touching if it is the case.

Has anybody else seen this situation? Seems like they moved a little while soldering. Included two pictures, one with just the resistors and the other with a green rectangle showing the area.

Comment if anybody knows what those are for.

 

image

image

  • Sign in to reply
  • Cancel

Top Replies

  • ajkahl
    ajkahl over 12 years ago +2
    HI Javier, Looking at the pioneer board schematic R8 and R9 are pullups for the I2C lines. In your case the side where they have pulled together is VDD for both of them, so while it is an assembly fault…
  • camuyano
    camuyano over 12 years ago in reply to ajkahl +1
    Great!, thanks. It is working very good. I am using some UART without any issues.
  • cy.gul
    cy.gul over 12 years ago +1
    Javier, Good catch. Looks like a manufacturing line defect, although in this case it should not impact any functionality since the shorted side is the VDD for the pull-up resistors, as Anthony mentioned…
Parents
  • ajkahl
    ajkahl over 12 years ago

    HI Javier,

     

    Looking at the pioneer board schematic R8 and R9 are pullups for the I2C lines. In your case the side where they have pulled together is VDD for both of them, so while it is an assembly fault it shouldn't cause you any concern.

     

    Anthony

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • ajkahl
    ajkahl over 12 years ago

    HI Javier,

     

    Looking at the pioneer board schematic R8 and R9 are pullups for the I2C lines. In your case the side where they have pulled together is VDD for both of them, so while it is an assembly fault it shouldn't cause you any concern.

     

    Anthony

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • Cancel
Children
  • camuyano
    camuyano over 12 years ago in reply to ajkahl

    Great!, thanks. It is working very good. I am using some UART without any issues.