Sudden Impact Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sudden Impact Wearables Design Challenge
  • More
  • Cancel
Sudden Impact Wearables Design Challenge
Blog Smart Clothes - 1 - Basic structure
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
  • Author Author: konorengineer
  • Date Created: 24 Dec 2014 6:31 PM Date Created
  • Views 673 views
  • Likes 3 likes
  • Comments 2 comments
  • sudden_impact
  • smart_clothes
Related
Recommended

Smart Clothes - 1 - Basic structure

konorengineer
konorengineer
24 Dec 2014

Welcome to in my second blog post!


Now I'm going to write a short summary of the structure of the Smart Clothes Project (SCP). There is a word that will be the keyword of my project in the coming weeks (months) :

H I T

 

What does it mean? This is the abbreviation of the main properties of SCP such as


Health parameters: the ECG, pulse, body temperature and the impact of the head during the downfall will be measured and logged. The factor of dehydration will be an optional feature if my time will allow me. 


Illumination of the cyclist: the visibility is an important quality during the cycling, especially in case of poor visibility. On the clothes sensors will measure the ambient light, and a (Fuzzy) logic will decide about the dress illumination.


Travel parameters: measure the acceleration and determine the speed and the profile of road.

 

image

HIT is going to be a very useful accessory for the afternoon (light) cycling and for the hard bike tour too. HIT is going to be a low cost and light-weight electronic device which is provided by battery. The cycling is an outdoor activity (in most cases), so the communication with computer and/or WiFi connection is not required (and not  the best choice). After that, you might ask, what could be the ideal communication for SCP? I think that the wireless communication is desired, so I chose the Bluetooth communication with Smart Phone (and after the communication is possible through the Internet). 

 

The following factors will be optimized during the design:

  • cost (low as possible)
  • weight (light as possible)
  • physical durability (durable and reliable are the most important parameters)


This means that the Tektronix TDS1202B-EDU Oscilloscope won't be on the bicycle, but it will be a very big help during the design and testing. image


I wish all competitors and readers a Merry Christmas and Happy Holidays!

 

Best regards,

Norbert Kovács


Recommended music for this peaceful time:

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

  • Sign in to reply
Parents
  • DAB
    DAB over 11 years ago

    I can also see your setup used for looking at the body during off road biking.

    I doubt anyone has thought of looking at how much damage you subject yourself to during such adventures.

    You can do some baseline measurements on good bike paths and then compare them to your other biking activities.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 11 years ago

    I can also see your setup used for looking at the body during off road biking.

    I doubt anyone has thought of looking at how much damage you subject yourself to during such adventures.

    You can do some baseline measurements on good bike paths and then compare them to your other biking activities.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • konorengineer
    konorengineer over 11 years ago in reply to DAB

    Yes, you are right: in the normal situation the ECG and other measuring methods are unnecessary. But the purpose of this Design Challenge is to prepare for the unforeseen events (bike crash, car crash, heart attack etc.).

     

    The SCP consists of PIE:

    • Prevention: the illumination reduces the probability of road accidents.
    • Information: to inform of road parameters.
    • Emergency: to inform of health parameters in critical situations.

     

    Well, this is the Hungarian PIE and I hope it is going to be tasty. image

     

    Norbert