Sudden Impact Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sudden Impact Wearables Design Challenge
  • More
  • Cancel
Sudden Impact Wearables Design Challenge
Forum Have a Question About the Sudden Impact Design Challenge? Ask it here!
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 115 replies
  • Subscribers 14 subscribers
  • Views 10847 views
  • Users 0 members are here
  • design_challenge
  • element14
  • leeds_beckett
  • tektronix
  • sudden_impact
  • element14_design_challenge
  • analog_devices
  • electrolube
Related

Have a Question About the Sudden Impact Design Challenge? Ask it here!

doctorcdf
doctorcdf over 11 years ago

Please direct any questions about the Sudden Impact design challenge to this discussion thread.

  • Sign in to reply
  • Cancel

Top Replies

  • Robert Peter Oakes
    Robert Peter Oakes over 11 years ago in reply to hawkeyethehacker +3
    Post what you have, that is better than nothing. No one expects everyone to get all they set out to do completed, we all have different skill levels and time available, I did not get every single thing…
  • doctorcdf
    doctorcdf over 11 years ago +3
    Good morning - In light of recent events, we have adjusted the following terms of the competition - The final submission date is Friday, May 8th, 2015 . We expect a minimum of 6 blog posts about each project…
  • kas.lewis
    kas.lewis over 11 years ago in reply to hawkeyethehacker +2
    Hopefully, I was starting to give up on the kit and was just going to do my own implementation using TI parts and ADI sensors that I already have. Hopefully that won't be necessary. For now though I am…
Parents
  • hawkeyethehacker
    0 hawkeyethehacker over 11 years ago

    Although this is not directly related to the project, it IS related to how the stuff connects.

    I noticed the AD8232 input does not have a SPI or I2C input/output. May I ask how one would receive the output from that eval board and wirelessly send the data?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • sunnyiut
    0 sunnyiut over 11 years ago in reply to hawkeyethehacker

    Hello Joshua, sorry may be i'm late to reply and u've already figured it out all the way. but still replying as i hope it may help u or others somehow.

    I'm not an expert and have never worked with this chip [AD8232] but it seems to be a beauty to me.

    AD8232 EVALZ has an analog output [TP15] which can be directly connected to a microcontroller's built in ADC. and obviously u can use an arduino. as the ECG has frequency components of 1Hz to 100Hz, simple 10bit low speed ADC is good enough to capture it. most interesting part is the board uses single supply and the output is already level shifted [not sure - i hope so], so the signal will stay in between 0 - 3v.

    AD8232 has built in opamp to imply low pass filter. They have built in configuration. but if u want u can utilize it in ur way through TP16, TP17. u may need some collection of SMD resistors and capacitors, as i see the board has lots of unused pads to provide flexibility to the user.

    the internal instrumentation amp has option to imply high pass filter to avoid motion and unnecessary signals due to displacements of electrodes. however, it has internal circuitry to detect if the electrodes are fully displaced [TP12, TP13]. but u have to buy electrodes or design wearable electrodes if u want to use it on the body surface of the athlete while performing [creepy].

    TP14 [fast restore] can be used to control the 'amplifier rail on' to stabilize the output for quick recovery after an abnormal signal [like lead-off].

    TP18 -> gives an option for DC LEADs off detection and TP21 can be used to shut the chip down.

    the RLD [right leg drive] will definitely help in noisy environment.

    however, may be I am not right with all the above stuffs. if anyone finds anything wrong please reply back to let me know.

    I loved this chip - except one limitation -> it has inputs for only two electrodes, means u can get only one lead combination at a time [LEAD I, LEAD II, LEAD III]. in my experience, i have seen most people having good signals [high QRS complex] for LEAD I, but few people has low LEAD I and LEAD II, but high LEAD III. so if he does not get good signals from one combination then he has to switch the electrodes manually for different combination. Now in a game running on, u cannot do that, right? and the device may show that u are struggling or something is wrong with the device :-p

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Reply
  • sunnyiut
    0 sunnyiut over 11 years ago in reply to hawkeyethehacker

    Hello Joshua, sorry may be i'm late to reply and u've already figured it out all the way. but still replying as i hope it may help u or others somehow.

    I'm not an expert and have never worked with this chip [AD8232] but it seems to be a beauty to me.

    AD8232 EVALZ has an analog output [TP15] which can be directly connected to a microcontroller's built in ADC. and obviously u can use an arduino. as the ECG has frequency components of 1Hz to 100Hz, simple 10bit low speed ADC is good enough to capture it. most interesting part is the board uses single supply and the output is already level shifted [not sure - i hope so], so the signal will stay in between 0 - 3v.

    AD8232 has built in opamp to imply low pass filter. They have built in configuration. but if u want u can utilize it in ur way through TP16, TP17. u may need some collection of SMD resistors and capacitors, as i see the board has lots of unused pads to provide flexibility to the user.

    the internal instrumentation amp has option to imply high pass filter to avoid motion and unnecessary signals due to displacements of electrodes. however, it has internal circuitry to detect if the electrodes are fully displaced [TP12, TP13]. but u have to buy electrodes or design wearable electrodes if u want to use it on the body surface of the athlete while performing [creepy].

    TP14 [fast restore] can be used to control the 'amplifier rail on' to stabilize the output for quick recovery after an abnormal signal [like lead-off].

    TP18 -> gives an option for DC LEADs off detection and TP21 can be used to shut the chip down.

    the RLD [right leg drive] will definitely help in noisy environment.

    however, may be I am not right with all the above stuffs. if anyone finds anything wrong please reply back to let me know.

    I loved this chip - except one limitation -> it has inputs for only two electrodes, means u can get only one lead combination at a time [LEAD I, LEAD II, LEAD III]. in my experience, i have seen most people having good signals [high QRS complex] for LEAD I, but few people has low LEAD I and LEAD II, but high LEAD III. so if he does not get good signals from one combination then he has to switch the electrodes manually for different combination. Now in a game running on, u cannot do that, right? and the device may show that u are struggling or something is wrong with the device :-p

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
Children
  • hawkeyethehacker
    0 hawkeyethehacker over 11 years ago in reply to sunnyiut

    These are all great points and I thank you for your input. I am editing my application accordingly image