Sudden Impact Wearables Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sudden Impact Wearables Design Challenge
  • More
  • Cancel
Sudden Impact Wearables Design Challenge
Documents Sudden Impact Wearables Design Challenge Competitors
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: doctorcdf
  • Date Created: 26 Nov 2014 8:20 AM Date Created
  • Last Updated Last Updated: 4 Sep 2015 6:17 PM
  • Views 1612 views
  • Likes 3 likes
  • Comments 6 comments
Related
Recommended

Sudden Impact Wearables Design Challenge Competitors

image
Sudden Impact Wearables Design Challenge

image  About this Challenge

image  Terms and Conditions

 

Joshua Bayfield | Ravi Butani | Shubham Garg | Austin Horning | Md. Kamrul Hussain | Cosmin Iorga | Dragan Knezevic |  Norbert Kovács | Kas Lewis | Hendrik Lipka | Robert Waters | Douglas Wong

imageJoshua Bayfield
United Kingdom
Project: Field Hockey Safety Monitor
Synopsis:

As someone who attends a public school, there are teams composed of all ages for many sports. After consulting with my school's Physical Education department, I have decided to cover Field Hockey.

Read Joshua's project blogs (tag safe_field_hockey)

imageRavi Butani
India
Project: Real Time Player Monitoring System
Synopsis:

Designing of low cost and battery powered wearable sensor module to stream and monitor, vital body parameters of sport person on Android/IoS Smartphone and MacOS/Windows/Linux PC using WiFi or on MacOS/Windows/Linux PC using long range Sub GHz transceiver at monitoring station.

Read Ravi's project blogs (tag real_time_monitor)

imageShubham Garg
India
Project: Universal Wearable Health Monitoring Device for Athletes
Synopsis:

Runners have some exciting smart watches, cyclist have computer providing their vital parameters. So, the big question is why this sort of things are not available to sports person. So, here I propose a device which will be remotely monitoring sports performance whether it is football or skiing or any other sports.

Read Shubham's project blogs (tag universal_wearable)

imageAustin Horning
United States
Project: Real Time Data for Coaches
Synopsis:

I have had a number of friends sustain serious injuries while playing high school and other youth sports, so this challenge is very relatable to me. Concussions are very serious injuries and must be treated as such, but they are not always noticeable, and some players continue to play after sustaining a concussion or other serious injury. The obvious solution is that provided in the premise of this challenge, to create a system of notification so that a coach could see real time data regarding the forces and hits that players are subjected to, as well as other vital signs to make sure that the players playing are healthy enough to play.

Read Austin's project blogs (tag real_time_coach)

imageMd. Kamrul Hussain
Bangladesh
Project: Total Player Monitoring
Synopsis:

My focus will be mainly on the sectors those I have experience to deal with before, like ECG, SPO2, Impedance measurement and EMG. But as well as these, I would like to work on a few other options which may need some basic research works too, like respiratory rate and hydration.

Read Md. Kamrul's project blogs (tag total_player)

imageCosmin Iorga
United States
Project: Wearable Sudden Impact and Health Monitor
Synopsis:

My project will be made of two types of units, as described below:

  1. One centralized receiver unit for coach/supervisor with data processing and visual display of each player’s health information and health alarms on the screen of a tablet computer or smart phone.
  2. Multiple wearable health monitor units with health condition alarm for athletes/players, which transmit the data through wireless connections to the centralized receiver
Read Cosmin's project blogs (tag wearable_sudden)

imageDragan Knezevic
Serbia
Project: Easily Configurable Wearable Sensors
Synopsis:

My conclusion was that it might be a good idea to make a generic system that will be easy to configure for some specific application on the field instead of making it specific for some sport.

Read Dragan's project blogs (tag easy_configure)

imageNorbert Kovács
Hungary
Project: Smart Clothes
Synopsis:

I would like to create a "smart clothes" which can log the health parameters (eg. heart rate, temperature etc) and cycling conditions (eg. acceleration, speed, profile of the trip etc.). If a bicyclist is exposed to visible by clothing, the risk of road accidents can be reduced. The bluetooth connection will be desirable to keep in touch between the dress and the person (via smart phone).

Read Norbert's project blogs (tag smart_clothes)

imageKas Lewis
Canada
Project: Improved Sports Helmet
Synopsis:
A sports helmet that monitors an athlete's body temperature, heart rate and rhythm as well as head trauma would be implemented to read and transmit these measurements back to a command post. There would be the possibility of adding an oxygen sensor by the athlete's mouth or nose to monitor their O2 intake.
The health related issues I would like to tackle with this setup is the immediate health risks an athlete may face while involved in the sport. These health risks would include heat stroke, sudden heart attack and seriousness of individual concussion as well as long term cumulative concussion force sustained by the athlete.
These risks will each be monitored by an individual or group of sensors.
Read Kas's project blogs (tag sports_helmet)

imageHendrik Lipka
Germany
Project: Impact Monitor for Skiers
Synopsis:

My proposal is to implement an impact monitor for skiers. Its purpose is to monitor and log the accelerations that affect the skier. When my son is on a ski run, I want to see afterwards (maybe at the end of the day) a nice graph of how much G's he had to cope with. If the acceleration exceeds a certain threshold, I want to get an instant notification on my phone (as long as I'm in range).  The device should be mounted to the ski helmet. It must be small enough not to disturb normal handling, and it also must not affect the helmet in case of an accident.

Read Hendrik's project blogs (tag impact_skiers)

imageRobert Waters
United States
Project: Team Heart Monitor
Synopsis:

I realized that we wear heart monitors while working out but then do not use them during sporting events.  I also realized that sports teams would spring for these items as it would give them a competitive advantage knowing how fast the players were wearing out.

Read Robert's project blogs (tag team_heart_monitor)

imageDouglas Wong
Canada
Project: Concussions & Stress Monitor
Synopsis:

I would like to split the project into 2 separate systems, 1 to monitor events that might cause mild traumatic brain injuries and one to monitor physiological stress. The reasons for the split are that the sensors need to be in very different places on the body and the function is completely different. It is also highly undesirable to have wires running around the body as most people will feel this is unacceptable.

Read Doug's project blogs (tag concussion_stress)
  • competitors
  • Design
  • challenge
  • Wearables
  • impact
  • sudden
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • fvan
    fvan over 11 years ago +2
    Completely missed the announcement ... Good luck everyone (especially to those combining multiple challenges ) ! Frederick
Parents
  • michaelwylie
    michaelwylie over 11 years ago

    Looks like a good mix of projects. There is some overlap, but I think that will spark some creativity in implementation. Looking forward to seeing the projects unfold.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • michaelwylie
    michaelwylie over 11 years ago

    Looks like a good mix of projects. There is some overlap, but I think that will spark some creativity in implementation. Looking forward to seeing the projects unfold.