Summer of Green Tech Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Summer of Green Tech Design Challenge
  • More
  • Cancel
Summer of Green Tech Design Challenge
Blog Smart Home Energy Management System - Blog Post #5 - OpenWeather API
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Summer of Green Tech Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: MarioPJ98
  • Date Created: 13 Oct 2023 2:50 PM Date Created
  • Views 511 views
  • Likes 6 likes
  • Comments 0 comments
  • seeeduino xiao
  • expansion board
  • competition
  • design challenge
  • summer of green tech design challenge
  • seeedstudio
  • green
  • challengers
  • json
  • green tech
  • Xiao
  • samd21
  • http
  • api
  • arduino
  • Nicla Vision Board
  • seeeduino
Related
Recommended

Smart Home Energy Management System - Blog Post #5 - OpenWeather API

MarioPJ98
MarioPJ98
13 Oct 2023
Smart Home Energy Management System - Blog Post #5 - OpenWeather API

As I mentioned in my previous blogs, I will be using an API to get the weather information. Specifically, I have used this tutorial.

ESP32 HTTP GET with Arduino IDE (OpenWeatherMap.org and ThingSpeak) | Random Nerd Tutorials

This tutorial is specifically for ESP32. I have tried first to run it with the Nicla Vision board and some libraries were not included/compatible for the Nicla Vision. Fortunately, I have a Huzzah32 feather board that I have used for a different project (link below).

 PiBCI - Project Proposal 

I had some experience with JSON files so modifying the code from the tutorial was pretty straightforward. The OpenWeather API offers many information about the weather. For this demonstration I decided to just use min and max temperature, feels like and the weather in general. I don't think I will display the weather on the screen of the Expansion Board but rather an image from the Github library. I had to convert the temperature because it was in Kelvin and I use Celsius (no Fahrenheit here). Below you can see my edited code.

/*
  Rui Santos
  Complete project details at Complete project details at https://RandomNerdTutorials.com/esp32-http-get-open-weather-map-thingspeak-arduino/

  Permission is hereby granted, free of charge, to any person obtaining a copy
  of this software and associated documentation files.

  The above copyright notice and this permission notice shall be included in all
  copies or substantial portions of the Software.
*/

#include <WiFi.h>
#include <HTTPClient.h>
#include <Arduino_JSON.h>

const char* ssid = "Your WiFi";
const char* password = "Your WiFi's Password";

// Your Domain name with URL path or IP address with path
String openWeatherMapApiKey = "Your OpenWeather API string for your page";
// Example:
//String openWeatherMapApiKey = "bd939aa3d23ff33d3c8f5dd1dd435";

// Replace with your country code and city
String city = "Your City";
String countryCode = "Your Country Code";

// THE DEFAULT TIMER IS SET TO 10 SECONDS FOR TESTING PURPOSES
// For a final application, check the API call limits per hour/minute to avoid getting blocked/banned
unsigned long lastTime = 0;
// Timer set to 10 minutes (600000)
//unsigned long timerDelay = 600000;
// Set timer to 10 seconds (10000)
unsigned long timerDelay = 10000;

String jsonBuffer;

void setup() {
  Serial.begin(115200);

  WiFi.begin(ssid, password);
  Serial.println("Connecting");
  while(WiFi.status() != WL_CONNECTED) {
    delay(500);
    Serial.print(".");
  }
  Serial.println("");
  Serial.print("Connected to WiFi network with IP Address: ");
  Serial.println(WiFi.localIP());
 
  Serial.println("Timer set to 10 seconds (timerDelay variable), it will take 10 seconds before publishing the first reading.");
}

void loop() {
  // Send an HTTP GET request
  if ((millis() - lastTime) > timerDelay) {
    // Check WiFi connection status
    if(WiFi.status()== WL_CONNECTED){
      String serverPath = "http://api.openweathermap.org/data/2.5/weather?q=" + city + "," + countryCode + "&APPID=" + openWeatherMapApiKey;
      
      jsonBuffer = httpGETRequest(serverPath.c_str());
      //Serial.println(jsonBuffer);
      JSONVar myObject = JSON.parse(jsonBuffer);
  
      // JSON.typeof(jsonVar) can be used to get the type of the var
      if (JSON.typeof(myObject) == "undefined") {
        Serial.println("Parsing input failed!");
        return;
      }
    
      //Serial.print("JSON object = ");
      //Serial.println(myObject);
      Serial.print("Temperature max: ");
      double max_temp = myObject["main"]["temp_max"];
      Serial.println(max_temp - 273.15);
      Serial.print("Temperature min: ");
      double min_temp = myObject["main"]["temp_min"];
      Serial.println(min_temp - 273.15);
      Serial.print("Feels like: ");
      double feels = myObject["main"]["feels_like"];
      Serial.println(feels - 273.15);
      Serial.print("Weather: ");
      Serial.println(myObject["weather"][0]["description"]);
    }
    else {
      Serial.println("WiFi Disconnected");
    }
    lastTime = millis();
  }
}

String httpGETRequest(const char* serverName) {
  WiFiClient client;
  HTTPClient http;
    
  // Your Domain name with URL path or IP address with path
  http.begin(client, serverName);
  
  // Send HTTP POST request
  int httpResponseCode = http.GET();
  
  String payload = "{}"; 
  
  if (httpResponseCode>0) {
    //Serial.print("HTTP Response code: ");
    //Serial.println(httpResponseCode);
    payload = http.getString();
  }
  else {
    Serial.print("Error code: ");
    Serial.println(httpResponseCode);
  }
  // Free resources
  http.end();

  return payload;
}

You can see below a video of the Huzzah32 that sends HTTP request to OpenWeather, read some data, and then print it on the Serial Monitor after some basic manipulation.

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

For next steps, I will need to connect via UART the Huzzah32 to either the Nicla Vision board or the Seeeduino XIAO. Having three board increases the complexity of the project and I am not sure if I can connect the three boards for communication. I am still looking for way to use just the Nicla Vision to access the API.