Summer of Green Tech Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Summer of Green Tech Design Challenge
  • More
  • Cancel
Summer of Green Tech Design Challenge
Forum Has anyone used the OneWire protocol with the Seeeduino XIAO under MicroPython?
  • Blog
  • Forum
  • Documents
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Summer of Green Tech Design Challenge to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • State Not Answered
  • Replies 5 replies
  • Subscribers 68 subscribers
  • Views 1817 views
  • Users 0 members are here
Related

Has anyone used the OneWire protocol with the Seeeduino XIAO under MicroPython?

Alistair
Alistair over 3 years ago

I am trying to use the OneWire protocol to talk to a DS18B20, but I don't think it is currently compiled in to MicroPython for SAMD21 based devices.

Am I correct? If so are there any recommended alternative libraries. If not then any thought as to what I am doing wrong?

  • Sign in to reply
  • Cancel

Top Replies

  • Alistair
    Alistair over 3 years ago in reply to scottiebabe +1
    That is the command I was needed. Thanks. Yes, it confirms that onewire is not compiled in for some reason. It is documented as it should be, so perhaps I should try and nightly build and see what I get…
  • shabaz
    0 shabaz over 3 years ago

    I've not used any of the boards/protocols you mention. However, MicroPython allows for general GPIO manipulation, and I believe 1-wire is slow enough that you could manually bit-bang your protocol if needed. That's what the author of this library has done:

    https://github.com/robert-hh/Onewire_DS18X20

    That library should work (or could be edited, since it is entirely in Python, manually bit-banging - no compiling needed).

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • scottiebabe
    0 scottiebabe over 3 years ago

    Can you post what you see when you type help('modules') into the REPL

    image

    (Pico example)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Alistair
    0 Alistair over 3 years ago in reply to shabaz

    Thanks for the the link. Following the same logic I found the same library, but sadly it is not detecting the sensor. I checked the wiring by connecting to an Arduino for a test and it worked, so I suspect it is an oddity around the XIAO and Micropython in some way. Perhaps it is timing as that feels critical and relying on quick execution looking at the code. I might connect it up to the scope to see what is actually happening at the hardware end and see it that gives me a clue. Thanks for the pointer though. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • Alistair
    0 Alistair over 3 years ago in reply to scottiebabe

    That is the command I was needed. Thanks. Yes, it confirms that onewire is not compiled in for some reason. It is documented as it should be, so perhaps I should try and nightly build and see what I get. 

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Verify Answer
    • Cancel
  • shabaz
    0 shabaz over 3 years ago in reply to Alistair

    There are sleep_us() operations in the code, it's very likely they may need tweaking (checking with an oscilloscope), since the timings won't be too accurate in that way at the microsecond level with MicroPython.

    I2C is a better protocol for on-board sensors (appreciate that doesn't help with the immediate problem, but for future use).