Summer of Sensors Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Summer of Sensors Design Challenge
  • More
  • Cancel
Summer of Sensors Design Challenge
Blog Blog Two– In the Air Tonight, unboxing, connecting and first try outs
  • Blog
  • Forum
  • Documents
  • DesignChallenge
  • Leaderboard
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Summer of Sensors Design Challenge to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: christophesky
  • Date Created: 14 Nov 2022 10:52 AM Date Created
  • Views 709 views
  • Likes 9 likes
  • Comments 0 comments
  • zmod4510-evk
  • HS4000-EVK
  • Summer of Sensors Design Challenge
  • In the Air Tonight
Related
Recommended

Blog Two– In the Air Tonight, unboxing, connecting and first try outs

christophesky
christophesky
14 Nov 2022
Blog Two– In the Air Tonight, unboxing, connecting and first try outs

The project so far:

 Blog One – In the Air Tonight Project Start 

 Blog Two– In the Air Tonight, unboxing, connecting and first try outs  <-- this blog

Coming: blog 3 - design, parameters and a plan

Coming : blog four - the build

Coming : blog 5 - extending and stretch objectives



In this blog I cover the unboxing and use of the sponsored kit provided. All resources for the sponsored kit are given on this page, where there are resources whcih are provided under EULA / other agreement (i.e. you have to request access, links are given instead), so lets get on with it

Arrival and Unboxing

imageimageimage

I do love a parcel from the fine folks at E14, not only for what is in the box, but the packaging. All recyclable.

One small box, containing two smaller boxes and some packing paper.

 

image 

Our two smaller boxed from Renesas, thank you! The HS4000 developer kit - this is for temp and relative humidity and the ZMOD4510 developer kit for outbdoor air quality.

image

Starting with the HS4000 dev evaluation board (for the HS4001)

image   image

Inside we have the host board (left) the sensor board (right), USB stick (with software) and then USB cable for PC connection.

  image  image  image

Quick uh-oh moment. My antivirus did not like the software which came on the USB and subsequently quarantined it.

image

Over to virustotalm submit the sample and ..image

and ...

image

Only one detection, static AI, heh. CLean on everything else (or at least not detected) So installed, and watcher left on. I have since removed the watcher and happy that there is nothing untowards going on.

Hopefully this is helpul for someone else, just in case you too get to have an Oh NO moment.

The USB has:

image

Simple install, took a few minutes.

image

Load up the demo application, temp and humidity

image

Connect up the sensor and leave it running for a while.

image

Initial thoughts:

- how small is that sensor!

From the evaluation kit, you can export the data as a CSV. 3 decimal place level of precision for Temp and Relative Humdity.

Date Time Temperature [C]  Relative Humidity [%]
24/09/2022 13:42:49 20.016 53.128
24/09/2022 13:42:50 20.036 53.165
24/09/2022 13:42:50 19.985 53.024
24/09/2022 13:42:51 20.036 53.055
24/09/2022 13:42:51 20.016 52.762
24/09/2022 13:42:52 20.005 52.64
24/09/2022 13:42:53 19.985 52.554
24/09/2022 13:42:53 20.016 52.53
24/09/2022 13:42:54 19.985 52.5
24/09/2022 13:42:54 19.995 52.426
24/09/2022 13:42:55 19.965 52.457

image

image

Look at how small that is. What is this? a sensor for ants?

You will see that the interconnect breaks out 4 contacts ... however the sensor has more than four Disappointed

Moving on, what is in the second box?

image    image    

image

Inside the sleeved outer, the box contains the carrier board, sensor board and USB cable for connecting to your PC.

It comes with bonus data sheets / notices shown, but no software?

Link for the sensor: https://www.renesas.com/eu/en/products/sensor-products/environmental-sensors/digital-gas-sensors/zmod4510-outdoor-air-quality-sensor-platform

from here you can see documentation, code samples and sample application

Once up and connected and a lot of faff on the FTDI driver (to not break other things) you can then use the demo application.

as with the previous temp and humidity HS 4001, you can also download your data as a file / save to file:

start_time run device_tracking making_code generalpurpose AQI Rmox_00 Rmox_01 Rmox_02 Rmox_10 Rmox_11 Rmox_12 Rmox_20 Rmox_21 Rmox_22 Rmox_30 Rmox_31 Rmox_32 Rmox_40 Rmox_41 Rmox_42 VDDH comment sleeptime (s)
2022-09-24T14:07:25.411825 1 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 218006.4 270799 329231.3 237584.2 289380.2 337543.6 228218.8 259302.3 295063.9 182618.6 211154.1 241460.7 143074.9 171853.4 203576.6 2.106251 0
2022-09-24T14:08:25.841026 2 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 741091.2 890767.4 1069265 702197.4 815018 945245.9 599564.5 619470.2 667810.5 387992.4 400536.3 431132.6 239587.6 257631.6 285429.9 2.106251 0
2022-09-24T14:09:26.180092 3 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 1166168 1438910 1802828 1140365 1346014 1566034 954689.6 940581.3 1011474 568815.2 560414.3 594842.5 320118.2 331719.6 358197.2 2.106251 0
2022-09-24T14:10:26.574429 4 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 1478277 1803823 2264535 1410303 1665444 1924423 1173946 1170201 1266777 698348.3 700843.1 741238.7 390617.7 399870.9 425470.8 2.106251 0
2022-09-24T14:11:26.915410 5 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 1922561 2258536 2904976 1806480 2235318 2684959 1578500 1539112 1626851 888006.2 854812.6 921458.5 471217.8 470765.3 496910 2.106251 0
2022-09-24T14:12:27.349567 6 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 2198211 2723194 3470107 2085573 2523647 3000792 1735258 1666019 1799520 983973 978068 1055649 527048.5 523222.8 556999.3 2.106251 0.01
2022-09-24T14:13:27.734640 7 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 2627793 3332375 4219147 2529164 3027176 3586840 2075698 2019819 2225570 1181971 1139769 1226734 604180.5 591533.2 623298.3 2.106251 0
2022-09-24T14:14:28.117960 8 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 2955846 3643161 4813432 2851873 3451346 4132483 2347938 2353304 2574746 1352571 1286459 1393106 680614.4 659909.1 699965 2.106251 0
2022-09-24T14:15:18.822128 9 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 3491304 4463348 5955593 3489061 4354979 5281343 2933033 2784315 2957488 1523250 1427215 1541868 750399.4 723575.5 773660.4 2.106251 0
2022-09-24T14:16:19.169147 10 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 4002119 5394842 7239310 4185652 5264099 6371310 3493549 3317027 3598685 1793264 1657995 1767985 838331.4 800905.5 841388.1 2.106251 0
2022-09-24T14:17:19.546156 11 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 4360107 5681700 7435388 4245012 5148716 6424996 3572724 3494673 3720065 1883483 1762242 1883483 904075.5 863954.9 907325.7 2.106251 0
2022-09-24T14:18:19.931679 12 x0000400DE4A830B2 x6320 [209, 157, 139, 113, 73, 73, 85, 118, 1, 0, 0, 0, 0, 0, 0, 0, 0, 0] 0 4770382 6228908 8136333 4730063 6308024 7968459 4209525 3904167 4162035 2072710 1913301 2051171 977262 925652.8 971879 2.106251 0

I do very much like the look of: https://www.renesas.com/eu/en/application/industrial/building-home-automation/quick-connect-iot#overview

image

But wonder if they might be outside of my tinkering budget!