Sustain The World - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sustain The World - Design Challenge
  • More
  • Cancel
Sustain The World - Design Challenge
Blog Blog8# Program to control the Motors to specific time.
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
  • Author Author: karthickiot
  • Date Created: 28 Oct 2020 4:35 PM Date Created
  • Views 919 views
  • Likes 1 like
  • Comments 1 comment
  • water motor control
  • software
Related
Recommended

Blog8# Program to control the Motors to specific time.

karthickiot
karthickiot
28 Oct 2020

The software program is important to control the watering system to water the plants in different pots with different water quantity.

 

#include <SPI.h>

const int EN = 8;                       // Set pin 8 to control Enable pin of TLE94112
const int CSN = 10;                     // Set pin 10 (CSN1) to control CSN of TLE94112 (default)

// Addresses of the control registers
const byte HB_ACT_1_CTRL = B0000011;    // Activation/deactivation of  HB1-4
const byte HB_ACT_2_CTRL = B1000011;    // Activation/deactivation of  HB5-8
const byte HB_ACT_3_CTRL = B0100011;    // Activation/deactivation of  HB9-12
const byte HB_MODE_1_CTRL = B1100011;   // Control mode (PWM enable, PWM channel) of HB1-4
const byte HB_MODE_2_CTRL = B0010011;   // Control mode (PWM enable, PWM channel) of HB5-8
const byte HB_MODE_3_CTRL = B1010011;   // Control mode (PWM enable, PWM channel) of HB9-12
const byte PWM_CH_FREQ_CTRL = B0110011; // PWM clock frequency and frequency modulation of the oscillator
const byte PWM1_DC_CTRL = B1110011;     // Duty cycle of PWM Channel 1
const byte PWM2_DC_CTRL = B0001011;     // Duty cycle of PWM Channel 2
const byte PWM3_DC_CTRL = B1001011;     // Duty cycle of PWM Channel 3
const byte FW_OL_CTRL = B0101011;       // LED mode for HS1/2 and active free-wheeling of HB1-6
const byte FW_CTRL = B1101011;          // Active free-wheeling of HB7-12
const byte CONFIG_CTRL = B1100111;      // Device ID

// Address of the status registers
const byte SYS_DIAG_1 = B00011011;      // Global Status Register
const byte SYS_DIAG_2 = B01011011;      // Overcurrent HB1-4
const byte SYS_DIAG_3 = B00111011;      // Overcurrent HB5-8
const byte SYS_DIAG_4 = B01111011;      // Overcurrent HB9-12
const byte SYS_DIAG_5 = B00000111;      // Open load HB1-4
const byte SYS_DIAG_6 = B01000111;      // Open load HB5-8
const byte SYS_DIAG_7 = B00100111;      // Open load HB9-12

const byte WRITE = 0b10000000; // Mask for write commands to control registers
const byte CLEAR = 0b10000000; // Mask for clear commands to status registers

void setup() {
  // Setup fo the parameters for SPI communication, set CSN and EN pins as outputs and set EN to High  
  Serial.begin(9600);                     // sets the baud rate for communication with the computer to 9600 bauds
  SPI.begin();                            // Initializes the SPI bus
  SPI.setBitOrder(LSBFIRST);              // Least significant bit is sent first 
  SPI.setClockDivider(SPI_CLOCK_DIV16);   // SPI clock frequency set to 1 MHz
  SPI.setDataMode(SPI_MODE1);             // Set SPI clock polarity and clock phase; CPOL = 0, CPHA = 1
  pinMode(CSN, OUTPUT);                   // sets CSN as output
  pinMode(EN, OUTPUT);                    // sets EN as output
  digitalWrite(EN, HIGH);                 // TLE94112 set in active mode (ENABLE pin = high)
}

void loop()
{
 activateMotor1_PWM(); 
 activateMotor2_PWM();                
 activateMotor3_PWM(); 
 activateMotor4_PWM(); 
}

void activateMotor1_PWM()
{
    writeRegister(HB_MODE_1_CTRL,0b1);      // Map HB1 to PWM channel 1
    writeRegister(PWM_CH_FREQ_CTRL,0b10);   // Set Frequency of PWM channel 1 to 100 Hz
    writeRegister(PWM1_DC_CTRL,0b11100110); // Set duty cycle of PWM channel to 90 %
    writeRegister(HB_ACT_1_CTRL,0b0110);    // Activate HS1/LS2
    delay(20000);                            // Wait 20000 ms
    writeRegister(PWM1_DC_CTRL,0b00110011); // Set duty cycle of PWM channel to 20 %
    delay(1000);                            // Wait 2000 ms
    writeRegister(HB_ACT_1_CTRL,0b0101);    // Activate LS1/LS2
    delay(300);                             // Wait 300 ms
    
    writeRegister(HB_MODE_1_CTRL,0b0);      // HB1 is not mapped to PWM channel 1
  }


void activateMotor2_PWM()
{ 
    writeRegister(HB_MODE_1_CTRL,0b1);      // Map HB1 to PWM channel 1
    writeRegister(PWM_CH_FREQ_CTRL,0b10);   // Set Frequency of PWM channel 1 to 100 Hz
    writeRegister(PWM1_DC_CTRL,0b11100110); // Set duty cycle of PWM channel to 90 %
    writeRegister(HB_ACT_1_CTRL,0b0110);    // Activate HS1/LS2
    delay(20000);                            // Wait 20000 ms
    writeRegister(PWM1_DC_CTRL,0b00110011); // Set duty cycle of PWM channel to 20 %
    delay(1000);                            // Wait 2000 ms
    writeRegister(HB_ACT_1_CTRL,0b0101);    // Activate LS1/LS2
    delay(300);                             // Wait 300 ms
    writeRegister(HB_MODE_1_CTRL,0b0);      // HB1 is not mapped to PWM channel 1
  }

void activateMotor3_PWM()
{
    writeRegister(HB_MODE_3_CTRL,0b1);      // Map HB1 to PWM channel 3
    writeRegister(PWM_CH_FREQ_CTRL,0b10);   // Set Frequency of PWM channel 1 to 100 Hz
    writeRegister(PWM1_DC_CTRL,0b11100110); // Set duty cycle of PWM channel to 90 %
    writeRegister(HB_ACT_3_CTRL,0b0110);    // Activate HS1/LS2
    delay(20000);                            // Wait 20000 ms
    writeRegister(PWM1_DC_CTRL,0b00110011); // Set duty cycle of PWM channel to 20 %
    delay(1000);                            // Wait 2000 ms
    writeRegister(HB_ACT_3_CTRL,0b0101);    // Activate LS1/LS2
    delay(300);                             // Wait 300 ms
    
    writeRegister(HB_MODE_3_CTRL,0b0);      // HB1 is not mapped to PWM channel 3
  }


void activateMotor4_PWM()
{
     writeRegister(HB_MODE_3_CTRL,0b1);      // Map HB1 to PWM channel 3
    writeRegister(PWM_CH_FREQ_CTRL,0b10);   // Set Frequency of PWM channel 1 to 100 Hz
    writeRegister(PWM1_DC_CTRL,0b11100110); // Set duty cycle of PWM channel to 90 %
    writeRegister(HB_ACT_3_CTRL,0b0110);    // Activate HS1/LS2
    delay(20000);                            // Wait 20000 ms
    writeRegister(PWM1_DC_CTRL,0b00110011); // Set duty cycle of PWM channel to 20 %
    delay(1000);                            // Wait 2000 ms
    writeRegister(HB_ACT_3_CTRL,0b0101);    // Activate LS1/LS2
    delay(300);                             // Wait 300 ms
    
    writeRegister(HB_MODE_3_CTRL,0b0);      // HB1 is not mapped to PWM channel 3
  }

int writeRegister(byte address, byte data)
{
/*   This function sends SPI commands to the address  "address" with the data "data"
 *   The data sent by the TLE94112EL to the Arduino Uno (SDO) and the data sent by the Arduino Uno to the TLE94112EL (SDI) are reported in the
 *   Serial Monitor (CTRL + SHIFT + M)
 */
  address = address | WRITE ;
  digitalWrite(CSN, LOW);               // take the CSN pin low to select the chip:
  byte byte0 = SPI.transfer(address);   // send address byte to the TLE94112 and store the received byte to byte 0
  byte byte1 = SPI.transfer(data);      // send data byte to the TLE94112 and store the received byte to byte 1
  digitalWrite(CSN, HIGH);              // take the CSN pin high to terminate the SPI frame
  Serial.println();                     // insert a carriage return to the serial monitor

  Serial.print("SDI:\t");
  printByte(address);                   // write address to the serial monitor
  printByte(data);                      // write data to the serial monitor
  Serial.print("SDO:\t");
  printByte(byte0);                     // write byte0 (Global Satus Register of the TLE94112EL) to the serial monitor
  printByte(byte1);                     // write byte1 (Data Byte sent by the TLE9412EL) to the serial monitor
  int result = ( ((int)byte0 << 8) | (int)byte1 ); // concatenates byte0 and byte1 in result
  return (result);
}

int readRegister(byte address)          // This function reads a register and returns the data sent by the TLE94112EL. Data sent and received by the TLE94112EL are displayed on the serial monitor
{
  digitalWrite(CSN, LOW);               // take the CSN pin low to select the chip:
  byte byte0 = SPI.transfer(address);   // send Low Byte
  byte byte1 = SPI.transfer(0);         // send High Byte
  digitalWrite(CSN, HIGH);              // take the CSN pin high to de-select the chip:
  Serial.println();
  
  Serial.print("SDI:\t");
  printByte(address);                   // write address to the serial monitor
  printByte(0);                         // write data to the serial monitor
  Serial.print("SDO:\t");
  printByte(byte0);                     // write byte0 (Global Satus Register of the TLE94112EL) to the serial monitor
  printByte(byte1);                     // write byte1 (Data Byte sent by the TLE9412EL) to the serial monitor
  int result = ( ((int)byte0 << 8) | (int)byte1 ); // concatenates byte0 and byte1 in result
  return (result);
}

int clearRegister(int address)          // This function clears a register and returns the data sent by the TLE94112EL. Data sent and received by the TLE94112EL are displayed on the serial monitor
{
  address = address | CLEAR ;
  digitalWrite(CSN, LOW);               // take the CSN pin low to select the chip:
  byte byte0 = SPI.transfer(address);
  byte byte1 = SPI.transfer(0);
  digitalWrite(CSN, HIGH);              // take the CSN pin high to de-select the chip:
  Serial.println();
  
  Serial.print("SDI:\t");
  printByte(address);                   // write address to the serial monitor
  printByte(0);                         // write data to the serial monitor
  Serial.print("SDO:\t");               
  printByte(byte0);                     // write byte0 (Global Satus Register of the TLE94112EL) to the serial monitor
  printByte(byte1);                     // write byte1 (Data Byte sent by the TLE9412EL) to the serial monitor
  int result = ( ((int)byte0 << 0) | (int)byte1 ); // concatenates byte0 and byte1 in result
  return (result);
}

void printByte(byte printByte)          // This function writes to the serial monitor the value of the byte printByte in binary form 
{
  for (int i = 7; i >= 0; i--)
  {
    Serial.print(bitRead(printByte, i));
  }
  Serial.print("\t");
}

  • Sign in to reply
  • DAB
    DAB over 6 years ago

    Could you provide us a summary of what the software is supposed to do and how you implemented it?

     

    DAB