Sustain The World - Design Challenge
  • Challenges & Projects
  • Design Challenges
  • Sustain The World - Design Challenge
  • More
  • Cancel
Sustain The World - Design Challenge
Blog Sustain the World Design Challenge - Getting Started
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
  • Author Author: dang74
  • Date Created: 6 Aug 2020 1:33 AM Date Created
  • Views 589 views
  • Likes 4 likes
  • Comments 2 comments
Related
Recommended

Sustain the World Design Challenge - Getting Started

dang74
dang74
6 Aug 2020

It is a real honor to be chosen as one of the participants in the Sustain the World Design Challenge.  Infineon and Newark Element 14 provided a really generous package consisting of 2 different ARM Cortex M4 development boards along with 3 different peripheral boards.

 

My entry for the challenge is to develop a controller for an automated sprinkler system that predicts the weather by means of detecting changes in the atmospheric air pressure.  When the conditions for rain are predicted the next scheduled sprinkling is delayed so that water can be conserved.

 

Initially I will develop with the XMC4200 Platform2GO development board.  This is my chosen path because this board has x2 sites for receiving Shield2GO peripheral boards and the pressure sensor board my project requires is in the Shield2GO format.  Since the rules of the contest require that the XMC4700 Relax-Lite board be used as part of your solution I will have to find a way to migrate to this development board eventually.

 

For my development environment I am using DAVE which is provided for free by Infineon.  DAVE combines the regular Eclipse IDE with a graphical method for selecting and configuring your peripherals.  The version of DAVE I am using is 4.4.2.

 

I will end this blog by attaching a couple of screen shots from DAVE.  One shows how different peripherals can be chosen from the NEW APPS menu item.  The other attachment shows how pin assignments are made in the VIRTUAL PIN VIEW. 

Attachments:
image
image
  • Sign in to reply

Top Comments

  • dang74
    dang74 over 6 years ago in reply to rati89 +1
    Thanks. The DAVE approach is working alright so far, but it's nice to know there are fall-backs.
  • dang74
    dang74 over 6 years ago in reply to rati89

    Thanks.  The DAVE approach is working alright so far, but it's nice to know there are fall-backs.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • rati89
    rati89 over 6 years ago

    Looking forwad for your results. Btw, you can also use the Arduino IDE. All three sensors are listed there and have code examples. Dave might be for MC programming working, but Arduino would be maybe easier to start. You can use also Visual Studio with an Platform.IO extension.

    Check out Github for installation and code examples: https://github.com/Infineon/