Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Flash Access to CC3100 BoosterPack with MSP432 LaunchPad
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
  • Author Author: Jan Cumps
  • Date Created: 2 Dec 2016 10:42 PM Date Created
  • Views 1468 views
  • Likes 5 likes
  • Comments 8 comments
  • wifi
  • safe and sound
  • uniflash
  • cc3100
Related
Recommended

Flash Access to CC3100 BoosterPack with MSP432 LaunchPad

Jan Cumps
Jan Cumps
2 Dec 2016

For generic use, you don't ever need to program the CC3100 BoosterPack.

 

image

That won't stop us, will it?

 

The CC3100 BoosterPack is intended to be used as a WiFi radio. It has the intelligence on it to set up connections and serve communication.

In a usual scenario, it works together with another controller. Data between the two is exchanged via SPI or UART.

There's no immediate need to access its flash . Or is there?

Well, let's not worry about that now. Let's just try to enable flash read/write access.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The normal development tool set for programming the CC3100 - or to upgrade its firmware - is with a dedicated board: the CC31XXEMUBOOSTCC31XXEMUBOOST

You use UniFlash (version 3.4.1 for the CC3X00 family, the latest version isn't CC3X00 ready at the time of writing) as the flasher.

In essence, CC31XXEMUBOOSTCC31XXEMUBOOSTis a USB COM to UART converter.

Uniflash talks to a COM port and expects that this links to the UART pins of the CC3100

image

 

The MSP432 LaunchPad (and many other LaunchPads) have this on board. The debugger is a USB to COM to 3V3 UART bridge.

I have tested this with an older version of the LaunchPad that has a different block of jumpers (the black MSP432 with pre-prod controller silicon).

 

Remove the jumpers of the RXD and TXD signals.

connect RDX with BoosterPack 1.4(TX), TDX with 1.3(RX)

connect a GND of the LaunchPad with a BoosterPack GND, and a 3V3 with a 3V3.

 

image

 

Connect both boards via USB to your PC. When connecting the LaunchPad, write down the COM port it gets assigned.

 

Now start UniFlash and choose New Target Configuration. (here's a short guide for our BoosterPack)

Select CC3X Serial(UART) Interface, then select the only available Board or Device option.

Press OK.

 

Enter the COM port that's assigned to the MSP432 UART

image

 

Press the Get Version button.

When the first red line appears in the UniFlash console, press and release the BoosterPack's RESET button (SW2).

Watch how UniFlash connects and logs the version info of your CC3100.

Then press the List File System button. You need to push the RESET every time UniFlash engages with the BoosterPack.

You'll get a nice listing of what's currently in flash, including an overview of the filesystem.

Warning: don't press the Format button. Believe me.

 

image

  • Sign in to reply

Top Comments

  • ipv1
    ipv1 over 9 years ago +1
    Hi, Here what I can recollect. For the CC3200 and CC3100 the later firmwares usually will require you to format the device since not all the space available to the user. I have had lots of problems with…
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to ipv1 +1
    Install CamStudio and record the process, maybe?
  • Jan Cumps
    Jan Cumps over 8 years ago +1
    fixed the video embedded in the blog post.
  • DAB
    DAB over 9 years ago in reply to Jan Cumps

    I wonder if it is a full device reformat like we used to have back in the old DOS days.

     

    You would loose all stored information and get a clean device ready to write to.

     

    Could be needed if you ever get a corrupted file or directory.

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago in reply to DAB

    I'm not sure , DAB. I can't find the reference back, but I recall that I read in one of the documents, wikis or support articles that you loose pre-loaded certificate files.

    I've had a discussion with ipv1 about that a long time ago. Maybe he remembers the full context?

     

    One day I hope to find that warning back in the doco.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Great post Jan.

     

    Now you have me curious, what happens if you hit the format button?

     

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<