Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe and Sound - Winter Survival Suit - Blog #14 (Final post)
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
  • Author Author: dwinhold
  • Date Created: 10 Jul 2017 1:44 AM Date Created
  • Views 1376 views
  • Likes 8 likes
  • Comments 5 comments
  • winners
  • safe & sound
  • dwinhold
  • winter survival suit
Related
Recommended

Safe and Sound - Winter Survival Suit - Blog #14 (Final post)

dwinhold
dwinhold
10 Jul 2017

Safe and Sound – Winter Survival Suit

Summary – Blog #14 (Final post)

 

This has been a great challenge that I have enjoyed immensely.  Since the start to completion there have been many challenges and accomplishments. I have to say the biggest challenge was getting the temperature sensors to work and the biggest accomplishment was water proofing the electronics. The idea of the suit has been on my mind for years, basically every time I went outside in winter time. I always thought to myself, if there was only a way to bring a heating blanket, that’s always plugged in. When this challenge came along, with the kit that was supplied by Texas Instruments, I could finally make it a reality.

 

In this blog I am showing the completed suit and how it works. I will show the convenience and safety that it provides as well as why I won’t got out in winter without it. I will also do a comparison to similar items on the market.

 

Completed suit and how it works:

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

 

Comparison:

Here is a side by side comparison to the existing heated clothing on the market at this time.

 

Heated jacket comparison
Winter Survival Suit Bosch Dewalt Makita

Heat Settings

User set temperature

Computer regulated

High, Medium & Low High, Medium, Low & Pre-heat High, Medium & Low
Heat Zones R Leg, L Leg, R Arm, L Arm, R & L Torso L Chest, R Chest & Mid-back L Chest, R Chest, Mid-back & Collar L Chest, R Chest & Mid-back
Heat Runtime

Full time all zone heating 3.2 Hrs

6 Hours 7.5 Hours 6 Hours
Normal use heat as needed 8 - 20 Hours
Pockets 2 5 5 5
Water resistant Yes Yes Yes Yes
Voltage 7.2V & 14.4V, Computer 5V 12V 12V / 20V 18V
Rechargeable Yes Yes Yes Yes
Weight 4.9 Lbs 3.5 Lbs 5.4 Lbs 3.8 Lbs
Material Polyester Polyester Polyester 94% Polyester / 6% Spandex
Warranty Long time 1 Year 1 Year

1 Year
 

 

 

 

 

 

Parts list and cost:

 

TI kit: The parts from the kit that I used were  MSP-EXP432P401RMSP-EXP432P401R and the  430BOOST-SHARP96430BOOST-SHARP96

                Total value: $33.50

 

Carbon Fiber: Ordered online from http://www.carbonheater.us/

                Total: $53.00

 

Sensors: I bought 8 temperature sensors (Twice) since I couldn’t get the first ones to work

                Total cost: $43.00

 

Wire: I bought very little wire since I had so much lying around

                Cost: $12.00

 

Batteries: The batteries and charger were fairly expensive. I am using ICR18650 batteries (8 required) and a 5V rechargeable USB battery to run the computer

                Cost: $102.24

 

Water proof spray: This was used to waterproof the electronics. The product was called “MG Chemicals Acrylic Lacquer Conformal Coating

                Cost: $23.20

 

Power relay module: This is used to switch the power on and off to the heating elements

                Cost: $13.99

 

Switches: These are used for user bypass in case of electronics failure.

                Cost: $29.94

 

Clothing: To make the suit itself I used a jogging suit

                Cost: $32.00

 

 

The total cost to make the suit: $342.87

 

 

 

Final thoughts:

 

After completing the suit, it works better then I had hoped. Unfortunately due to the extreme heat we are having I didn't try the suit on. I can't wait until winter to be using it every day, especially the -20 or colder weather. I want to thank everyone who has read my blogs, helped me with ideas and helped me through issues I encountered. I want to thank our great sponsors Texas Instruments and Element14.

 

Thank you everyone!!

 

Dale Winhold

  • Sign in to reply

Top Comments

  • dwinhold
    dwinhold over 9 years ago in reply to DAB +2
    Thank you for the comment DAB!! I like the idea of going to a supermarket to use their freezer. I will have to make some calls and see if anyone will allow it!! Dale W
  • e14phil
    e14phil over 9 years ago in reply to DAB +2
    restaurants are the same, they have walk in freezers
  • mcb1
    mcb1 over 9 years ago +1
    It's always the case when something like this is completed just in time that you don't need it I get the impression the commercial suits are more a heated work jacket, rather than an extreme weather survival…
Parents
  • DAB
    DAB over 9 years ago

    Great finish and demo.

     

    Remember, you can always go down to the nearest supermarket and ask to try it out in one of their walk in freezers.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14phil
    e14phil over 9 years ago in reply to DAB

    restaurants are the same, they have walk in freezers

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • e14phil
    e14phil over 9 years ago in reply to DAB

    restaurants are the same, they have walk in freezers