Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe and Sound - Winter Survival Suit Post #12
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
  • Author Author: dwinhold
  • Date Created: 11 Jun 2017 4:17 AM Date Created
  • Views 432 views
  • Likes 6 likes
  • Comments 1 comment
  • safe & sound
  • dwinhold
  • winter survival suit
Related
Recommended

Safe and Sound - Winter Survival Suit Post #12

dwinhold
dwinhold
11 Jun 2017

Hi Everyone,

 

This will be a short update on how things are coming along. In the past week I have been fighting a bad flu bug so I didn't get as far as I thought.

 

So, I have been wiring the power that goes to the heat elements complete with disconnects. Where the power runs into the 8 switch relay is where I put in the by pass switches. Now there is the ability for the user to heat the suit in case of computer malfunction. Due to the importance of this suit we can't rely 100% on the computer, if the user is out in extreme cold and the computer fails, without a bypass, they would freeze.

 

image

One of the biggest concerns of mine as well as others is moisture. I have solved this issue with the electronics, I am using a conformal coating to waterproof all electronics and wiring (this is shown in a previous blog). I have been testing the heating elements (Made from carbon fiber) to see what happens if they get wet from moisture. There isn't any effect to the element if it gets a bit damp from moisture, no shorting or over heating. Now the element heats up from the positive being hooked to 1 end and the negative hooked to the other. I haven't tested to see what happens if the element gets soaked in water as of yet.

 

I am getting very close to doing the final testing of the suit. My next blog will be of the fully assembled suit and showing the pre-testing of how it works.

 

Thank you for reading this update

 

Dale Winhold

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +1
    Hi Dale, Condolences on the cold, hate being sick. The wiring job looks good and the heat shrink should help with the moisture issue. DAB
Parents
  • DAB
    DAB over 9 years ago

    Hi Dale,

     

    Condolences on the cold, hate being sick.

     

    The wiring job looks good and the heat shrink should help with the moisture issue.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Hi Dale,

     

    Condolences on the cold, hate being sick.

     

    The wiring job looks good and the heat shrink should help with the moisture issue.

     

    DAB