Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe and Sound Wearables- Code Composer Studio Woes
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
  • Author Author: jomoenginer
  • Date Created: 21 Mar 2017 7:28 AM Date Created
  • Views 991 views
  • Likes 6 likes
  • Comments 5 comments
  • code composer studio
Related
Recommended

Safe and Sound Wearables- Code Composer Studio Woes

jomoenginer
jomoenginer
21 Mar 2017

So, lately I have been running into a series of issues with Code Composer Studio and I thought I would share these with other folks in case the may be helpful.

 

1. After a recent TI Update, or rather Upbreak, when attempting to import a project through the TI Resource Explorer in CCS 7.0.0.x, the following error is seen:

 

Error importing project. Location cannot be resolved: "c:/ti/tirtos_msp43x_2_20_00_06resources/msp_exp432P401RLaunchpad/driverExamples/tiDriverExamples/emptyExamples/com_ti_rtsc_tirtosmsp430_example_100.projectspec"!

 

NOTE: The tirtos_msp43x and resources directories are collapsed and a '/' is used instead of '\' to separate the folders. This is on Windows

 

Issue logged with TI:

https://e2e.ti.com/support/development_tools/code_composer_studio/f/81/p/582313/2138715#2138715http://

 

At this time, there is no resolution for this in CCS 7.0.0.x and it is suggested to use the latest CCS, well at least as of 03202017, CCS 7.1.0.x.

http://processors.wiki.ti.com/index.php/Download_CCS#Download_the_latest_CCS

 

2. The other issue has been seen in CCS 6.x as well as 7.0.0.x where, at least in my case, if the .cfg file is left open in the Editor window when CCS is closed, once CCS is started again, the following error is seen:

 

Error Report

 

Sorry, I'm having problems creating this editor. An unexpected exception was thrown.

 

org.eclipse.rtsc.xdctools.INVALID_CODEGEN_LOCATION: Invalid codegen location "

 

In my case, if I close the file and then reopen it the issue goes away.

 

This issue has also been seen by others when just opening a .cfg file.

 

Issue filed with TI:

https://e2e.ti.com/support/embedded/tirtos/f/355/t/544313

 

3. Another issue was when I attempted to add C++ Style Classes to my project.  When I initially added a C++ Class, I ran into the following error:

 

"warning #10247-D: creating output section "HEAP_CACHE" without a SECTIONS"

 

To resolve this, I removed the 'iostream' and namespace entries in the file. Also, since I have both 'C' and 'CPP', I have found it is best to add the following in the header file:

#ifdef __cplusplus

extern "C" {

#endif

 

// Standard "C" code here

 

#ifdef __cplusplus

}

#endif

 

I found the following link to be helpful:

C++ Support in TI Compilers - Texas Instruments Wiki

 

Also, in TI-RTOS for MSP43x, there is an C++ example that shows an implementation of C++ in TI-RTOS.

This is located:

   TI-RTOS for MSP43x - v2.20.00.06

     Documents->Development Tools->MSP-EXP432P401R->Kernel Examples->C++ Example (bigtime)

 

Using this example, I set the following in the .cfg file:

     System (Hwi and Swi) stack size - 768

     Heap Size - 2048

     Enable Assets - False (Unchecked)

     Enable Logs - False (Unchecked)

 

4. One bright side, with the release of Code Compose Studio 7.x, the now provide the Full License for CCS 6.x.  This means no more limitations in CCS for time, code size, debug probe or target used.

    

     See the Licensing - CCSv6 Wiki for more info:

         http://processors.wiki.ti.com/index.php/Licensing_-_CCSv6

 

Hopefully this is helpful to someone.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +1
    Seeing someone else's pain is always useful to anyone considering the use of a product. One person's "intuitively obvious" is another person's "obtuse" software. DAB
  • Jan Cumps
    Jan Cumps over 9 years ago +1
    Good that you filed / updated the support issues. For #1, the ti\tirex-content; vs \ti change created issues when I was migrating from 6.X to 6.2 (the intro of the new Resource Explorer). Several projects…
  • jomoenginer
    jomoenginer over 9 years ago in reply to Jan Cumps +1
    Jan, The fun part is that with CCS 7.1 the download location for Resource Explorer changed from C:\ti\tirex-content to C:\ti so if you download a new package from Resource Explorer in CCS 7.0.0 it will…
Parents
  • DAB
    DAB over 9 years ago

    Seeing someone else's pain is always useful to anyone considering the use of a product.

     

    One person's "intuitively obvious" is another person's "obtuse" software.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 9 years ago

    Seeing someone else's pain is always useful to anyone considering the use of a product.

     

    One person's "intuitively obvious" is another person's "obtuse" software.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • jomoenginer
    jomoenginer over 9 years ago in reply to DAB

    Yeah, the real pain is when attempting to add C++ into the mix especially when trying to use modules that were written in "C" like the Graphics libs since they use the standard variable types such as int8_t for strings rather than ints.  Out of the box, TI ARM Compiler used C89 so it's best to change this to C99. However, the C++ compiler only supports up to C03 thus does not support the standard types and will cause compiler errors. I ended up creating a new project but using the GNU C++ compiler which supports up to C11 with the added build option "-std=c++11". It still has issue, so I ended up putting the Graphic calls into a separate ".c" file and reference it from the ".cpp" files. I'm still trying to iron this out.