Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe and Sound : Winter/Cold Weather Survival Suit Blog#9
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
  • Author Author: dwinhold
  • Date Created: 29 Apr 2017 5:42 PM Date Created
  • Views 1469 views
  • Likes 4 likes
  • Comments 7 comments
  • water_proof
  • safe & sound projects
  • safe & sound
  • dwinhold
  • winter survival suit
  • cold
Related
Recommended

Safe and Sound : Winter/Cold Weather Survival Suit Blog#9

dwinhold
dwinhold
29 Apr 2017

This update is about water proofing my project. Everything done here is the first time I ever worked with this product and it was done live, so if it fails we will all see it go wrong. There are 3 videos attached, the first is showing the product, second is applying it to the board and third is putting the powered board under running water.

 

I use an Arduino Uno as a test so if this doesn't work I don't wreck the MSP432.

 

So, what do you think? Will it work? Fail? Here is the challenge, post below before you watch the last video and say weather you think it worked or if I ruined my Arduino Uno. Don't give it away (at least for a couple of days) after you watch.

 

Video #1 (The Acrylic Conformal Coating)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Video #2 (Spraying it on the board) **As a note - Take every safety precaution when using this, it is poisonous**

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Video #3 (Water testing)

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

Hope you enjoyed watching.

 

Dale Winhold

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +3
    Nice update. I would try a salt water mixture to test the boards. I worry about human sweat soaking through the clothing to the boards. DAB
  • mcb1
    mcb1 over 9 years ago +1
    Water and electronics are an interesting mix. From my observations over the years, it is not immersion in clean water that causes a problem. High frequency circuits my have some changes due to the capacitance…
  • dwinhold
    dwinhold over 9 years ago in reply to mcb1 +1
    Hi Mark, Thank you for the reply. I definitely agree that water and electronics aren't a good mixture. Clean water is what was the closest for this experiment, I will have to try it out in salt water as…
  • dougw
    dougw over 9 years ago in reply to Workshopshed

    Yes, interesting to see that the chip in a socket was protected ....

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • balearicdynamics
    balearicdynamics over 9 years ago in reply to DAB

    By the point of view of the protection I think that it is not needed to check the coated board; it is sufficient to make tests with a conductive surface and see what happens with different environmental agents like salt water, basic water, acid water, several organics etc.

    Instead I am curious too to see what happens in a real non-conventional environment (like a sera boat) to all the non-coated parts, like the USB connector, just to mention one.

     

    I can say that there is a series of technical specifications that means that some electronic components or tools are certified to operate in marine environments. This is a complex world I worked with a client in Genova (Italy) in the mid of '80s. Just as an example, the following link is a list of some providers of this kind of components: Military Specification, Aerospace, Marine, Automotive Electronic Components on ThomasNet.com

    I have no t found the regulatory specifications but can be found on the Internet.

     

    Enrico

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Workshopshed
    Workshopshed over 9 years ago

    A far from ideal candidate for this kind of spray, glad to see it survived so far.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Nice update.

     

    I would try a salt water mixture to test the boards.

     

    I worry about human sweat soaking through the clothing to the boards.

     

    DAB

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 9 years ago

    Nice. Think I would have put female headers on the Arduino to avoid spray on the pins...

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>