Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe & Sound -Flood early-warning Alarm Pack #1: Introduction to Project
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
  • Author Author: fyaocn
  • Date Created: 18 Feb 2017 12:48 PM Date Created
  • Views 1029 views
  • Likes 5 likes
  • Comments 4 comments
Related
Recommended

Safe & Sound -Flood early-warning Alarm Pack #1: Introduction to Project

fyaocn
fyaocn
18 Feb 2017

1. Description of Proposed Project

This project is designed for villagers or passerby who may be exposed to great danger of unexpected flood discharge. This alarm pack sends alarm to persons lingered in Reservoir Downstream Riverbed, allows them enough time to take precautions.

With further reseach, there have been some shortcomings in my proposed plan. I would revised a little to make it practical. I would replace OP3001 with Water Clarity sensor TSW-10 for clarity detection.

Further study shall be made to arrange the alarm pack nodes along the river and transimission data to downstream. This appears more challengous, but the TI-CC2650 via Zigbee protocle can do the job. At lease a pair of CC2650 shall be needed and within the time limit, I do not think I can make it operational. I will try to work on it after placing another order for CC2650 design packs.

2. Hardware and software

2.1 Principle Blocks

The sensors of  alarm pack is  in a waterproof hollow rod erected in riverbed.

The PCB capacity sensor immersed in water can measure the water lever with capacity variation.

TSW-10 water clarity sensor immersed in water can sense the water clarity if more soil is flushed with the water as another sign of flood.

These data are sent for Cloud backup with CC3100 for WIFI or CC2650 for BLE communication. Only one boostpack, CC3100 or CC2650  can be attached to the MSP432 launchpad. Therefore it is better to used CC3100 boostpack for cloud connection. With CC2650, most of the clouding programming shall be done on mobile APP side, it can be made as one option solution if time is enough.

 

2.2 Hardware

The following design kits shall be used,

EXP432P401R- Central monitoring and capacitor sensor detection.

CC3100MODBOOST_ Internet connection

430BOOST-SHARP96430BOOST-SHARP96Memory LCD Booster Pack-local setting and User interface(Optional since the alarm pack immersed in water LCD can be little use underwater but I will use the LCD durging test procedure

One TSW-10  clarity sensor shall be used instead of OP3001(On boostpack , it is hard to be watertight )

MSP432P401 is core MCU to control all the operation and communication jobs, including water level sensing, water pollution sensoring, sensor data cloud backup, alarm trigger, internet connection, sign and sound alarming.

 

2.3 Software

TI CCS shall be used for IDE platform since all the library, samples and documents are embedded in this software. No further programming or debugging software shall be needed.

Extra effort on customized PCB board design for this alarm pack shall be made if the project can be completed in time and passed pilot test. CADSTAR shall be used for this purpose.  MSP432P401  and CC3200 , which is compatible with CC3100, shall be integrated in this design.

As to the cloud, Amazon AWS IoT+Lambda service or Azure can be used for IoT connection. But more flexible dweet.io can be better choice. I will finalized in my design.

 

3 I hope I can complete the design in time and design one customized prototype PCB board as final product.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 9 years ago +2
    Interesting project. There are a number of ways to detect the water rising, so I will be interested in seeing what you choose. DAB
  • fyaocn
    fyaocn over 9 years ago in reply to jkutzsch +2
    Thanks. As you suggested. Siren is one of good choice for alarm. But in my design, cloud connection part is more challege. In fact, single alarm pack in riverbed is of no used since any one can see the…
  • fyaocn
    fyaocn over 9 years ago in reply to DAB

    MSP432 is good at capacitive sensing. I would try this with self-made sensor. I can post my calculation process for verification.

    Thanks.

    F. Yao

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • fyaocn
    fyaocn over 9 years ago in reply to jkutzsch

    Thanks.

    As you suggested. Siren is one of good choice for alarm. But in my design, cloud connection part is more challege.

    In fact, single alarm pack in riverbed is of no used since any one can see the flood even before the water touches the sensors of alarm pack. Sensors far away sending alarm to cloud, trigger alarm signal downstream can be real thing instead of demo toys. Of course, this bring challenge to me within required development time.

    F Yao

    Another interesting part for the Dev Kits is Energy-harnest Power Board, It would be great if I  can make the system maintenance-free. But I am afraid I have included enough in my draft design. But more furbishment is neccessary even after the design contest.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • jkutzsch
    jkutzsch over 9 years ago

    Very interesting.  Driving through areas in Arizona with all of the signs warning of flash floods I could see something like this being of use!

     

    How are you implementing the Alarm system?  Will it be something like a large siren that can be heard for some distance?  I have seen those used for Tornado warnings and they can be quite effective in getting one's attention!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 9 years ago

    Interesting project.

     

    There are a number of ways to detect the water rising, so I will be interested in seeing what you choose.

     

    DAB