Safe and Sound
  • Challenges & Projects
  • Design Challenges
  • Safe and Sound
  • More
  • Cancel
Safe and Sound
Blog Safe & Sound -Flood early-warning Alarm Pack #2: Development Packs
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
  • Author Author: fyaocn
  • Date Created: 24 Mar 2017 3:15 AM Date Created
  • Views 420 views
  • Likes 5 likes
  • Comments 0 comments
Related
Recommended

Safe & Sound -Flood early-warning Alarm Pack #2: Development Packs

fyaocn
fyaocn
24 Mar 2017

It has taken some time to receive the development kits. Just got them yesterday and can not wait to share these pics.

1. Total packs

image

2 Texas Instruments Main Application MCU  MSP-EXP432P401RMSP-EXP432P401R

This is the Top-star in this projects, great balanced between extra low power comsumtion and high performance

image

3.CC3100MODBOOST Wi-Fi Network Processor and  BOOSTXL-CC2650MABOOSTXL-CC2650MA BLE Network Processor

Another parts fit in my projects for RF connection. I have planned with CC3100 only, while CC2650 poses more challenges.

In this sense, my project will evolve from single product into one ecosystem. I would like to take a try.

image

image

 

4  430BOOST-SENSE1430BOOST-SENSE1 Capacitive Touch Booster Pack and  430BOOST-SHARP96430BOOST-SHARP96 Memory LCD Booster Pack

These are Input and Output Interface, which are optional parts in my projects. I will show how to use them.  Since extra sensors and buzzer shall be used, the pin may not enough for them to be integrated in my project.

image

 

5.BQ25570EVM-206 Power Management Bat and  DLP-7970ABPDLP-7970ABP NFC Transceiver

These two parts are not used in my project, I shall make brief introduction to them.

 

image

But ,BOOSTXL-SENSORS Sensors Booster Pack which is listed in the delivery list are not shown. I have check the packing list, it is there but not in the box.

Maybe I have misplace them in wrong place, I have to check again and use some alternative sensor. But that would not be of any problem. I can fix it.

6. It appears that I am on the way of building several jungle. I would reschedule my plan. The ecosystem need more skill and more effort, at least triple that of one Alarm Pack.

But the design philosophy of TI boost back sparks my though, I would try to make it work in time.

Fortunately,  TI offers one fast-tracing Tools of Energia. I will use Energia in stead of CCS for the development. Only  TI-RTOS can not be fully applied in Energia.

Now, it is time to roll up and to go.