Twist, Turn and Move Design Challenge with TE Robotics
  • Challenges & Projects
  • Design Challenges
  • Twist, Turn and Move Design Challenge with TE Robotics
  • More
  • Cancel
Twist, Turn and Move Design Challenge with TE Robotics
Blog ARDUMOBO blog 3: Ultrasonic sensors testing
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: a33333
  • Date Created: 22 Aug 2022 3:22 AM Date Created
  • Views 1357 views
  • Likes 6 likes
  • Comments 1 comment
Related
Recommended

ARDUMOBO blog 3: Ultrasonic sensors testing

a33333
a33333
22 Aug 2022

Obstacle detection

For obstacle detection my mobile robot will use two HC-SR04 ultrasonic sensors. One sensor will be mounted at the front of the truck and the other at the back of the truck so that obstacle detection will be possible in both forward and reverse mode. 

This sensor module is advertised to provide a 2cm to 450cm range with an accuracy of  3mm. The sensor generates a 40 KHz ultrasonic burst. It works by measuring the propagation delay between the end of the burst and the start of the reflected acoustic signal. By multiplying the speed of sound with the propagation delay one can find out an estimate of the distance to the obstacle (actually this is twice the distance since the acoustic signal has to be reflected by the obstacle.)

image

Testing the sensors

I tested four different sensors. The next pictures show my testing setup. Since for my application an accuracy of one to two centimeters is acceptable, I was not very interested to find out how accurate (at millimeter range) the sensors are. I just wanted to make sure the sensors are functional. I tested the four sensors at distances that I plan to detect for my application: 30, 20 and 10 cm.  

image

 image

All sensors behaved OK, with an accuracy within one centimeter. 

  • Sign in to reply
  • robogary
    robogary over 4 years ago

    Cool. Did you test 4 different HC-SR04s by the same vendor ?