Twist, Turn and Move Design Challenge with TE Robotics
  • Challenges & Projects
  • Design Challenges
  • Twist, Turn and Move Design Challenge with TE Robotics
  • More
  • Cancel
Twist, Turn and Move Design Challenge with TE Robotics
Blog Pool Butler Blog #10 Twist Turn & Move - Propulsion Addendum - schematic, Arduino code, TE connectors, SMD relay card, & photos
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Leaderboard
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: robogary
  • Date Created: 5 Sep 2022 2:15 PM Date Created
  • Views 939 views
  • Likes 9 likes
  • Comments 3 comments
  • ardunino
  • pool butler
  • te connectivity
  • Twist Turn and Move Robotics Design Challenge
  • terobotics
  • Turn and Move Design Challenge with TE Robotics
Related
Recommended

Pool Butler Blog #10 Twist Turn & Move - Propulsion Addendum - schematic, Arduino code, TE connectors, SMD relay card, & photos

robogary
robogary
5 Sep 2022

This an an blog update for the Pool Butler Propulsion control system. The previous propulsion blog contained the listed details:

Pool Butler Blog #2 Twist Turn & Move -the Airboat Propulsion compartment 29-Jul

1. building the junk pile strobe tach to measure propeller speed.
2. building of a side project with the MPU 6050 gyro sensor and a SSD1306 display to experiment with that sensor.
3.First build of the propulsion enclosure:
3a.... to test the RC pulse width measure code
3b. ...to measure and chart the motor speed VS DC volts and required amps with the 8060 propeller

This blog addendum contains:

  1. the Pool Butler propulsion controls schematic
  2. updated photos showing the provided TE connectors and SMD relay 
  3. Pool Butler propulsion system Arduino code

Propulsion Control with cover on

image

Propulsion Control - SMD relay mounted & wired on a thru hole breadboard with screw type terminal boards

image

image

2.Propulsion Controls SCHEMATIC

image

// ---------------------------------------------------------------------------
//propulsionWithRollCutoff.ino
//Arduino Nano old bootloader
// Use the Arduino serial monitor to get CH1_PWMtime and CH2_PWMtime center and endpoint value to normalize values.
// This a unique application that allows the propeller to get both forward & reverse, the reverse to help with deceleration
//
// *** MEASURED DATA ****
// channel 2 is used for speed reference
// CH2_PWMtime center = 1498 to 1506, usec pulsewidth
// CH2_PWMtime full fwd = 1919, usec pulsewidth
// CH2_PWMtime full back = 1133, usec pulsewidth
//
// MPU6050 is a MEM gyro used to detect pitch, roll, and yaw. if roll or pitch exceed 35 degrees, the PitchRoll_OK bit drops out to remove power to the prop
//This program was first written for a generic L298N H bridge, but is slightly modified to control a DRI0002 DFrobot L298N H bridge
//
// ---------------------------------------------------------------------------


unsigned long CH2_PWMtime; //pulsewidth time of Channel 2 (into pin 4) RC in microseconds, 1000 = full REV (or -90 degress), 1500=zerospeed or 0 degrees, 2000=full FWD (or +90 degrees)
unsigned long timeout = 23000; //timeout of PWM , set timeout for reading a pulsewidth at 15% moree than max expected 20ms (tried 2300 and caused problems)

int CH2_PWMtime_int; // CH1_PWMtime is an unsigned long, convert it to integer

int CH2_PWM_REF_usec ; // magnitude of microseconds pulse width from 1500 usec centerpoint

int CH2_PWM_SpdRef ; // RHS speed reference scaled for 255 = 100%
int CH2_PWMtime_int_LastScan=1500;
int FWD=LOW; // direction of Channel 2 speed ref
int REV=LOW; // direction of Channel 2 speed ref

#include "Wire.h"
#include <MPU6050_light.h>

MPU6050 mpu(Wire);
unsigned long timer = 0;
float roll=0.0;
float pitch=0.0;
float yaw=0.0;
//**********************Tip Over Protection Adjustments********
int roll_limit_degrees=30;
int pitch_limit_degrees=25;
int PitchRoll_OK = HIGH;
//**********************************************************

void setup()
{
pinMode(2, OUTPUT); // High when prop is spinning
pinMode(4, INPUT); // RC receiver Channel 2 motor speed control input

pinMode(9, OUTPUT); // PWM motor FWD, bit low in reverse DFRobot DRI0002 E1 & E2 pins are PWM control
pinMode(10, OUTPUT); // PWM motor REV, bit low in FWD DFRobot DRI0002 M1 & M2 pins, FWD=0 REV=1
pinMode(13, OUTPUT); // MPU 6050 Calibrate process
Serial.begin(115200);

// MPU6050 setup - ?? get a calibration cycle on a reboot, and also on entering and exiting the serial monitor
Wire.begin();

byte status = mpu.begin();
digitalWrite(13,HIGH); // Arduino Nano D13 LED
Serial.print(F("MPU6050 status: "));
Serial.println(status);
while(status!=0){ } // stop everything if could not connect to MPU6050

//Serial.println(F("Calculating offsets, do not move MPU6050"));
delay(2000);
// mpu.upsideDownMounting = true; // uncomment this line if the MPU6050 is mounted upside-down
mpu.calcOffsets(); // gyro and accelero
Serial.println("Done!\n");
digitalWrite(13,LOW); // Arduino Nano D13 LED
}

void loop()

{
// get pitch roll and yaw from the MPU 6050
mpu.update();

if((millis()-timer)>100)
{ // print data every 100ms
// Serial.print("X : ");
// Serial.print(mpu.getAngleX());
roll=(mpu.getAngleX());

// Serial.print("\tY : ");
// Serial.print(mpu.getAngleY());
pitch=(mpu.getAngleY());

//Serial.print("\tZ : ");
//Serial.println(mpu.getAngleZ());
//yaw = (mpu.getAngleZ());

timer = millis();
}

if ((abs(roll)<(roll_limit_degrees))&& ((abs(pitch))<(pitch_limit_degrees)))
{ PitchRoll_OK = HIGH;
digitalWrite(12,HIGH);}
else
{PitchRoll_OK = LOW;
digitalWrite(12,LOW);}
// Serial.print("PitchRoll_OK = ");
// Serial.println(PitchRoll_OK);
// delay(2000);

// Reads a pulse (either HIGH or LOW) on a pin. For example, if value is HIGH, pulseIn() waits for the pin to go HIGH, starts timing, then waits for the pin to go LOW and stops timing. Returns the length of the pulse in microseconds. Gives up and returns 0 if no pulse starts within a specified time out.
// Works on pulses from 10 microseconds to 3 minutes in length.

CH2_PWMtime = pulseIn(4, HIGH, timeout); // pulseIn(pin, value, timeout) value is HIGH or LOW, timeout and value are long int
// Serial.print("CH2 Time: ");
// Serial.println(CH2_PWMtime);
// Serial.print("CH2 Spd Ref: ");
// Serial.println(CH2_PWM_SpdRef);

CH2_PWMtime_int = (int) CH2_PWMtime; //convert unsigned long to int
if (CH2_PWMtime_int==0) {CH2_PWMtime_int=CH2_PWMtime_int_LastScan;} // 0 is a missed scan , zero directions
if (CH2_PWMtime_int>1999) {CH2_PWMtime_int=1999;} // max limit forward
if (CH2_PWMtime_int<1000) {CH2_PWMtime_int=1000;} // max limit reverse

Serial.print("CH2 Time: ");
Serial.println(CH2_PWMtime_int);

/// create fwd and reverse direction bits

if ((CH2_PWMtime_int - 1500) >= 30 ){ FWD = HIGH; } else {(FWD=LOW);} // 10 allows some deadband switching bridges
if ((CH2_PWMtime_int - 1500) <= -30 ){ REV = HIGH; } else {(REV=LOW);} // -10 allows some deadband switching bridges
// if (CH2_PWMtime_int==0) {FWD = LOW; REV =LOW;} // 0 is a missed scan , zero directions

Serial.print("FWD = ");
Serial.println(FWD);
Serial.print("REV= ");
Serial.println(REV);

/// create a speed reference in microsends
CH2_PWM_REF_usec = abs(CH2_PWMtime_int - 1500); // zero to 500usecs = 0 to 100 % speed
CH2_PWM_SpdRef = (CH2_PWM_REF_usec/2); // cheap and dirty way to make speed reference, top = 500 microseconds, which corresponds to an analogWrite value 255. divie by 2 makes it just a tad slower.
// Serial.print("255 is top speed reference ");
// Serial.println(CH2_PWM_SpdRef);


//if (CH2_PWM_SpdRef>200)
// {
// CH2_PWM_SpdRef =(CH2_PWM_SpdRef+45);
// } // if near top speed kick in that leftover remainder spdref
// }
// Serial.print("255 is top speed reference ");
// Serial.println(CH2_PWM_SpdRef);

if (CH2_PWM_SpdRef>50) // relay for prop running LEDs
{
digitalWrite(2,HIGH);
}
else
{
digitalWrite(2,LOW);
}

// output logic for the H Bridge DFRobot DRI0002
analogWrite(9, (CH2_PWM_SpdRef)); // analogWrite values from 0 to 255 //comment out for generic L298N module

if ((FWD==HIGH)&& (PitchRoll_OK==HIGH))
{
// analogWrite(9, (CH2_PWM_SpdRef)); // analogWrite values from 0 to 255 remove comment out for generic L298N module

analogWrite(10, 0);
}
else if ((REV==HIGH)&& (PitchRoll_OK==HIGH))
{
// analogWrite(9, 0) ; // analogWrite values from 0 to 255 remove comment out for generic L298N module
// analogWrite(10,(CH2_PWM_SpdRef));
analogWrite(10, 255);
}
else
{
analogWrite(9, 0); // analogWrite values from 0 to 255
analogWrite(10, 0) ;
}
delay (50);



if (PitchRoll_OK==LOW)
{ delay(2000);}

CH2_PWMtime_int_LastScan=CH2_PWMtime_int;
}

  • Sign in to reply
Parents
  • DAB
    DAB over 4 years ago

    Nice update.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 4 years ago

    Nice update.