Ultimate RoadTest
  • Challenges & Projects
  • Design Challenges
  • Ultimate RoadTest
  • More
  • Cancel
Ultimate RoadTest
Blog Project "code name" Part 021
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 19 Jun 2012 9:37 PM Date Created
  • Views 693 views
  • Likes 1 like
  • Comments 1 comment
  • ultimate_roadtest
Related
Recommended

Project "code name" Part 021

COMPACT
COMPACT
19 Jun 2012
June 20th
Return of the Code Inspector

During my perusal of the basic_wifi_application and other MSP430 examples I have noticed small annotation errors and minor "assumption" errors (some of which I have previously mentioned).

One such example is the standard blink led demonstration. It assumes that there are always LEDs connected to P1.0 and P1.1.

This is not the case with the MSP430 Fraunchpad where the equivalent LEDS are connected to PJ.0

This is minor but could catch a novice out.

 

More importantly to me is the basic_wifi_application. Apart from misspelling 'the' several times, reference to the LEDs are incorrect. They should be;

 

Code RefPCB RefI/O PinFunction
LED4(In a comment - actually means LED8)n/an/a
LED5LED6P3.5WLAN Successful
LED6LED7P3.6SMART Config Process active
LED7LED8P3.7CC3000 successful connection

 

 

 

Watch out for Boobie Traps!

The MSP430 contains a number of peripherals that are connected to I/O Pins.

I/O PinDescription
P2.7Enable Accelerometer and Thermistor (and LDR if installed)
P3.0Accelerometer X Output (Analog)
P3.1Accelerometer Y Output (Analog)
P3.2Accelerometer Z Output (Analog)
*P3.3LDR Output (Analog) [If installed]
P1.4Thermistor Output (Analog)
*PJ.432.768kHz Crystal [if installed]
*PJ.532.768kHz Crystal [if installed]
P2.1TXD to USB
P2.0RXD to USB

 

Also watch out for pins connected to WiFi-SL Module when used. Details of this are in a previous blog entry.

 

Please note that not all MSP430 I/O pins are brought out the standard headers.

Some are brought out to optional headers (eZ-RF and TP12-TP15 pads under LEDs) and some like PJ.4 and PJ.5 not at all where you have to make your own arrangements (which could be to use the pads where the crystal would be soldered).

 

Note: This and some recent blogs may appear that I am repeating myself but I am documenting them down for easy reference.

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    Good catches.

    Hidden documentation errors are the bain of any manufacturer's offerings.

     

    Repitition is good.  Sometimes you do not fully appreciate an impact when you first announce it, but when you see it again and investigate it more carefully, then learning can occur. image

     

    Good Update,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    Good catches.

    Hidden documentation errors are the bain of any manufacturer's offerings.

     

    Repitition is good.  Sometimes you do not fully appreciate an impact when you first announce it, but when you see it again and investigate it more carefully, then learning can occur. image

     

    Good Update,

    DAB