Ultimate RoadTest
  • Challenges & Projects
  • Design Challenges
  • Ultimate RoadTest
  • More
  • Cancel
Ultimate RoadTest
Blog Project "code name" Part 030
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 27 Jun 2012 8:19 AM Date Created
  • Views 674 views
  • Likes 1 like
  • Comments 1 comment
  • ultimate_roadtest
Related
Recommended

Project "code name" Part 030

COMPACT
COMPACT
27 Jun 2012
June 27th

More on the C2000 Multi-DC/DC Color LED Lighting Kit Interfacing.

Like the MSP430 Fraunchpad Serial Port, the C2000 Multi-DC/DC Color LED Lighting Kit control serial port is also via a USB interface IC.

In order to use the C2000 Multi-DC/DC LED Color LED Lighting Kit with the MSP430, JP4 on the C2000 is removed to disconnect it from the output buffer from the USB interface and the TX and RX lines

which are annotated on the PCB are connected through to the MSP430. In my case via the CD4052.

 

The default baud rate is set at 57,600 bps in the C2000 application.

The code is very easy to bring up in CCS. It's the same process used for the MSP430WARE but instead we use the controlSUITE.

 

The C2000 Multi-DC/DC Color LED Lighting Kit comprises of a 32-bit F28027 Picolo Microcontroller that controls two types of switching power supplies to light up LEDs.

It has SEPIC(buck/boost) power supplies that can accomodate voltages below and above the target output voltage and a Boost power supplies.

The system monitors both the output voltage and current using its 4.6MSPS 12 bit ADC.

Switching is accomplished with independent PWM timers.

 

Development is through CCS and example code is provided.

  • Sign in to reply
Parents
  • DAB
    DAB over 14 years ago

    Makes sense, the common serial interface keeps your options open and the C2000 takes care of implementing your lighting commands based upon the parameters you send.

     

    Cool,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 14 years ago

    Makes sense, the common serial interface keeps your options open and the C2000 takes care of implementing your lighting commands based upon the parameters you send.

     

    Cool,

    DAB