• Products and Partners
    Products and Partners
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
Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog First_Ideas
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
  • Author Author: e14 Contributor
  • Date Created: 1 Aug 2015 7:25 PM Date Created
  • Views 952 views
  • Likes 4 likes
  • Comments 15 comments
  • solar_farm
Related
Recommended

First_Ideas

e14 Contributor
e14 Contributor
1 Aug 2015

Hey everyone! Currently, I am unable to do much because I am traveling; however, I will try to summarize my plan and talk about current ideas even though I do not currently have anything concretely set. Basically, I plan to use PVC pipes and some plastic clear boxes (for letting sunlight through) with a pump and adder of nutrients. Since, I do not want to spend a lot of money, I am looking for a hopefully sustainable and relatively cheap way for a vertical farm, which means that one of my first concerns is looking for cheap solar panels (an oxymoron). I haven't decided where to put the solar panels, but most likely I will put them at the top or sides of the support beams. Most of the solar power will be stored for hourly sensor checks and refills of fertilizer and water. The rest will be used to light plants in the back of the farm that are more shaded. So that basically wraps up the basic idea.

 

For the first week, I will search online for a few materials and try to get a general estimate on energy costs and the optimal concentration of fertilizer in water, but other than that just going to do general research like find out if the packet of LEDs contains the right spectrum of light wavelength for photosynthesis. Also if anyone reading this knows what types of plants you can choose, it would be great if they could comment it. I will try to start thinking about the specific plant I'll use to make the boxes fit the right specifications. Probably one of the first and easiest things I will do is set up a small system with an arduino to find out the conductivity of water at different salinity levels so that I can find out whether the changes are significant enough that I can suffice with cheap home made sensors. Luckily for me, this project is indoors, so I really do not have to worry too much about making sure everything gets direct sunlight so long as the plants aren't in the shade of something.

 

So now an in-depth summary.

There are three boxes stacked at a 45 degree angle to maximize sunlight and decrease space used. I power valves, sensors, and control systems (mixers, feeders, and pumps to control the flow of water) with solar panels.

Sensors

First off, there are the basic temperature/ humidity sensors from the micro controller. Then there are photo resistors and currency testers  which help control salination levels and light intensity. Also there is an ultrasonic sensor to tell the depth of the water to make sure the plants always have enough space to grow- both upwards and for their roots not to compete for resources. As a somewhat interesting side-note, a hydroponic farm is much better at resource control for packing in many plants because you do not have to worry too much about resource competition, although you still have to worry about not squishing the roots and limiting plant growth. The information from these will either send off warnings or automatically change the problem.

Boxes

Connected by pvc pipe containing the nutrient fluid for the plants

There is a thin layer of foam for the plants to grow on. The boxes are open to help control humidity and CO2 levels. Underneath the foam they have water.

Hopefully, when I manage to clear out some of the storage bins at my home, I can figure out if I need a humidity changing system, but I seriously doubt I will need it. However, if it should become important I am thinking about making the foam watertight to prevent water vapor from escaping and affecting the air above the foam (also saving a lot of water since in Texas even inside, water would evaporate pretty quickly). Unfortunately it will also invite a host of problems-mainly where to put the ultrasonic sensor then since the foam would no longer float on top of the water and move with it. .

So that is the end of my blog post for now. I will try to post a picture of a framework when I get back home and buy some of the iron poles.

  • Sign in to reply

Top Comments

  • DAB
    DAB over 11 years ago +1
    Are you planning to control the temperature for the plants? You have to be careful if they get too hot or too cold. DAB
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds +1
    I have had great success with the misting and spaying systems for Greens with small root structure [ lettuce etc] and Cloning cuttings [Apple,Lemon, Grape]. Get to bigger root structures and it never worked…
  • RWReynolds
    RWReynolds over 11 years ago in reply to e14 Contributor +1
    My grow space will be in our garage and is not climate controlled. So heat is a bigger concern for me. I'm thinking of implementing am evaporation style cooler. something I've wanted to build anyway, for…
  • RWReynolds
    RWReynolds over 11 years ago

    Great information Michael.

     

    Another method that might achieve acceptable aeration is to use a simple misting or sprinkler style nutrient/water delivery system.

     

    Guys, what's your preferred grow medium for hydroponics? I have used clay pellets in the couple of hydro projects I've done in the past. But I'm thinking of using coconut coir for this project. Any preferences?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago

    Sorry I was a bit vague with the last message.

     

    The water/nutrient mix you are using, needs more than just the correct amount of nutrients to work. The roots need a little bit of oxygen to work, if you let air come into contact with water the water will absorb a little oxygen out of the air to replace the bit the plants are using,

     

    You could add chemical  oxygen, Hydrogen peroxide does this well, but it is an expensive way to solve the problem. A more common way to Oxygenate the water is to increase the water/air interaction. Ie add an air pump and air stone to the system or by agitating the surface of the water. I preffer to use a "air Lift Pump" Because it does both and lets me move the water to a filtering point.

     

    Soil based plants die when over watered because the roots get no oxygen. But in aquaponics the plant is able to survive because although they are submerged in water, the water is oxygenated.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Figured out how to do it. I can dissolve oxygen at the beggining if I need too. Although condensed oxygen is not a gas I want in the house really... Especially near electronics. Maybe collected from outside environment?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to m.ratcliffe

    Thanks for the tip

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago

    I found that the more DO [Dissolved oxygen] I had in the water the better the results, Blocking off the system with foam might cause you a bit of a problem if you have no water/air interaction elsewhere in the system. It sounds like an interesting project, I need a Conductivity Sensor myself and might hold off for a review on your diy solution.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<