Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Blog Vertical Farming Check In pt 2: Seeds, Kits and more!
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
  • Author Author: element14Dave
  • Date Created: 22 Aug 2015 7:18 PM Date Created
  • Views 2344 views
  • Likes 3 likes
  • Comments 35 comments
Related
Recommended

Vertical Farming Check In pt 2: Seeds, Kits and more!

element14Dave
element14Dave
22 Aug 2015
image
Vertical Farming Design Challenge

image  All About Vertical Farming

image  Overview Video

image  Prizes

image  Terms and Conditions

image  Kit List

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

 

Hey there Vertical Farming Design Challengers!

 

Above is a quick video talking about some updates for the Vertical Farming Design Challenge.

 

As mentioned in the video, please let us know when you have received your seeds in the comments section below. We will ask you all to begin the planting process on the same day once everyone has received their seeds.

 

Why Adriana Lettuce?

 

This species has been selected since it does well indoors and it has a short (48 day) maturity.  They germinate better in cooler conditions (under 75°F/24°C) – ideally between 60°-68°F (15.5-20°C)


Below is a Germination guide from the seed supplier, johnyseeds.com.


image


CULTURE:

Lettuce is hardy and can be planted as early as the soil can be worked. It is a cool weather crop and grows best at temperatures of 60-65°F (15.5-18.3°C). Careful variety selection is important for hot weather plantings. Sow every 3 weeks for a continuous supply of fresh lettuce.


THERMAL DORMANCY:

Lettuce seed can enter thermal dormancy when exposed to high temperatures. Optimum germination results at soil temperatures of 60°-68°F (15.5-20°C). The priming process in pelleted lettuce seeds broadens the temperature range in which the seeds will germinate, overcoming some of their thermal dormancy.


TRANSPLANTING:

Sow in flats, 4 seeds/in., or in 3/4" plug trays, barely covering seeds with fine vermiculite, 3-4 weeks before transplanting outdoors. Shade the flats on sunny, warm days if necessary to keep the soil surface cool, below 75°F (24°C), until germination. If sowing into flats, transplant 1-2" apart into flats, pots, or cell-type containers about 2 weeks later. Harden seedlings by reducing water and temperature for 2-3 days before planting outdoors. Properly hardened transplants can survive temperatures as low as 20°F (-6°C). Transplant iceberg and romaine lettuce 10-12" apart, in rows 18" apart. Other types 8-10" apart in rows 12-18" apart for full size heads or 6" apart for mini heads.


DIRECT SEEDING:

Seeds germinate even at low, 40°F (4°C), soil temperature, but poorly above 75°F (24°C) depending on the variety and seed lot. Sow seeds 1" apart, rows 12-18" apart. Cover seed lightly, about 1/8", and firm soil gently. Thin iceberg and romaine lettuce to one plant every 10-12", other types 8-10" for full size heads or 6" for mini heads. Dry soil must be watered to ensure coolness and moisture, and for uniform germination.


SALAD MIX/BABY LEAF:

Sow in a 2-4" wide band, about 60 seeds/ft.


MT0 SEEDS:

A variety's description followed by MT0-10 indicates that the seed offered for sale has been tested for the presence of Lettuce Mosaic Virus and that no LMV was found in a sample of at least 10,000 seeds. MT0-30 indicates that no LMV was found in a sample of at least 30,000 seeds.


NOTE:

A disease-free test result does not guarantee a seed lot to be disease-free, only that in the sample tested, the pathogen was not found.


DAYS TO MATURITY:

For full-size heads in mild temperatures from direct seeding; subtract 10-14 days if transplanting. Note: Maturity can be 3 or more weeks later in cool weather, and up to 1 week earlier in hot weather.


AVG. DIRECT SEEDING RATE:

For full-size heads (precision seeded): 220'/1,000 seeds, 5,300'/oz., 5.5 oz./acre 2.5" apart in rows 18" apart. For baby leaf: 16'/1,000 seeds, 400'/oz., 6,400'/lb. at 60 seeds/ft.


TRANSPLANTS:

20,000 plants/oz.

 

We've also pulled together a quick guide to planting seed indoors, you can find that here .

  • Sign in to reply

Top Comments

  • sftwrngnr
    sftwrngnr over 10 years ago in reply to m.ratcliffe +2
    True enough, but, as I see it, a critical aspect of the design challenge is the IoT aspect of it, which ostensibly requires the other MCU and its accompanying wireless interface. Not saying I can't have…
  • element14Dave
    element14Dave over 10 years ago +2
    Hey there Vertical Farming US challengers, I have received the 915 Mhz boards from Silicon Labs today, I'll be sending them out via UPS Next Day Air so you get them before the weekend. Sorry for the delay…
  • element14Dave
    element14Dave over 11 years ago +1
    Hello Vertical Farming challengers, We have received a few messages from people that UPS is attempting to collect duties on the seeds coming over to you. We are working to resolve the issue on our end…
  • m.ratcliffe
    m.ratcliffe over 10 years ago in reply to sftwrngnr

    I believe the wording was you must use the supplied MCU, nothing about using other MCU's and the supplied one, so you can start building with any MCU of your choice and use the supplied MCU for a backup monitoring/alarm system.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 10 years ago in reply to sftwrngnr

    No John, I don't think anyone who required a 915MHz kit has received them yet. Dave said he would let us know when E14 had received them from SiLabs and shipped them out to us. No word yet. Getting a little concerned.

     

    I have written control code for the EFM32ZG. I think it wll port pretty easily. But I have no idea what working with the radio will entail.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sftwrngnr
    sftwrngnr over 10 years ago

    Has everyone else received their Silicon Labs wireless starter kits? I have not as of right now.  The rules in the contest were pretty clear, that you can only use the processors provided.  Somewhat difficult to build an IoT system if I in fact have no possible way to connect to the internet.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to m.ratcliffe

    Let me know...

     

    Initial State is a bit pricey now. I got in on an introductory thing so it's not so bad. And I use it for work as well so it's worth it. There are several free Linux hosting sites out there that offer MySQL support. You generally have to implement the LAMP stack yourself and any DB and applications you want. I'm sure there's something like Initial State for free. They were when they were in beta.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • m.ratcliffe
    m.ratcliffe over 11 years ago in reply to RWReynolds

    Thanks Rick, I got the Simply-studio up and running on my linux desktop, Just not had time to really have a look at what I can do with it yet. I will most likley need a bit of help in a week or so when I try to impliment it.

     

    I was hoping for some sort of Cloud Solution for the MySQL, Ive just checked out "initial State" Looks good but a bit pricey, I will read more into it. Good idea to blog it because it could be useful to many.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>