Vertical Farming
  • Challenges & Projects
  • Design Challenges
  • Vertical Farming
  • More
  • Cancel
Vertical Farming
Documents Vertical Farming Design Challenge | Challenger List
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: patkelly
  • Date Created: 28 Jul 2015 9:02 AM Date Created
  • Last Updated Last Updated: 4 Aug 2015 3:11 PM
  • Views 6396 views
  • Likes 8 likes
  • Comments 69 comments
Related
Recommended

Vertical Farming Design Challenge | Challenger List

Many thanks to all who applied for the Vertical Farming Design Challenge - there were a great many imaginative ideas on how best to build an energy efficient, small footprint,  vertical "layered" farm that is a true IoT solution. .
However, we could only have 15 sponsored competitors - and in this instance we've selected:
Ognyan Chikov | Keith Earns | John Henderson | Calla Klafas | Erik Lau | Jose Marques | James O'Donnell | Kowshik Patel | Michael Ratcliffe | Rick Reynoldsôa | Clem Martins | Ajit Singh | Shane Sissons | Joshua Tsai | Srinivasan Kanni Udaiyar |

imageOgnyan Chikov
Bulgaria
Project: Automated Farm
Synopsis:
My technical solution is made of few elements that in collaboration with each other will lead to build a complete system for operating vertical farming. The Solution is not only including software and hardware for automation and monitoring, but a new type of growing surface that will be used rather than overall footprint of the build.
Read Ogynyan's project blogs (tag automated_farm)

imageKeith Earns
United States
Project: Project EDEN
Synopsis:
EDEN uses aeroponic nutrient misting systems to grow indoors, without the need for soil. All self- contained, so no runoff. Vertical farming allows use of lateral space. With fresh produce less can be imported and thrown into the trash. Photosynthetically Active LED spectrum, CO2/pH automation, and humidity control will be active to ensure plants grow in near- optimal conditions.
Read Keith's project blogs (tag project_EDEN)

imageJohn Henderson
United States
Project: Ambient Growth
Synopsis:
The prototype shall incorporate a small scale environmental control module that shall be capable of modulating the ambient growth temperature of the plant growing area such that the plants will successfully grow.  Furthermore, the prototype shall utilize LEDs as grow lights such that the grow period can be extended significantly to optimize growth of the plants. It is also possible that a high voltage generator and grid lattice may be incorporated in the grow chamber to provide for ionization and additional plant growth stimulation.
Read John's project blogs (tag ambient_growth)

imageCalla Klafas
Australia
Project: Aquaponic Salad Garden
Synopsis:
This project aims to develop a design of a small form factor vertical garden that is setup as an easy picking shelf for fresh ingredients for the kitchen of an urban apartment in Sydney.
Read Calla's project blogs (tag aquaponic_salad_garden)

imageErik Lau
United States
Project: The Plant
Synopsis:
The proposed automation system will include methods to regulate pH temperature, water level, power usage, and feed for the fish. We will be able to regulate the system, either through the internet web page or on site computer connection.
Read Erik's project blogs (tag the_plant)

imageJose Marques
Portugal
Project: Modular Farm
Synopsis:
My goal is to develop a simple modular automated system to support indoor plant growing of fruits and vegetables. Simple means anyone with a minimum technological or botanic background should be able to install and operate it. Because it is fully automated, the human factor is minimized and we make sure the plants will have what they need when they need it. The modular approach is very important for scalability. In this way the system will be flexible enough to be used either as a domestic growing system or as an industrial production facility.
Read Jose's project blogs (tag modular_farm)

imageJames O'Donnell
United States
Project: Vertical Hyperponic Farm
Synopsis:
To demonstrate a vertical hydroponic farm, I will create a scale version that will demonstrate many of the required features. This will consist of four sections: water treatment, germination, seedling/microgreens, and nft channels. I will focus on measuring energy, water, nutrient, and other material use while controlling the nutrient solution, temperature, and lighting.
Read James' project blogs (tag vertical_hydroponic_farm)

imageKowshik Patel
India
Project: Cylindrical Farm
Synopsis:
Combining a cylindrical bottom for greater surface area, mystifying nozzle and automation controls. This build will use IoT applications to help increase biomass production in India.
Read Kowshik's project blogs (tag cylindrical_farm)

imageMichael Ratcliffe
United Kingdom
Project: Adapted Greenhouse
Synopsis:
This project will adapt the challenge of connectivity and power efficiency to an already established greenhouse.
Read Michael's project blogs (tag handheld_sensor)

imageRick Reynolds
United States
Project:Vertically Oriented Modular System
Synopsis:
My proposal consists of the design and implementation of a modular hydroponics based, vertically stackable, growing unit and wireless control and monitoring system. The concept of smaller stackable units will allow for small, home-based, installations as well as the ability for unlimited expansion to fully commercial installations. My proposal for this challenge is to build one complete stackable growing unit, a localized wireless control module and a remote wireless master control and monitoring module.
Read Rick's project blogs (tag modular_hydroponics)

imageClem Martins
United States
Project: Hydroponics Using Water Bottles & Control
Synopsis:
This build will be using recyclable materials like waterbottles and egg cartons to grow leafy vegitables. It will also document daily progress of this hydroponic, closed system using grpahs and pictures published on the cloud.
Read Clem's project blogs (tag hydroponic_water_bottles)

imageAjit Singh
India
Project: New Delhi Vertical Farm
Synopsis:
We are building a fully automated, low energy footprint, indoor vertical farm in New Delhi, India. Natural environment in Delhi is characterized by extreme temperatures not conducive for traditional techniques employed in vertical farming - hydroponics and aquaponics. The space we have at our disposal is 1,000 sqaure feet. The space will have artificial smart lighting and air conditioning - through water based coolers, misters, foggers and exhaust fans.
Read Ajit's project blogs (tag new_delhi_farm)

imageShane Sissons
United Kingdom
Project: Ferris Farm
Synopsis:
This project will use a motorized system which will provide light, water, food and air movement. The mechanical design will include a rotating platform with an integrated feeding system.
Read Shane's project blogs (tag mechanical_farm)

imageJoshua Tsai
United States
Project: Solar Farm
Synopsis:
This project integrates solar power technology into a sensor-rich, fully automated hydroponic vertical farming application.
Read Joshua's project blogs (tag solar_farm)

imageSrinivasan Kanni Udaiyar
India
Project:Simple IoT Based Plant, Soil and Water Management System 
Synopsis:
Each of the plant species (vegetable,fruit,herb) chosen will be arrayed up on a wall mountable tray / container(eco-friendly) with soil and necessary manure.The material chosen for the tray/container will be eco friendly or reusable.The supporting material will contain the plant seed, soil and manure.The containers will be mounted on a pipe in order to support DRIP IRRIGATION(efficient water utilisation).Nutrients will be passed on along with the drip irrigation.
Read Srinivasan's project blogs (tag simple_iot)
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • shabaz
    shabaz over 11 years ago +6
    Good luck everyone! Many projects here look extremely interesting. Don't forget the rule that weekly blog content is needed, and of good quality, to stay in the game! It would be a shame for any of these…
  • ravi_butani
    ravi_butani over 11 years ago in reply to shabaz +5
    I have not participated due to lack of time in coming months... But i have hands on experience with EFM32 Giant Gecko Kit as we have EFM32 donated lab by silicon labs in my institute... So Will be happy…
  • sleuz
    sleuz over 11 years ago +4
    I want to welcome all contestants to our Vertical Farming Design Challenge! It was pretty tough to only pick 15 applications among all the great ideas. We at Würth Elektronik are very excited of what the…
  • e14 Contributor
    e14 Contributor over 11 years ago

    Why aren't my blogs going to the vertical farming blog?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to shanesissons

    Maybe I'll pull a Keith Richards and falll out. Now that would make a great video blog!

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Jan Cumps
    Jan Cumps over 11 years ago

    It's nice to see the excitement of the contenders to start with the design. That may be a sign that this is going to be an exercise that will introduce some innovative designs.

     

    I can't wait to see the first things materialize.

    • Cancel
    • Vote Up +2 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shanesissons
    shanesissons over 11 years ago in reply to RWReynolds

    Just remember element14 isn't liable if u get stuck at the top but it would make a good video blog

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • RWReynolds
    RWReynolds over 11 years ago in reply to shanesissons

    But I've already begun germination! image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shanesissons
    shanesissons over 11 years ago in reply to e14 Contributor

    Waiting for confirmation off element14dave and no news on what plants yet they have said there will be a brief in the parcel a few of us think it will be a food based crop but no actual evidence yet let's just hope it's not coconuts

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to e14 Contributor

    Anyone know when the stuff is supposed to get here? Also, has anybody got confirmation about the specifics of our plant choice?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to shanesissons

    White collar anyone? It's like Sherlock Holmes.... but more spy like. Not sure if this is the best place to put that..... Also Legend of Korra?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • shanesissons
    shanesissons over 11 years ago in reply to sftwrngnr

    Very true about the stuff that's out there these days seems like I'm watching people on YouTube that are more interesting than cable TV

    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • sftwrngnr
    sftwrngnr over 11 years ago in reply to shanesissons

    So what's funny Shane,

    Is the other day at work, I happened to see a "inane facts about Gilligan's Island that are too mundane to actually click on, but you're going to anyway" link (not the actual title), and I was thinking very similar thoughts as you. Geek reality tv show with the vertical farm projects of doom on a deserted island... Then I got to thinking... it would probably be way better than some of the mindless drivel that's currently "out there."

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>