Imagine a World Without Cords
  • Challenges & Projects
  • Design Challenges
  • Imagine a World Without Cords
  • More
  • Cancel
Imagine a World Without Cords
Blog It's Alive! Part 002
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 9 Oct 2012 8:14 PM Date Created
  • Views 710 views
  • Likes 1 like
  • Comments 1 comment
  • wireless_power_challenge
  • wp_challenge_one
Related
Recommended

It's Alive! Part 002

COMPACT
COMPACT
9 Oct 2012

External Adapter Power

The bq receiver is designed for an adapter input. This means in addition to being powered wirelessly there is an option to connected an alternate power source.

This could be USB power since it too is 5 volts.

The amount of power available from a USB port is dependent upon the its circumstance. You can have anything from 500mW to 2.5W available.

To ensure that I have 500mA of current available I use USB ports directly from a PC or from a powered Hub with sufficient power capacity.

This is well demonstrated with some USB powered external Hard Disks that require 5 Watts (5V @ 1A ) which have two USB connectors where one is a standard USB plug for communications and power and the other for just power.

 

Here is my test rig with external USB power lead attached (but currently turned off just for the photo).

image

 

I've tested by connecting it up to my notebook PC USB port and it works!

  • Sign in to reply
Parents
  • ssilberhorn
    ssilberhorn over 14 years ago

    Monte... exciting stuff... I can't wait to see your "magic" :-)

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • ssilberhorn
    ssilberhorn over 14 years ago

    Monte... exciting stuff... I can't wait to see your "magic" :-)