Imagine a World Without Cords
  • Challenges & Projects
  • Design Challenges
  • Imagine a World Without Cords
  • More
  • Cancel
Imagine a World Without Cords
Blog It's Alive! Part 017
  • Blog
  • Forum
  • Documents
  • Files
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: COMPACT
  • Date Created: 26 Nov 2012 8:29 PM Date Created
  • Views 950 views
  • Likes 1 like
  • Comments 3 comments
  • wireless_power
  • wireless_power_home
  • wireless_communication
  • wireless_power_challenge
  • wireless_power_charging
  • qi_standard
  • solder_paste
  • wp_challenge_one
Related
Recommended

It's Alive! Part 017

COMPACT
COMPACT
26 Nov 2012

An EAGLE Eye for Detail

Fine Tuning Parts Libraries

I've made plans to produce my own solder paste stencils.

For this I need accurate solder paste masks for the components.

 

The bq51013a part from one of the many EAGLE parts libraries has an incorrect solder paste(tCream) mask - it has a single large rectangle and needs to be divided into 4 separate smaller rectangles.

This can be seen from first PCB layout picture from Part 015.

To most this seems an unimportant issue but it is important because doing it correctly increases the chances of success.

The reason for having 4 smaller rectangles to produce a solder ponds with the right height be compatible with those formed on the smaller pin.

A single large rectangle has a high risk of forming an overly tall solder blob which can throw out the component alignment.

 

Also I've noticed that the parts libraries seem to have inconsistencies between them particularly with the component overlays.

Some have printing over the exposed pads, others are the size of the components others are larger than the components and so on and so forth.

I'll have to select and edit the ones for my PCB to keep them consistent.

 

My First Attempt at a Solder Paste Stencil

Solder paste Stencils are usually made out of staineless steel and there are some organisations that offer Kapton and Mylar substitutes.

This is a picture of my first attempt using self adhesive vinyl. It's not ideal because a single pin divider broke off but it's a great start (and is still useable for this project).

The idea is that the vinyl solder mask is temporarily adhered onto the PCB, the solder paste even spread across it and then the vinyl stencil leaving the desired solder paste deposits.

 

The ruler in the picture is in Centimetres with millimeter graduations to give an idea of the small scale I'm dealing with.

The solder pad sizes are about 0.23mm x 0.7mm.

 

image

  • Sign in to reply
Parents
  • DAB
    DAB over 13 years ago

    Hi Monte,

     

    Have you considered using your 3D printer to make the masks?

     

    It looks like a perfect application for stencils.

     

    Just a thought,

    DAB

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • COMPACT
    COMPACT over 13 years ago in reply to DAB

    My 3D printer is not accurate enough for fine pitch SMD components.

    The thinnest resolution is about 0.15mm (6mil) and where possible I use 0.4mm layers.

    The flex of ABS filaments around tight corners is not great at the best of times.

    Then there's the issue of stranding for a single layer of ABS.

    The usual process to produce a 3D item is to print a 2mm disposable raft.

    This raft holds the work to the platform.

    Peeling a single layer successfully would be unlikely

     

    Cheers

    Very Compact

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • COMPACT
    COMPACT over 13 years ago in reply to DAB

    My 3D printer is not accurate enough for fine pitch SMD components.

    The thinnest resolution is about 0.15mm (6mil) and where possible I use 0.4mm layers.

    The flex of ABS filaments around tight corners is not great at the best of times.

    Then there's the issue of stranding for a single layer of ABS.

    The usual process to produce a 3D item is to print a 2mm disposable raft.

    This raft holds the work to the platform.

    Peeling a single layer successfully would be unlikely

     

    Cheers

    Very Compact