Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Blog 08 Short introduction to dermatology and dermatoscopy using multispectral imaging
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: janisalnis
  • Date Created: 25 Jun 2014 10:23 PM Date Created
  • Views 2697 views
  • Likes 0 likes
  • Comments 9 comments
  • beyond_the_phone
Related
Recommended

08 Short introduction to dermatology and dermatoscopy using multispectral imaging

janisalnis
janisalnis
25 Jun 2014

Previous blog entry:07 Wireless charging of dermatology device "Skimager"

Next blog entry: 09 Raspberry Pi and multispectral LED ring powered from the Qi Wireless Power kit - towards open source dermascope


 

During  the Wireless Power Challange I have implemented wireless charging of skin dermatology device "Skimager". Here I will try to give some medical explanation what this device is doing.

 

Skin cancer melanoma is the fifth most common type of cancer. Dermatologists distinguish different risk groups by age, gender, skin color, sunburn history, hair color, number of nevi (birthmarks), part of the body, personal disease history as well as melanoma occurrence in family. Early detection is an efficient way to diagnose and manage skin cancer.

 

Skin structure

  The epidermis is the top layer of the skin mostly  made  of  flat  cells  called  squamous  cells.  Below  the squamous cells deeper in the epidermis are round cells called basal cells. Cells called melanocytes are scattered among the basal  cells.  They  are  in  the  deepest  part  of  the  epidermis. Melanocytes  make  the  pigment  (color)  found  in  skin.  When skin  is  exposed  to  UV  radiation,  melanocytes  make  more pigment, causing the skin to darken, or tan. Melanin is the primary determinant of skin color.

Melanocytic nevus (nevomelanocytic nevus, nevocellular nevus): benign proliferation of melanocytes, the skin cells that make the brown pigment melanin. Hence, most nevi are brown to black. They are very common; almost all adults have at least one, usually more. They may be congenital or acquired (usually at puberty).

 

Dermis:  The  dermis is  the  layer under  the  epidermis. The dermis  contains  many types  of  cells and  structures,  such as blood  vessels,  lymph vessels,  and  sweat and sebum glands.  Sebum is an oily substance that helps keep your skin from drying  out.  Sweat and sebum reach  the  surface of your skin through tiny openings called pores.


Tumors

  In general, cancers are caused by damage to DNA. Melanomas are usually caused by DNA damage resulting from exposure to ultraviolet (UV) light from the sun. Cancer is an abnormal growth of cell in a human body. Normal cells grow and divide to form new cells as the body needs them.  When normal cells become old or get damaged, they usually die, and new cells take their place. But sometimes this process goes wrong and new cells form when the body doesn’t need them, and old or damaged cells do not die as they should. The buildup of extra cells often forms a mass of tissue called a growth or tumor. Growths on the skin can be benign (not cancer) or malignant (cancer). Benign growths are not as harmful as malignant growths. 


Melanoma is most common skin cancer that can originate in any part of the body that contains melanocytes. Melanoma stages:

0:   The melanoma involves only the top layer of skin. It is called melanoma in situ.
I:    The tumor < 1 mm thick, the surface may appear broken down. Or the tumor is 1...2 mm thick, and the surface is not broken down.

II:   The tumor is 1...2 mm thick, and the surface appears broken down. Or, the thickness of the tumor is more than 2 millimeters, and the surface may appear broken down.

III:   The melanoma cells have spread to nearby lymph node or to tissues nearby.

IV:  Cancer cells have spread to the lung or other organs, skin areas, or lymph nodes far away from the original growth.

 

These tumors have very indistinct margins. By allowing the surgeon to correctly identify the true extent of the tumor, repeat surgery often is decreased.

 

In 2013 I listened to a talk by leading Swedish cancer researcher Dr. Katharina Svanberg. She told that newest studies show that within lifetime human body successfully fights with ca 20 tiny cancer formations that the person does not even notice.

 

 

Dermatoscopy


Dermatoscopy - Wikipedia, the free encyclopedia

Dermatoscopy (also known as dermoscopy or epiluminescence microscopy) is the examination of skin lesions with a dermatoscope.

Dermoscopy cameras usually magnify the image 10 x. Small, inexpensive  hand-held  devices such  as  the DermLite  or DermScope illuminate a skin lesion with polarized light, thus greatly reducing specular reflection. However, diagnosis of the lesions imaged  is  still left  up  to the  physician,  which is subjective  and  therefore can  vary  significantly.

Doctors use so called ABCDE-rule to distinguish benign from malignant spots on skin. A-Asymmetry, B-Border, C-Color, D-Diameter, E- Elevation.

http://www.sun-protection-and-products-guide.com/ABCDE-rule-for-skin-cancer.html

image

Basically, any mole or growth that is CHANGING needs to be checked by a physician.

 

 

Multispectral imaging


Accuracy of the diagnosis also decreases for non-expert physicians who do not specialize in melanoma detection. Furthermore, the use of white light does not allow for accurate depth and chromophore analysis. Multispectral imaging provides additional depth and chromophore information and computer aided analysis of dermoscopy  images can be more objective.

 

  • Ultraviolet wavelength causes skin fluorescence in longer wavelength. One can measure fluorescence parameter (malignant). Ultraviolet and blue wavelengths penetrate only ski surface layer.
  • Infrared wavelength penetrates skin up to 1.5 mm deep. Nevus is visible in blue but in infrared it is practically not visible. This means that it is on the skin surface and not deeply in the tissue.
  • All nevi show increased eritrema (blood perfusion redness) index meaning that all pathologies are having higher blood perfusion.
  • Bruises show increased bilirubin index. Bilirubin has strong absorption in blue.
  • Melanin shows increased absorption at blue that gradually decreases through green, red and infrared colors.

 

At the University of Latvia non-invasive melanoma diagnosis using multispectral imaging are done in collaboration with the hospital and optical methods were verified by histological methods. In order not to upset the tested person name “Melanoma index” is replaced by “C43 indicator”.

Below are absorption spectra of skin chromphores and LED emission spectra.

image

There are 4 LEDs for each wavelength to make illumination uniform. Light from LEDs is sent through a linear polariser sheet. In front of camera is another polariser sheet oriented at 90 degrees. This is a powerful method to eliminate direct reflection from the surface. Skin under investigation is illuminated for 1 s with each color and photo is taken.

image

Below is image obtained in white light, red, green, blue, infra-red and ultraviolet illumination.

image

Such diagnostic information can be extracted and mapped on the original photo:

  • Hemoglobin index R/G    H=I660/I545 nm
  • Bilirubin index B/R           B=I450/I545
  • Melanin index G/R/IR     M=I545/I660/I940

Picture below shows white light image and maps of Hemoglobin H, Bilirubin B, Melanin M for a) hemangioma, b) papilloma (wart), c) blood vessels.

image

Results are published in a recent article:

J. Spigulis,  U. Rubins, E. Zaharans, J. Zaharans, L. Elste,
A device for multimodal imaging of skin
Proc. SPIE 8574, Multimodal Biomedical Imaging VIII, 85740J (March 13, 2013); doi:10.1117/12.2003510

 

Nice South Korea OptoBioMed  promotional video about a similar working device:
https://www.youtube.com/watch?v=5Lpb6w2kotQ

 

 

Next blog entry: 09 Raspberry Pi and multispectral LED ring powered from the Qi Wireless Power kit - towards open source dermascope

  • Sign in to reply

Top Comments

  • michaelkellett
    michaelkellett over 12 years ago +1
    Am I missing something here - what does this have to do with Wireless Power (or even E14) ? MK
  • mcb1
    mcb1 over 12 years ago in reply to michaelkellett +1
    I think it explains the end game in Janis's Wireless Challenge project ... but a personal blog might have been better. mark
  • michaelkellett
    michaelkellett over 12 years ago +1
    Hello Janis - I understand why you posted it now - the way E14 blogs work is that they get put up on the front page as single entitites and it isn't at all obvious how they might fit into a series of blogs…
  • janisalnis
    janisalnis over 12 years ago in reply to michaelkellett

    Thanks for a good tip to insert links to previuos and next blogpost.

    For some time I was thinking to make just one long blog entry. It is bettter to keep smaller blog entries because it makes commenting easier.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to michaelkellett

    MK

     

    Sometimes the blog might be in different areas.

     

    I sometimes resort to looking at their profile to see their content

    Yours shows no blog post authored but you participated in these.

    image

     

    I had to keep adding the links in mine and sometimes going back and adding them to existing ones.

     

    mark

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelkellett
    michaelkellett over 12 years ago in reply to janisalnis

    I think the best solution would need to come from E14 making a change to the website so that when you look at  a blog it offer you a list of the blogger's other blogs to choose from. Your number's will help ( I didn't know until today that you had 7 other blogs already !).

     

    MK

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • janisalnis
    janisalnis over 12 years ago in reply to michaelkellett

    I numbered the blog entries. Hope this helps.

    Alternative would be to copy/paste everything into one very long blog unit.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 12 years ago

    Hi Janis,

     

    Very interesting.  My mom gets regular checkups and has had over a dozen lesions removed so I well understand the need for keeping the unit on full charge and I agree that wireless recharging can go a long way to achieve this requirement.

     

    Look forward to your next post.

     

    DAB

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
>