Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Blog Shaky hands and precision soldering do not mix
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: aemarconnet
  • Date Created: 14 Apr 2014 2:21 PM Date Created
  • Views 3099 views
  • Likes 1 like
  • Comments 13 comments
  • wireless_power_challenge
  • beyond_the_phone
Related
Recommended

Shaky hands and precision soldering do not mix

aemarconnet
aemarconnet
14 Apr 2014

For prototyping purposes i was hoping to try my hand at soldering some leads to a super-cap charger from TI. Unfortunately the package is a 16VQFN and my feeble attempt at tacking leads onto these 0.2MM pitch pads did not end well. I think the photo below gives a good indication of of the size of the package. (keep in mind my hands are not HUGE)

 

image

 

After a little over an hour of effort trying to solder leads to this package i gave up. I will have to build a breakout PCB for this, but it seems my solder paste is expired and i will need some more single-sided, copper-plated, PC board. The order is placed on amazon and i should have them soon this week.

 

Anybody have recommendations for soldering these small packages? The only re-flow i have done is repair to electronics like the XBox 360 GPU (Red Ring of Death).

 

Wish me luck!

Alex

  • Sign in to reply

Top Comments

  • DAB
    DAB over 12 years ago +2
    Just wait until your eyesight fails and you get arthritis in your hands. That's when you know its time to let others do these kinds of things. DAB
  • mcb1
    mcb1 over 12 years ago in reply to DAB +1
    The eyesight is enough .. let alone adding shaky hands or arthritis. I had to replace a smd chip the other day, and despite having the appropriate hot air smd tool, it was still strange to rely on heating…
  • michaelwylie
    michaelwylie over 12 years ago +1
    I solder almost exclusively under a microscope because of stuff like this. Advice for soldering leads to that? It's really ambitious and it makes me anxious just to think about it. I can just imagine getting…
  • aemarconnet
    aemarconnet over 12 years ago in reply to michaelwylie

    Why yes indeed you are correct, it is a "Tassimo" and it is one of my most important tools. Something has to keep me going when projects are on a roll. On the flip side, If you were to look in the top right drawer of that desk you would find a bottle of scotch for when projects just aren't working.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago in reply to aemarconnet

    Hahaha, is that a coffee maker? Love it! All the essentials.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aemarconnet
    aemarconnet over 12 years ago in reply to michaelwylie

    It works well, i was actually quite surprised with the quality of my X-Tronic solder station/re-flow station, i bought it a few years back and it has been good to me. i think i only spent ~70 USD on the unit and it came with that lamp as well as spare heating elements and a variety of solder and reflow tips.

     

    Unfortunately, the rest of my setup is missing right now. I'm still living out of boxes (when it comes to my basement office). If you look in the background you can see some of the units i need to sort through. i have a veritable wall of boxes (not shown) 30 feet long and 2-3 deep. But i did manage to find my multimeter and soldering iron. So I've got the bare essentials.

     

    image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • michaelwylie
    michaelwylie over 12 years ago

    That's a nice setup, I like it. You've got enough there to be dangerous (it's a North American expression). 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • aemarconnet
    aemarconnet over 12 years ago in reply to michaelwylie

    Thanks Michael,

     

    I definitely appreciate the advice!  I know attempting to solder with an iron was fool-hardy but I just couldn't find my copper clad board, and i thought to myself: "Boy, I've got a half-decent iron with an ultra-fine tip, why not give it a shot?"....Looking back, not such a great idea

     

    I've got a re-flow station built into my soldering iron (which is probably where some of the confusion came from). I was using the high-magnification portion of the glass and i simply don't have the finesse or practice that i would need to pull it off.

     

    image

     

    copper board should have shipped by now, so i should have it by Wednesday.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>