Products
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
Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Blog Smart ID Card #5
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: kevjose
  • Date Created: 27 Jun 2014 7:28 AM Date Created
  • Views 1825 views
  • Likes 0 likes
  • Comments 6 comments
  • e-ink
  • wireless_power_challenge
  • beyond_the_phone
  • qi
  • arduino
Related
Recommended

Smart ID Card #5

kevjose
kevjose
27 Jun 2014

Well. It seems I have missed the deadline for project completion.

 

Present state of the project:

1) Soldering the circuit boards is complete

2) Communication between all the Arduinos verified to be working individually. (Wireless communication, I2C)

3) Verified that the ID side Arduino boots fast enough (on wireless power) for the application to be practical

4) Most of the code written but still in pieces

 

Probably the messiest "proof-of-concept" ever:

image

The circuit boards:

image

I have decided to use Arduino Uno instead of Arduino Yun with the stationary module because Arduino Yun has issues powering the wireless chip. I will most probably require a separate 3.3V regulator to provide adequate current to the chip with a Yun.

 

While the project is probably ineligible to be judged for the challenge, I would still like to complete it in the next two days (weekends coming up).

 

For now, I will write a program on Processing which will find and parse the data relevant to the unique ID.

 

I would like to thanks Element14, Würth Elektronik and all the community members for making my FIRST RoadTest Challenge possible and this enjoyable. I also sincerely apologize for my inability to complete the project in time.

 

Thank You

Kevin Jose

  • Sign in to reply
Parents
  • mcb1
    mcb1 over 12 years ago

    Probably the messiest "proof-of-concept" ever:

    I've seen worse.

     

    It would be great to see your completed project, and shows you are committed to the task.

     

    Most of the 3v3 regulators are low power, and Terry King has some notes about it and solutions here.

    http://arduino-info.wikispaces.com/Nrf24L01-2.4GHz-HowTo

     

    Mark

    PS I still haven't heard if my larger displays have come in stock ... so glad I decided not to wait.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • kevjose
    kevjose over 12 years ago in reply to mcb1

    I will take this project to its logical conclusion. I only wish I had managed time better.
    Did go through Terry King's notes but adding a cap did not seems to make a lot of difference for me on the Yun. (Well, I could be wrong but it does make sense because the Yun is running an AVR and a linux cumputer on 5V, 500mA suppply)

     

    Well, I wont speak too soon but you are looking pretty good on the polls image Congratulations on the project.
    I should get back to coding!

    Thanks for all the help.

    Kevin.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • kevjose
    kevjose over 12 years ago in reply to mcb1

    I will take this project to its logical conclusion. I only wish I had managed time better.
    Did go through Terry King's notes but adding a cap did not seems to make a lot of difference for me on the Yun. (Well, I could be wrong but it does make sense because the Yun is running an AVR and a linux cumputer on 5V, 500mA suppply)

     

    Well, I wont speak too soon but you are looking pretty good on the polls image Congratulations on the project.
    I should get back to coding!

    Thanks for all the help.

    Kevin.