Wireless Power - Beyond the Phone
  • Challenges & Projects
  • Design Challenges
  • Wireless Power - Beyond the Phone
  • More
  • Cancel
Wireless Power - Beyond the Phone
Documents 5W Load Schematic
  • Blog
  • Forum
  • Documents
  • Files
  • Events
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: mcb1
  • Date Created: 29 Mar 2014 10:35 AM Date Created
  • Last Updated Last Updated: 8 Oct 2021 7:50 AM
  • Views 3114 views
  • Likes 0 likes
  • Comments 13 comments
Related
Recommended

5W Load Schematic

For the Beyond the Phone challenge I have been waiting for my kit to arrive.

 

After some Customs and UPS delivery delays, it arrived.

 

One concern I had was that since the kit was dispatched from the USA, the power plug and voltage may not suit our angled pins and 230v AC.

imagerather than the what we usehttp://nz.element14.com/productimages/farnell/standard/2254795-40.jpg

 

 

So as I feared the kit includes the wrong pings, but the voltage is 110/230 so it will fit with a travel adaptor

http://media2.dicksmith.co.nz/media/catalog/product/cache/3/small_image/150x/9df78eab33525d08d6e5fb8d27136e95/m/7/m7_dsnz_m7308_v0_4105.jpg which I thought we had ... but I can't find it if we do have one laying around.

 

 

Option 2

I checked and I did have some other 5v USB outlets that claim to be 1.2A but in reality the voltage tends to fall to the lower end of an acceptable USB voltage.

 

Placing the Receiver onto the unit, D5 flashes but not much else.

A bit of digging around in the Tx spec sheet suggests it flashes when transfer is occurring (I would hate to use that output as the Buzzer as the chip data suggests)

 

The Rx or part of the load gets warm, but no pretty red LED's.

 

Since there are 4 parts to this kit, establishing where the problem lays is a process that needs to be done.

Its no different to sorting out whats wrong with your car ... narrow it down an bit and you have a better chance of fixing it.

 

POWER

Its always a good idea to see if you have power.

TI have placed labelled test points on the kit that you can get a meter onto  ....well done.

The meter verified there was 5v which dropped to 4.8 or so, but when D5 flashed (ie when the load came on) so that's not the issue.

 

Jumpers

Try to establish what jumpers should be where is a little hard.

The images are not quite big enough to be very clear, and the smallish image shows where the jumpers should be if the LED load isn't in place .... but does the load board emulate this.?

 

Document http://www.ti.com/lit/ug/sluua44a/sluua44a.pdf gives the settings which showed JP6 needed to be shifted to the Fixed position, as per the image copied from the User guide

http://www.we-online.de/web/en/index.php/show/media/07_electronic_components/produkte_3/wireless_power/Wireless_Power_Kit_Solution.pdf

 

 

   hard to see but is in the middle of the board and should be on the two lower pins.

Fullscreen contentimage_52538.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

Looking at the Load board three of the zero ohm resistors have been removed (R2, R3, and R6) and the flux residue suggests this is post production.

The remainders emulate the jumper settings shown (as if the LED board wasn't used) and these match the spec sheet.

 

The TX board has placeholders labelled JP1 and JP2 BUT these aren't jumpers they are connections for Temp sensor and Ext LED.

This annoys me since the receiver uses JP for jumpers and plain J for connectors, yet the Tx board uses both for connectors ...

Both items find themselves used as a pair so it stands to reason to use the same terminology.  ..... more documentation checking required Mr TI.

 

Voltages

Some of the TI documents for this kit and receiver refer to using 19v going into the TX.

Clearly the cut and paste failed to pick it up, as the transmitter markings show 5v, and some of the other documents also state 5v ....so Mr TI, you might need to review your documentation and stop confusing the buyers.

 

Having established that its 5v In and 5v OUT to the load, the next check was am I getting that.

A quick check with a meter showed that 5v give or take some fluctuations was being generated at the output of the receiver unit with the load attached, but still no red leds.

 

LED Load Board

I tried searching for some information on the board PMP8603 Rev A, but alas I failed.

I got a nice picture which detailed some of the parts used, and that's about it.

 

The board has a very nice inductor and some connectors and leds.

Checking the Leds showed they all work or illuminate, and feeding 5v into the Vin and Gnd resulted in nothing.

 

Looking at the underside and comparing the picture

Fullscreen contentimage_52539.html Download
<html><head><title>Jive SBS</title></head>
<body><font face="arial,helvetica,sans-serif">
<b>Error</b><br><font size="-1">
An general error occurred while processing your request.
</font></font></body></html>

 

My board seems to have C3 populated, which is in parallel with C2.

 

There are 4 groups of 11 LEDs in series and from the spec sheet, the Fb (voltage) is 1.9v meaning that 5v wont light them up.

The chip has to boost the voltage to around more than 20v before passing thru a 798 ohm resistor.

 

I could only measure 7.6v out of U1 (the marking is SF98) which I can't find any information for.

I assume its a booster converter and certainly is wired that way.

 

So until I can identify the boost IC and replace it, my LED's won't light.

 

 

Verification

If anyone would care to check the jumper settings, and the voltage being delivered to the load board, I'd be grateful.

If Wurth could provide the schematic that would also be useful.

 

Mark

 

edit 05 Apr 2014.

I have obtained a travel adapter and tried using the supplied power pack, with the same results (ie no LED's) and voltages in the 6.5-7 v instead of the 20 odd volts.

Hendrik has kindly provided the link to the converter chip.

My board has an extra capacitor at C3 which shouldn't cause an issue as its on the output, however a schematic would prove very useful.

  • wireless_power
  • beyond_the_phone
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • hlipka
    hlipka over 12 years ago in reply to mcb1 +1
    See this images for the voltages I measured: community.element14.com/.../contentimage_5F00_178659.html (all voltages are references to ground - I used J2 while the board was on the receiver). Regarding…
Parents
  • hlipka
    hlipka over 12 years ago

    Regarding the confusion about the 19V input: the user guide for the receiver EVM refers to another transmitter board (called bqTESLA, equipped with a bq500210). This is stated right in the description of the test setup. The kit we got is combined by Würth, not by TI. But maybe the docs could clarify that better nonetheless.

    Oh, and the converter on the LED board seems to be a LMR64010 from TI (the marker is actually 'SF9B'). I suggest you verify that nothing else is amiss on this board before you replace it...

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to hlipka

    Hendrik

    Thanks for clarifying the converter IC, the 8 and B look very similar ...

     

    I wonder if someone could check the voltage that appears at any of the vias when the leds are on.

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • mcb1
    mcb1 over 12 years ago in reply to hlipka

    Hendrik

    Thanks for clarifying the converter IC, the 8 and B look very similar ...

     

    I wonder if someone could check the voltage that appears at any of the vias when the leds are on.

     

    Cheers

    Mark

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • hlipka
    hlipka over 12 years ago in reply to mcb1

    See this images for the voltages I measured:

    Fullscreen contentimage_178659.html Download
    <html><head><title>Jive SBS</title></head>
    <body><font face="arial,helvetica,sans-serif">
    <b>Error</b><br><font size="-1">
    An general error occurred while processing your request.
    </font></font></body></html>
    

    (all voltages are references to ground - I used J2 while the board was on the receiver).

    Regarding the Jumpers:

    • JP1=LOW
    • JP2=LOW
    • JP3=DIS
    • JP4=OUT
    • JP5=unused
    • JP6=ADJ

    (all are either on default, or like they are set by the zero-ohm resistors on the LED board)

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mcb1
    mcb1 over 12 years ago in reply to hlipka

    Hendrik

    Thanks very much for that.

    I'll do some checking.

     

    Mark