element14 presents
  • Challenges & Projects
  • More
element14 presents
e14 presents blogs Build Inside the Box - Doremino #1 | Concept
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: embedded_sergey
  • Date Created: 7 May 2021 11:14 PM Date Created
  • Views 1637 views
  • Likes 1 like
  • Comments 2 comments
  • starwars
  • buildinsidethebox
  • arduinomusic
  • build inside the box
  • arduino
  • bitb
Related
Recommended

Build Inside the Box - Doremino #1 | Concept

embedded_sergey
embedded_sergey
7 May 2021

Hi, everybody!

 

First of all, thanks a lot to the organisers who gave me the opportunity to participate for free!

Second, I failed to get it done it time. The box was delivered two weeks ago and it coincided with my exam session in college (actually, the last exam was today).

 

But there are good news too: I have finally found the idea that I am able and wish to realise with my limited skills of a first-year student. I will first introduce what inspired me and then present the actual concept. The realisation of this project will be done during the summer as everything is new for me.

 

That's what I have recently done playing around with Arduino. The roots of the Build Inside the Box project are from here.

 

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

 

The beauty of this ugly instrument is that everyone can play it regardless of a player's musical education and skills. So, I decided to go further with that and design a musical instrument for educational purposes based on all the components I found in the Box:

  1. Arduino MKR Zero + SD card represent an ideal duet for fast processing and storing music samples.
  2. OpAmp (MCP604) is a necessary component for an electronic musical instrument.
  3. two VL51L1X are used as sensors defining a note/a chord based on the distance between them and hands (the closer a hand to the sensor, the lower a tone).
  4. OLED display shows an instrument/sample that is in use now.
  5. transmissive sensor (TCST1103) is a nice component for making an encoder to select a musical instrument/sample on the display.
  6. temperature sensor is used for some sound effect, like a delay or a reverb (the higher the temperature, the stronger a sound effect).
  7. 5V power bank will allow to have a standalone musical instrument.
  8. Wago connectors for loudspeakers

 

What I need to get:

  1. a bunch of resistors and caps to amplify of an input signal
  2. two 5V-loudspeakers
  3. several buttons for UI control

 

Working principle of the device:

The name of an accord (left hand) and a note (right hand) are displayed on the screen based on the distance between VL51L1X and a hand. So, the user may not only intuitively play, but also learn musical theory behind. There won't be flexible tones, only fixed notes and chords for each musical samples. One sample is designed to play one popular melody. Thus, a user will not only will have fun with the instrument, but can also learn musical theory directly on practice.

 

Next things to do:

  • connect VL51L1X to Arduino MKR
  • connect MCP604 to Arduino MKR and a speaker using Wago221
  • test the working principle
  • Sign in to reply

Top Comments

  • mayermakes
    mayermakes over 5 years ago +1
    I would have loved to see your take on the box in full, but life tends to get in the way sometimes. Either way good rendition of the imperial march, the crescendo is fitting. When you get it done please…
  • embedded_sergey
    embedded_sergey over 5 years ago in reply to mayermakes

    Thank you Clemens for the feedback!
    Yes, it is just an idea, but I will realise it during the summer and post my progress step by step.

     

    P.S. Other participants have showed so much progress over a such short period. I am really proud of them! Hope to reach that level too and become a real makerimage

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 5 years ago

    I would have loved to see your take on the box in full, but life tends to get in the way sometimes.
    Either way good rendition of the imperial march, the crescendo is fitting.
    When you get it done please post it on here so we can See what you came up with!