element14 presents
  • Challenges & Projects
  • More
element14 presents
e14 presents blogs Project QuickShot Arduino Sketch
  • Episodes
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: airbornesurfer
  • Date Created: 8 Feb 2019 1:36 PM Date Created
  • Views 721 views
  • Likes 2 likes
  • Comments 0 comments
  • project quickshot
  • project quick shot
  • arduino_tutorials
  • code
  • arduino
  • air mouse
  • gesture mouse
Related
Recommended

Project QuickShot Arduino Sketch

airbornesurfer
airbornesurfer
8 Feb 2019
image
NES Zapper on RetroPie

element14 presents  |  AirborneSurfer's VCP Profile |  Project Videos

 

For Project QuickShot, I essentially wrote a gesture-controlled "airmouse" for the ATmega32u4 on the Adafruit featherboard. Here is the final version of the sketch.

 

//*****************************************************
//Project QuickShot v1.0
//Arduino-driven Light Gun Emulator for LCDs
//Jan 11, 2019
//
//Matthew Eargle
//Element14 Presents
//element14.com/presents
//AirborneSurfer Productions
//airbornesurfer.com
//
//Based on code by Jim Lindblom
//
//*****************************************************
// The SFE_LSM9DS1 library requires both Wire and SPI be
// included BEFORE including the 9DS1 library.
#include <Wire.h>
#include <SPI.h>
#include <SparkFunLSM9DS1.h>
#include <Mouse.h>

LSM9DS1 imu;

#define LSM9DS1_M  0x1E // Would be 0x1C if SDO_M is LOW
#define LSM9DS1_AG  0x6B // Would be 0x6A if SDO_AG is LOW
const int mouseButton = 10;


//Refresh rate between polling intervals, lower is smoother movement
#define REFRESH_RATE 1
static unsigned long lastRefresh = 0;

void setup()
{

  Serial.begin(115200);
  pinMode(mouseButton, INPUT);
  Mouse.begin();

  // Before initializing the IMU, there are a few settings
  // we may need to adjust. Use the settings struct to set
  // the device's communication mode and addresses:
  imu.settings.device.commInterface = IMU_MODE_I2C;
  imu.settings.device.mAddress = LSM9DS1_M;
  imu.settings.device.agAddress = LSM9DS1_AG;
  // The above lines will only take effect AFTER calling
  // imu.begin(), which verifies communication with the IMU
  // and turns it on.
  if (!imu.begin())
  {
    Serial.println("Failed to communicate with LSM9DS1.");
    Serial.println("Double-check wiring.");
    Serial.println("Default settings in this sketch will " \
                   "work for an out of the box LSM9DS1 " \
                   "Breakout, but may need to be modified " \
                   "if the board jumpers are.");
    while (1)
      ;
  }
}

void loop()
{
  digitalWrite(mouseButton, HIGH);

  int clickState = digitalRead(mouseButton);
  // Update the sensor values whenever new data is available
  if ( imu.accelAvailable() )
  {
    // To read from the accelerometer, first call the
    // readAccel() function. When it exits, it'll update the
    // ax, ay, and az variables with the most current data.
    imu.readAccel();
  }

  // if the mouse button is pressed:
  if (clickState == LOW) {
    // if the mouse is not pressed, press it:
    if (!Mouse.isPressed(MOUSE_LEFT)) {
      Mouse.press(MOUSE_LEFT);
    }
  }
  // else the mouse button is not pressed:
  else {
    // if the mouse is pressed, release it:
    if (Mouse.isPressed(MOUSE_LEFT)) {
      Mouse.release(MOUSE_LEFT);
    }
  }

  if ((lastRefresh + REFRESH_RATE) < millis())
  {
    moveMouse();

    lastRefresh = millis();
  }
}

void moveMouse()
{

  // Now we can use the ax, ay, and az variables as we please.
  Serial.print("Move X,Y: ");
  int xMove = ((imu.calcAccel(imu.ax) * 10));
  Serial.print(xMove);
  Serial.print(", ");
  int yMove = ((imu.calcAccel(imu.ay) * -10));
  Serial.print(yMove);
  Mouse.move(xMove, yMove, 0);
  Serial.println();
}