element14 presents
  • Challenges & Projects
  • More
element14 presents
Clem's Massive Hoarding Problem make magic magnetic devices yourself by learnign from the Hoard! - Clems massive hoarding problem
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: mayermakes
  • Date Created: 19 May 2024 12:41 PM Date Created
  • Views 1567 views
  • Likes 6 likes
  • Comments 8 comments
  • clems massive hoarding problem
  • magnets
  • magnetic base mount
  • magic
Related
Recommended

make magic magnetic devices yourself by learnign from the Hoard! - Clems massive hoarding problem

mayermakes
mayermakes
19 May 2024

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Among the Hoard of many makers are seemingly magical devices.
this tool holder has amagnetic base that can be switched on and off with a switch. there are no electronics at play even thought the switch looks like it.
There is no electromagnet or other high tech magic at works it is a simple physical principle that does all the heavy lifting ( got it?).

When looking closely at how the device works we can recreate the mechanism and use it in our own projects.
The yellow 3d print in the video is part of an upcoming element14 presents video and it uses the same working principle to tightly lock together two plates, but also with almost no force it can be unlocked and taken apart. no fasteners or electromagnets needed.

the trick is a clever alignment of the magnetic fields. the magnets are evenly spaced and 3 of them face with the north pole up, while only one has the south pole orientated upwards.
this configuration means that there is only one position where the plates can have all magnets attract there counterparts in the other half of the mechanism.

by aligning them correctly we can lock them together magentically, but if only one of them is not aligned this pair will repell an therefore lift the plate unevenly which in turn forces the other aligned magnets further apart making the bond so week it is not noticeable when you lift the device. Because the magnetic filed s act perpendicular to our turning axis it is also very easy to turn the plate to align or misalign the magnets, which is exactly the same principle the switch on the commercial magnet base uses.

next time you were supposed to throw a thing out...make sure you learned everything it has to offer from it first.

  • Sign in to reply
Parents
  • DAB
    DAB over 2 years ago

    Nice post Clem.

    It is always fun to play with magnets.

    By the way, did I ever tell you how my new theory explains how permanent magnets work?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 2 years ago in reply to DAB

    Can´t wait to hear your theory

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago in reply to mayermakes

    In my book Reverse Engineering the Universe, I introduced the idea that what we call electricity is actually photon flow at the atomic level.

    When you look at the atomic configuration of atoms in magnets, you get an interesting structure where five or six atoms form a back to back pyramid structure.

    When you create this structure in the lab or in a falling meteor under a magnetic field, you set up a flow of photons around the base of the pyramid structure that is perpendicular to the magnetic field.

    Once the atoms solidify, the flow of photons is maintained around the structure, thus generating the same magnetic field used when the structure was being formed.

    If you think back to the "Domain" theory for magnets, each of these atomic structures can replace each domain so that you get a permanent magnet that is stable until you either remelt the material or you destroy the structure. The more evenly distributed these structures are, the stronger the overall magnetic field.

    When you introduce rare earth elements into this structure, they contribute more photons to the flow, thus increasing the resulting magnetic field.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • DAB
    DAB over 2 years ago in reply to mayermakes

    In my book Reverse Engineering the Universe, I introduced the idea that what we call electricity is actually photon flow at the atomic level.

    When you look at the atomic configuration of atoms in magnets, you get an interesting structure where five or six atoms form a back to back pyramid structure.

    When you create this structure in the lab or in a falling meteor under a magnetic field, you set up a flow of photons around the base of the pyramid structure that is perpendicular to the magnetic field.

    Once the atoms solidify, the flow of photons is maintained around the structure, thus generating the same magnetic field used when the structure was being formed.

    If you think back to the "Domain" theory for magnets, each of these atomic structures can replace each domain so that you get a permanent magnet that is stable until you either remelt the material or you destroy the structure. The more evenly distributed these structures are, the stronger the overall magnetic field.

    When you introduce rare earth elements into this structure, they contribute more photons to the flow, thus increasing the resulting magnetic field.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • mayermakes
    mayermakes over 2 years ago in reply to DAB

    interesting, where could I find that book?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • DAB
    DAB over 2 years ago in reply to mayermakes

    Lulu.com.

    Search for my name or the title.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • mayermakes
    mayermakes over 2 years ago in reply to DAB

    haha... lulu = childrens name for pee in german.
    Iĺl take a look at that loo.