element14 presents
  • Challenges & Projects
  • More
element14 presents
Off-Grid MakerShop Building an off grid Maker Shop - The idea, the dream
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join element14 presents to participate - click to join for free!
  • Share
  • More
  • Cancel
Group Actions
  • Group RSS
  • More
  • Cancel
Engagement
  • Author Author: KalebTheMaker
  • Date Created: 12 Oct 2022 3:38 PM Date Created
  • Views 3779 views
  • Likes 14 likes
  • Comments 22 comments
  • homestead
  • diy
  • solar power
  • off-grid
Related
Recommended

Building an off grid Maker Shop - The idea, the dream

KalebTheMaker
KalebTheMaker
12 Oct 2022

Hello and welcome to this new blog topic where I will post my journey through building an off-grid maker shop! There are several projects that need to be completed before I can build the shop, and that is what much of this blog series will be about. Here is a preliminary list of all the projects that will happen (with more added as time goes on, and not in order)

  • Large Solar Array (Probably in the range of 8-10kw, with 600Ah @ 48v of battery storage)
  • 1000' of large AWG wire run from power generation to shop/house
  • Micro Hydro power generation (There is a year-round creek through the property, and a seasonal creek with a waterfall)
  • Low power monitoring dashboard (Bank of LED's and switches rather than LCD screens to monitor valves, tanks, solar etc.)
  • Solar Monitoring Stations (Solar powered Arduino/Pi's for running sensors on different applications)
  • Mesh Network and or back-haul point to point network for above monitoring stations
  • Water Tank Level Sensors (These will be designed and fabricated. Total of 8 2500g tanks to monitor)
  • Local Voice Assistant (Possibly MyCroft - another interface to all available data from sensors)
  • Smart Home hub (Homeassistant?)
  • Water pumping Station & Automation (Need to pump from spring tanks to seasonal well tanks when they are low. solar, batteries, pump & automation)
  • Voltage and Current Sensors (For solar input, battery input/output)
  • Gate opener interface (Commercial gate opener, but possible LoRA remote, notifications at the house/shop of proximity/open. Motor Controller, web interface)
  • State of Charge Sensors (Battery Banks)
  • The Shop (40x80 steel building)

The Dream

This has been my dream for more than 10 years. To move away from the city and get back to my home county where I could build a home and dream shop to work and live. I grew up in a rural community and worked there for much of my adult life. I moved to a larger city for about 12 years for work and had some fun, made friends, and did quite a few really cool projects, but as time went on I realized I wanted to be in a smaller community with some property and my own shop. Living in the city, I had a decent home which was quite expensive, and had to rent shop space which was also expensive. The house just didn't have room for everything. That got to be too much, my kid was raised and out of the house and then COVID hit and I knew I wanted to get out of the city. I sold that home, packed up my shop, and rented a shop in a small town in my home county for less than I was paying for just my house. I lived in a 20x20 room with no insulation and a bathroom that was outside 200' away from the apartment. I have been living there for about 18 months while looking for a property where I could build this dream.

The Property

Over those 18ish months, I probably looked at 30-35 different properties. My requirements were some flat land for development, grid power, water and septic. From there I would develop what I need. I could find plenty of those properties, but almost none of them had much flat land for development. They were 10-40 acres with maybe .25ac of flat land to develop total. Nothing was meeting my requirements and the search was beginning to be a drag. 

One day a property came up in my search and I almost dismissed it because it was off-grid - No power, water, or septic from utility, no phone lines, no cable - nothing. But... It was only 15 minutes from town, only 2 miles of dirt road, and more water developed on the property than I could know what to do with. On top of that, it had a nice bathroom, a septic system, and a small cabin. I fell in love with it, negotiated like crazy, and got a really good deal on it. 

Its mine now and its called "Bonesnapper Ridge" (Named after my favorite cat Bonesnapper). Take a look at this map that I made so you can see where everything is, and where the new projects are proposed.

image

The Projects

Above is a preliminary list of projects that need to be done. I want to build as many of these as possible with as much open hardware and open-source software as I can manage. It may make sense to go commercial where the application is critical, such as solar power. But I will definitely take into consideration the company and its use of open-source in its solution.

In addition to the projects above, there are several more mundane projects that need to be done:

  • Quick remodel on the cabin so I have a place to live (Nearly done at the time of this post)
  • Install two shipping containers & build a roof over them so I have a place to move my shop tools. (Containers are there, and need to be leveled)
  • Move a mountain (clear trees and flatten out some space for the shop building pad) (90% complete at the time of this post)
  • Build a small temporary solar solution for minimal power. (Complete. Needs more panels, and relocation of panels.)
  • Build a large custom desk in the house so I have a place to sit and write these blogs and work on projects. (Computer, electronics, and fabrication stations)
  • Fireplace install (It's going to get cold!)

I won't bore you with these mundane projects (unless you want me to, let me know!), but I will be posting regularly on the main projects at the top of this post, and hopefully, make detailed videos of some of them.

The projects that have the highest priority right now are completing the mundane tasks so I can finish moving up there, Gate Opener/Closer, Large Solar Array, Micro Hydro, LED Monitoring Station, Tank Monitoring, and Automation.

Current Status

I've been at the property for almost two months now. I hired a guy to do a bunch of dirt work to clear space for the shop pad, and installed a small 200w solar power system so I can work up there. Starlink is installed, so I have really great (better than I have had at the rental) internet. I have done a remodel of the cabin so it is *mostly* livable, walls, floor, and ceiling remodeled. There is still no kitchen, plumbing, or electrical wiring in the house. But I am just pretending like I am camping up there. I am living up there full-time now and so far its been amazing!

That's it for now, I'll post thoughts and ideas, projects as they are being worked on, and most likely posts asking for assistance from all of you. I know there are some things on my list that I don't quite know how to do. So let me know what you think of all of this and stay tuned! LOTS more to come!

This is just the intro to this series. Be sure to check out all of the blogs and projects in the series on the Main Off-Grid MakerShop page. 

-Kaleb

  • Sign in to reply
  • hifromkatie
    hifromkatie over 3 years ago

    We've got Mycroft running at home as a voice assistant in the kitchen, generally fine, but won't detect the children talking at all

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • beacon_dave
    beacon_dave over 3 years ago in reply to KalebTheMaker

    "...and there are some pretty clever ways of dealing with debris and getting air out of the system..."

    I'm getting the feeling that there could be a lot more clever ways of dealing with it in the foreseeable future. Slight smile   You have the advantage of introducing remote monitoring and remote actuators to the problem.

    I seem to recall one of the advantages of the crossflow turbine was that they tended to be self-cleaning as any debris entering at the top gets flushed out by the water passing through it and exiting at the bottom. Although perhaps not if it is a tree trunk which will tend to relocate your turbine some distance downstream given half the chance.

    What are the winter months going to be like? Any challenges there for off-grid power - panels covered in snow, frozen streams, massive demand for heat?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 3 years ago in reply to Fred27

    I grew up in a rural area (not that far from here) on five acres, and have always been a camping type of guy. But I did live in Sacramento for about 12 years prior to this. And I have never lived completely off the grid. The challenges are already here! haha

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • KalebTheMaker
    KalebTheMaker over 3 years ago in reply to beacon_dave

    Hydro is really interesting, and there are some pretty clever ways of dealing with debris and getting air out of the system. I am prepared to do regular maintenance on these systems if it does require clearing out a tank every few days. 

    About the north-facing, I would say it's the only downside to this property. But where I am located, water is a huge problem. There are two (and maybe a new third!) springs that are overflowing and the year-round stream. It was worth it to deal with placing my solar in a different location. Also, on the plus side, in the summer the shop will be in the shade for much of the day!

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
  • Fred27
    Fred27 over 3 years ago

    Wow - that's quite a project. From someone who has always lived in urban areas, I can hardly imagine the fun and freedom (and undoubtedly challenges) you have ahead of you.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • More
    • Cancel
<>