#badass Online Film Festival
  • Challenges & Projects
  • element14 presents
  • #badass Online Film Festival
  • More
  • Cancel
#badass Online Film Festival
Documents #badass Woman Project Entry - Roxana Bucina
  • Blog
  • Forum
  • Documents
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join #badass Online Film Festival to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Engagement
  • Author Author: kellyhensen
  • Date Created: 13 May 2020 6:50 PM Date Created
  • Last Updated Last Updated: 22 May 2020 1:39 PM
  • Views 3026 views
  • Likes 8 likes
  • Comments 14 comments
Related
Recommended

#badass Woman Project Entry - Roxana Bucina

Name:

Roxana Bucina

 

Current home town:

Bucharest, Romania

 

Did you attend university?

Institutul Politehnic Bucuresti, BS EE

Michigan Technological University, MS EE

 

Current Job:

English Teacher

 

Favorite projects from element14 presents or youtube:

https://www.youtube.com/watch?v=LtoBzOMwlRQ

 

Tell us about your project:

My project is a Display with LEDs.

Besides scrolling text my project displays rotating borders and images.

All three functions can be accessed using 2 switches, so it is a four-state display.

The images displayed are easily created by using the links given below:

 

My question is: How do I automatically send the *.ino file to Arduino? When I download it to the computer I want Arduino to start running it. Do I need an Ethernet Shield?

 

Are there any links or files you'd like to provide that support your project?  Code snips, 3d print files, etc.

 

Border Display

 

int scrollspeed = 50;

int flag=0;

//Columns

int clockPin1 = 2; //Arduino pin connected to Clock Pin 11 of 74HC595

int latchPin1 = 3; //Arduino pin connected to Latch Pin 12 of 74HC595

int dataPin1 = 4;  //Arduino pin connected to Data Pin 14 of 74HC595

 

 

//Rows

int clockPin2 = 5; //Arduino pin connected to Clock Pin 11 of 74HC595

int latchPin2 = 6; //Arduino pin connected to Latch Pin 12 of 74HC595

int dataPin2 = 7;  //Arduino pin connected to Data Pin 14 of 74HC595

 

 

//BITMAP

 

byte bitmap1[5][3]={

  {170,170,170},

  {0,0,1},

  {128,0,0},

{0,0,1},

  {170,170,170}

};

byte bitmap2[5][3]={

   {73,146, 4},

  {128,0,1},

  {0,0,0},

  {128,0,1},

  {36, 73, 255}

};

byte bitmap3[5][3]={

   {36,73,2},

  {128,0,1},

  {0,0,0},

  {128,0,1},

  {73, 146, 255}

};

void setup() {

  Serial.begin(9600);

  pinMode(latchPin1, OUTPUT);

  pinMode(clockPin1, OUTPUT);

  pinMode(dataPin1, OUTPUT);

 

 

  pinMode(latchPin2, OUTPUT);

  pinMode(clockPin2, OUTPUT);

  pinMode(dataPin2, OUTPUT);

 

 

  //Clear bitmap

  //for (int row = 0; row < 5; row++) {

  //  for (int zone = 0; zone <3; zone++) {

  //    bitmap[row][zone] = 0;

  //  }

//  }

}

//FUNCTIONS

// Displays bitmap array in the matrix

void RefreshDisplay()

{

  for (int row = 0; row < 5; row++) {

    int rowbit = 1 << row;

    digitalWrite(latchPin2, LOW);//Hold latchPin LOW for transmitting data

    shiftOut(dataPin2, clockPin2, MSBFIRST, rowbit);   //Transmit data

 

 

    //Start sending column bytes

    digitalWrite(latchPin1, LOW);//Hold latchPin LOW for transmitting data

 

 

    //Shift out to each matrix

    for (int zone = 0; zone < 3; zone++)

    {

      switch (flag){

        case 0:

      shiftOut(dataPin1, clockPin1, MSBFIRST, bitmap1[row][zone]);

      break;

      case 1:

      shiftOut(dataPin1, clockPin1, MSBFIRST, bitmap2[row][zone]);

      break;

      case 2:

      shiftOut(dataPin1, clockPin1, MSBFIRST, bitmap3[row][zone]);

      break;

      }

    }

   //flip both latches at once to eliminate flicker

    digitalWrite(latchPin1, HIGH);//Return the latch pin 1 high to signal chip

    digitalWrite(latchPin2, HIGH);//Return the latch pin 2 high to signal chip

    //Wait

    delayMicroseconds(50);

  }

}

// Plot each character of the message one column at a time, updated the display, shift bitmap left.

void XProcess()

{

 

      for (int refreshCount = 0; refreshCount < scrollspeed; refreshCount++)

      {

        RefreshDisplay();

 

          }

        }

 

void loop() {

  flag=(flag+1)%3;

  XProcess();

}

 

http://grafitgroup.ro/arduino.php

http://grafitgroup.ro/arduino3.php

 

Project video:

https://www.youtube.com/watch?v=lXalK3yUjXg&feature=youtu.be

You don't have permission to edit metadata of this video.
Edit media
x
image
Upload Preview
image

Attachments:
roxana-files.zip
  • badass
  • badass women makers and engineers
  • Share
  • History
  • More
  • Cancel
  • Sign in to reply

Top Comments

  • roccsi
    roccsi over 6 years ago in reply to davedarko +2
    Thank you I hope so too. This is the first time that I take part in element14 presents, next time I will be more attuned to the community and hopefully not in lockdown. This is a product that I am still…
  • rocits
    rocits over 6 years ago +1
    Can you enable playlists on your video so there is no viewing errors. I've added the video to a YouTube playlist here to keep track of channels/videos: https://www.youtube.com/watch?v=CFDZhLtOt5g&list…
  • roccsi
    roccsi over 6 years ago +1
    Thank you for your great advice! Yes there are so many things I can add! I have to see what webgl/threejs is all about. I've seen some examples and documents, I just hope it doesn't break an image into…
Parents
  • roccsi
    roccsi over 6 years ago

    Thank you for your great advice! Yes there are so many things I can add!

    I have to see what webgl/threejs is all about. I've seen some examples and documents, I just hope it doesn't break an image into bits and make my grid redundant. But even then my grid is easier to use than having to create an image first. And a device that outputs the image is still needed.

    I will use webgl for sure if it can improve the display.

    I didn't know that firefox could have helped me embed my code, that would have been very helpful (the truth is I tried to have as few video stops and restarts as possible, but my choice of filming printouts was not a good idea.)

    I listed the youtube video, is there anything else I should do for it to appear in a playlist?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Comment
  • roccsi
    roccsi over 6 years ago

    Thank you for your great advice! Yes there are so many things I can add!

    I have to see what webgl/threejs is all about. I've seen some examples and documents, I just hope it doesn't break an image into bits and make my grid redundant. But even then my grid is easier to use than having to create an image first. And a device that outputs the image is still needed.

    I will use webgl for sure if it can improve the display.

    I didn't know that firefox could have helped me embed my code, that would have been very helpful (the truth is I tried to have as few video stops and restarts as possible, but my choice of filming printouts was not a good idea.)

    I listed the youtube video, is there anything else I should do for it to appear in a playlist?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • More
    • Cancel
Children
  • rocits
    rocits over 6 years ago in reply to roccsi

    With threejs you have a massive amount of control for drawing, solid geometry & stylized post processing, then you can simply right click the page and save as an image/or automate the DataURL image into your system.

    https://threejs.org/examples/?q=pixe#webgl_postprocessing_pixel

     

    Sketch : https://two.js.org/examples/dynamic-vertices.html

    3D Paint : rompola.com

     

    If want just abstract artistic animation etc.. maybe look at :

    https://shadertoy.com

     

    Yep, your video is working fine on YT playlist now! Thanks!

    https://www.youtube.com/watch?v=lXalK3yUjXg&list=PLUqSARZt5KdEc90IqY_D4yOoR3qGEeSMC&index=12&t=0s