Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Electronic solution to replace A4/Letter-sized notices
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 2 replies
  • Subscribers 41 subscribers
  • Views 338 views
  • Users 0 members are here
  • epaper
  • digital_signage
  • low power
  • arduino
  • zigbee
Related

Electronic solution to replace A4/Letter-sized notices

beacon_dave
beacon_dave over 10 years ago

The majority of existing digital signage systems are expensive and also require power and data installing which can add to the cost.

 

The low power sleep modes of Atmel processors along with the likes of low power e-Paper display technology however could make a battery-based solution feasible. Low power wireless could potentially avoid the need for physical data wiring to the display.

 

Smart energy gas meters use Lithium thionyl Chloride cells which can power a ZigBee transmitter at 30minute intervals for around 12+ years which means that it should be possible to power a e-Paper display for at least couple of years before needing to replace the batteries.

 

Uses for this could include room booking information on meeting room doors, timetables for transport, wayfinding, etc. where the information may only be updating infrequently.

  • Sign in to reply
  • Cancel
Parents
  • clem57
    clem57 over 10 years ago

    interesting... Where are links to some of these things?

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • beacon_dave
    beacon_dave over 10 years ago in reply to clem57

    There is a low cost eval kit from Atmel/Pervasive displays although this only covers the smaller displays

    EPD Xplained Pro

    Pervasive Displays Inc. - EPD Xplained Pro

     

    Atmel application reference note

    http://www.atmel.com/images/atmel-42358-wireless-coin-cell-operated-wireless-epaper-display-applicationnote_at03303.pdf

     

    Larger ePaper displays are available however and this size would be about right for electronic notices

    Pervasive Displays - MpicoSys 10.2" Solutions

     

    The gas meter I have is:

    G370 ZigBee Smart Ultrasonic Gas Meter | Landis+Gyr

    which is powered by a Lithium thionyl chloride D cell which wirelessly outputs a meter reading every 30minutes over zigbee networking. estimated battery life >10years.

     

    Lithium thionyl chloride D cell

    SL2780/S - TADIRAN BATTERIES - Battery, Lithium Thionyl Chloride, 19 Ah, 3.6 V, D, Raised Positive and Negative, 32.9 mm…

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • beacon_dave
    beacon_dave over 10 years ago in reply to clem57

    There is a low cost eval kit from Atmel/Pervasive displays although this only covers the smaller displays

    EPD Xplained Pro

    Pervasive Displays Inc. - EPD Xplained Pro

     

    Atmel application reference note

    http://www.atmel.com/images/atmel-42358-wireless-coin-cell-operated-wireless-epaper-display-applicationnote_at03303.pdf

     

    Larger ePaper displays are available however and this size would be about right for electronic notices

    Pervasive Displays - MpicoSys 10.2" Solutions

     

    The gas meter I have is:

    G370 ZigBee Smart Ultrasonic Gas Meter | Landis+Gyr

    which is powered by a Lithium thionyl chloride D cell which wirelessly outputs a meter reading every 30minutes over zigbee networking. estimated battery life >10years.

     

    Lithium thionyl chloride D cell

    SL2780/S - TADIRAN BATTERIES - Battery, Lithium Thionyl Chloride, 19 Ah, 3.6 V, D, Raised Positive and Negative, 32.9 mm…