Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Group USB charging System for 24 or more
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 1 reply
  • Subscribers 41 subscribers
  • Views 334 views
  • Users 0 members are here
Related

Group USB charging System for 24 or more

e14 Contributor
e14 Contributor over 11 years ago

Too many wall warts.

 

     At least once a year I spent a great week on a houseboat. Approx between 20 to 30 people have many personal devices with them iPhones,iPads, iPods etc.

During the daytime the houseboat runs off the 12vdc battery system and at night time 2-4 hours the generator is running to charge up the batteries and to run 110vac stuff i.e microwave ovens.

What would be great is a project box with 24 or more USB female connectors mounted on the box to charge up 24 or more of these devices capable of 110vac or 12 vdc as the input to the transformer.

That way only the cables would be needed to connect without needing to use individual power supplies and cigarettes lighters plugs and 12 cube tapes to accommodate everyone's devices.

Can that be a future episode ?

  • Sign in to reply
  • Cancel
Parents
  • gadget.iom
    gadget.iom over 11 years ago

    A simple approach to this project could be to parallel a string of USB outputs as a bus.

    A PSU such as this could take care of the 12V DC provision: SD-15A-5 - MEAN WELL - CONVERTER, DC/DC, 15W, 5V | Farnell element14 UK and a PSU such as this could take care of the 110V AC supply: HWS30-5/A - TDK LAMBDA - PSU, 30W, 5V | Farnell element14 UK.

     

    These supplies could then be manually switched into the USB Bus with a changeover switch, depending on what supply is most appropriate at the the time.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • gadget.iom
    gadget.iom over 11 years ago

    A simple approach to this project could be to parallel a string of USB outputs as a bus.

    A PSU such as this could take care of the 12V DC provision: SD-15A-5 - MEAN WELL - CONVERTER, DC/DC, 15W, 5V | Farnell element14 UK and a PSU such as this could take care of the 110V AC supply: HWS30-5/A - TDK LAMBDA - PSU, 30W, 5V | Farnell element14 UK.

     

    These supplies could then be manually switched into the USB Bus with a changeover switch, depending on what supply is most appropriate at the the time.