Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Automated greenhouse system
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 4 replies
  • Subscribers 43 subscribers
  • Views 625 views
  • Users 0 members are here
Related

Automated greenhouse system

e14 Contributor
e14 Contributor over 11 years ago

Hi Ben!

I am interested in both growing plants and electronics. It would be nice if you could build a small grennhouse (maybe 1x1x1m) and use a raspberry pi to control a water pump to control humidity (perhaps a evaporator to create a mist or a dripping system), a fan to controll overheating and also a heatinglamp to control prevent freezing.   

  • Sign in to reply
  • Cancel
Parents
  • D_Hersey
    D_Hersey over 11 years ago

    A small greenhouse is called a 'cold-frame' where I come from.  It is amazing how popular things like bi-metals are in this game, still.  They are the ultimate in reliability. 

     

    Before you make a scheme to regulate humidity, measure it to see if that is a problem.  Many green plants actually like some variability in their params.  In the case of watering, letting the pot dry up a bit then watering it rather generously (with water with lotsa dissolved O)  rather than maintaining it in a damp condition is usually better.  It any small, harmful, organisms exist in the soil, they will not like drying up, a condition the large plant, with its ability to integrate moisture can survive for awhile.  I've even noticed that when I automatically water, the leaves of the plant open up a little prior to the watering event, convincing me that they have some way to tell time.

     

    Please give more specifics including drawings and/or pics.  This is an interesting project.

     

    Some cold frames have a coupla barrels of water at the bottom to integrate temperature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • D_Hersey
    D_Hersey over 11 years ago

    A small greenhouse is called a 'cold-frame' where I come from.  It is amazing how popular things like bi-metals are in this game, still.  They are the ultimate in reliability. 

     

    Before you make a scheme to regulate humidity, measure it to see if that is a problem.  Many green plants actually like some variability in their params.  In the case of watering, letting the pot dry up a bit then watering it rather generously (with water with lotsa dissolved O)  rather than maintaining it in a damp condition is usually better.  It any small, harmful, organisms exist in the soil, they will not like drying up, a condition the large plant, with its ability to integrate moisture can survive for awhile.  I've even noticed that when I automatically water, the leaves of the plant open up a little prior to the watering event, convincing me that they have some way to tell time.

     

    Please give more specifics including drawings and/or pics.  This is an interesting project.

     

    Some cold frames have a coupla barrels of water at the bottom to integrate temperature.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Children
  • e14 Contributor
    e14 Contributor over 11 years ago in reply to D_Hersey

    4x3-cedar-coldframe-lids-iso-1.jpg

    I was thinking about something like this with a dripping system to water the plants. If it is true what you say about the dry out thing then couldn´t you set the water sytem to active when the soil has been dry for a while. I am open for suggestions and are hoping for ideas, and maybe Ben will make one in a video.