Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum Two way Single wire communication without CLK
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 6 replies
  • Subscribers 44 subscribers
  • Views 1341 views
  • Users 0 members are here
  • Controllers
Related

Two way Single wire communication without CLK

moulirajesh
moulirajesh over 11 years ago

hi Ben,

i got a project for you can you interface two micro controllers to transmit and receive data with a single wire no clock line should be added as both the micro controllers should be able to transmit and receive

  • Sign in to reply
  • Cancel

Top Replies

  • michaelkellett
    michaelkellett over 11 years ago +1
    It's not that hard to do, original (10MHz co-ax cable) Ethernet works like that, CAN works like that (although usually uses two wires in a differential mode but it doesn't have to). So one reasonably easy…
  • michaelkellett
    michaelkellett over 11 years ago in reply to clem57 +1
    CAN and Ethernet have no concept of Master or Slave. LIN does and One-Wire sort of does but it can be worked round (although I wouldn't use it except as an utter last resort.) If the OP can tell us what…
Parents
  • johnbeetem
    johnbeetem over 11 years ago

    RS-485 is often used to daisy-chain a master to a bunch of slaves.  The master sends out a message that includes address bits and expects one of the slaves to respond.  RS-485 is differential pair (a good idea if you're going any distance) but you can go single wire if you like.  The UART has to ignore received data when it's transmitting -- this is called half duplex.

     

    IMO the OP is probably better off with UART (two signal wires) or SPI (2, 3, or 4 wires depending on what you want to do).

     

    As a footnote for your amusement, a lot of ARM processors use SWD (Single Wire Debug) in place of JTAG to talk to the chip's debug module.  I've only seen SWD implemented as two signal wires: clock and bi-directional data.  It's called SWD because there's an asynch version that uses a single data wire.  But since everyone implements the two-wire synchronous version, it's pretty silly calling it SWD image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • johnbeetem
    johnbeetem over 11 years ago

    RS-485 is often used to daisy-chain a master to a bunch of slaves.  The master sends out a message that includes address bits and expects one of the slaves to respond.  RS-485 is differential pair (a good idea if you're going any distance) but you can go single wire if you like.  The UART has to ignore received data when it's transmitting -- this is called half duplex.

     

    IMO the OP is probably better off with UART (two signal wires) or SPI (2, 3, or 4 wires depending on what you want to do).

     

    As a footnote for your amusement, a lot of ARM processors use SWD (Single Wire Debug) in place of JTAG to talk to the chip's debug module.  I've only seen SWD implemented as two signal wires: clock and bi-directional data.  It's called SWD because there's an asynch version that uses a single data wire.  But since everyone implements the two-wire synchronous version, it's pretty silly calling it SWD image