Ben Heck Featured Content
  • Challenges & Projects
  • element14 presents
  • element14's The Ben Heck Show
  • Ben Heck Featured Content
  • More
  • Cancel
Ben Heck Featured Content
Forum ARDUINO reef tank controller
  • Blog
  • Forum
  • Documents
  • Events
  • Polls
  • Files
  • Members
  • Mentions
  • Sub-Groups
  • Tags
  • More
  • Cancel
  • New
Join Ben Heck Featured Content to participate - click to join for free!
Actions
  • Share
  • More
  • Cancel
Forum Thread Details
  • Replies 10 replies
  • Subscribers 44 subscribers
  • Views 1232 views
  • Users 0 members are here
Related

ARDUINO reef tank controller

e14 Contributor
e14 Contributor over 11 years ago

reef tank controller.  Control light , water tem,  PH, dosing ,

  • Sign in to reply
  • Cancel

Top Replies

  • frankenpc
    frankenpc over 11 years ago +3
    I made one of those. Background I'm a salt water tank enthusiast. I wanted something sophisticated so I could automate many of the dull tasks. I started with a Arduino Mega as the foundation. I added an…
  • frankenpc
    frankenpc over 11 years ago in reply to balearicdynamics +1
    I used Atlas Scientific modules. All you do is solder on a BNC connector and a I2C bus to an Arduino and you can then issue a command to calibrate the new PH probe using three different PH solutions (low…
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to frankenpc +1
    Thank you Roger. It sounds strange to me that calibration don't need a precise ... calibrated value but only three average low/med/high. How can it be precise? Is there some trick ?
Parents
  • frankenpc
    frankenpc over 11 years ago

    I made one of those.  Background I'm a salt water tank enthusiast.  I wanted something sophisticated so I could automate many of the dull tasks. I started with a Arduino Mega as the foundation.  I added an ethernet/SD card shield.  I added PH and TDS probe I2C modules from Atlas Scientific and a RTC module (temperature compensated for accuracy). 

     

    I then built a bus based on RJ45 connectors.  It had 1 serial, 1 1-wire, I2C, and gnd/+5. 


    For power, I purchased one of those 8 channel DJ power centers.  It's just a glorified power strip with the ability to manually turn on/off each individual plug.  I created a I2C 8 channel relay module that I piggy-backed on the power center and wired it in. 

    For communications, I added two RJ45 jacks wired in parallel.  This allows me to run standard CAT 5 Ethernet between it and the Arduino while leaving a jack free to daisy chain to another power center if I so choose.

     

    On the power center I plugged in the following:

    • Main lighting
    • Moon light
    • Left wave pumps (for wave motion control)
    • Right wave pumps (for wave motion control)
    • Skimmer
    • Heater
    • Dosing pump 1
    • aux

     

    So in total, I had the following talking to the Arduino:

    • 8 channel power
    • 1 wire thermometer
    • PH
    • TDS
    • Clock
    • Keypad
    • LCD

     

    The application ran a sequential timer system along with the LCD update and keypad polling algorithms.  I integrated calibration routines in addition to everything else so I could do the three stage sensor calibrations (low/med/high solution calibration).  As far as the dosing pump goes, it was only doing kalkwasser top offs.  But I could easily done PH adjustments.  But I found the kalkwasser did fine.  The whole thing logged to a simple web page so I could monitor everything over Ethernet.  It stored the logs on the SD card in CSV format so I could dump it into a spreadsheet and view the trends.

     

    Yack yack yack...if you have any questions, let me know.


    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Reply
  • frankenpc
    frankenpc over 11 years ago

    I made one of those.  Background I'm a salt water tank enthusiast.  I wanted something sophisticated so I could automate many of the dull tasks. I started with a Arduino Mega as the foundation.  I added an ethernet/SD card shield.  I added PH and TDS probe I2C modules from Atlas Scientific and a RTC module (temperature compensated for accuracy). 

     

    I then built a bus based on RJ45 connectors.  It had 1 serial, 1 1-wire, I2C, and gnd/+5. 


    For power, I purchased one of those 8 channel DJ power centers.  It's just a glorified power strip with the ability to manually turn on/off each individual plug.  I created a I2C 8 channel relay module that I piggy-backed on the power center and wired it in. 

    For communications, I added two RJ45 jacks wired in parallel.  This allows me to run standard CAT 5 Ethernet between it and the Arduino while leaving a jack free to daisy chain to another power center if I so choose.

     

    On the power center I plugged in the following:

    • Main lighting
    • Moon light
    • Left wave pumps (for wave motion control)
    • Right wave pumps (for wave motion control)
    • Skimmer
    • Heater
    • Dosing pump 1
    • aux

     

    So in total, I had the following talking to the Arduino:

    • 8 channel power
    • 1 wire thermometer
    • PH
    • TDS
    • Clock
    • Keypad
    • LCD

     

    The application ran a sequential timer system along with the LCD update and keypad polling algorithms.  I integrated calibration routines in addition to everything else so I could do the three stage sensor calibrations (low/med/high solution calibration).  As far as the dosing pump goes, it was only doing kalkwasser top offs.  But I could easily done PH adjustments.  But I found the kalkwasser did fine.  The whole thing logged to a simple web page so I could monitor everything over Ethernet.  It stored the logs on the SD card in CSV format so I could dump it into a spreadsheet and view the trends.

     

    Yack yack yack...if you have any questions, let me know.


    • Cancel
    • Vote Up +3 Vote Down
    • Sign in to reply
    • Cancel
Children
  • gadget.iom
    gadget.iom over 11 years ago in reply to frankenpc

    Sounds like an excellent implementation image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to frankenpc

    It is an excellent implementation.

     

    Roger, how did you created the Ph-meter ? I am curious as I have done one but so many years ago that I remembered just now reading your post image

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • frankenpc
    frankenpc over 11 years ago in reply to balearicdynamics

    I used Atlas Scientific modules.  All you do is solder on a BNC connector and a I2C bus to an Arduino and you can then issue a command to calibrate the new PH probe using three different PH solutions (low/med/high) and you are set!  The module then polls the probe and sends the PH reading back to the Arduino.  It's a smart module as well.  As it polls the probe, it's averaging measurements to get a more reliable reading to compensate for noise.  Atlas makes taking measurements really easy.

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to frankenpc

    Thank you Roger. It sounds strange to me that calibration don't need a precise ... calibrated value but only three average low/med/high. How can it be precise? Is there some trick ?

    • Cancel
    • Vote Up +1 Vote Down
    • Sign in to reply
    • Cancel
  • frankenpc
    frankenpc over 11 years ago in reply to balearicdynamics

    The three are very precise calibration fluids.  I can't remember the exact numbers.  I THINK they were 2, 7, 10 if I remember correctly.  So, once the device knows which one the probe is immersed in, it knows exactly what the value should be.  Then, it calibrates a curve based on those three.  When you think about it, how would you obtain hundreds of precision PH mixtures necessary to exactly calibrate a PH probe?  For our purposes, it's accurate enough. 

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to frankenpc

    Mathematically 3 points determine a curve or straight line.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • balearicdynamics
    balearicdynamics over 11 years ago in reply to clem57

    Clem,

     

    in the cases of chemical measures - as many other environmental measures - it is not really true. Ph has not always a true linear conductivity variation but follows several kind of curves and there are many parameters that can influence the measure.

    • Cancel
    • Vote Up 0 Vote Down
    • Sign in to reply
    • Cancel
  • clem57
    clem57 over 11 years ago in reply to balearicdynamics

    No, I understand the nonlinear qualities of Ph. I just stated in Math 3 points are needed to determine if and only if one has a curve (Ph) or a straight line (some linear model). Aw many a angle as well. LOL